LESENSE_PerCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE

LESENSE peripheral control descriptor structure.

Definition at line 567 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

LESENSE_ControlACMP_TypeDef acmp0Mode
LESENSE_ControlACMP_TypeDef acmp1Mode
LESENSE_ControlDACConv_TypeDef dacCh0ConvMode
LESENSE_ControlDACData_TypeDef dacCh0Data
LESENSE_ControlDACOut_TypeDef dacCh0OutMode
LESENSE_ControlDACConv_TypeDef dacCh1ConvMode
LESENSE_ControlDACData_TypeDef dacCh1Data
LESENSE_ControlDACOut_TypeDef dacCh1OutMode
uint8_t dacPresc
LESENSE_DACRef_TypeDef dacRef
LESENSE_WarmupMode_TypeDef warmupMode

Field Documentation

LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode

Configure how LESENSE controls ACMP 0.

Definition at line 607 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode

Configure how LESENSE controls ACMP 1.

Definition at line 610 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0ConvMode

Configure how LESENSE controls conversion on DAC channel 0.

Definition at line 573 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data

Configure DAC channel 0 data control.

Definition at line 569 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0OutMode

Configure how LESENSE controls output on DAC channel 0.

Definition at line 578 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACConv_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1ConvMode

Configure how LESENSE controls conversion on DAC channel 1.

Definition at line 586 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data

Configure DAC channel 1 data control.

Definition at line 582 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ControlDACOut_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1OutMode

Configure how LESENSE controls output on DAC channel 1.

Definition at line 591 of file em_lesense.h .

Referenced by LESENSE_Init() .

uint8_t LESENSE_PerCtrlDesc_TypeDef::dacPresc

Configure the prescaling factor for the LESENSE - DAC interface. Valid range: 0-31 (5-bit).

Definition at line 597 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_DACRef_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacRef

Configure the DAC reference to be used. Set to lesenseDACRefVdd to use VDD and set to lesenseDACRefBandGap to use band gap as reference.

Definition at line 603 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode

Configure how LESENSE controls ACMPs and DAC in idle mode.

Definition at line 613 of file em_lesense.h .

Referenced by LESENSE_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_lesense.h