glib_circle.c File Reference
Silicon Labs Graphics Library: Circle Drawing Routines.
License
Copyright 2015 Silicon Labs, http://www.silabs.com
This file is licensensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        glib_circle.c
       
       .
      
       #include <stdint.h>
      
      
       #include "em_types.h"
      
      
       #include "
       
        glib.h
       
       "
      
      
| Functions | |
| EMSTATUS | GLIB_drawCircle ( GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius) | 
| Draws a circle with center at x, y, and a radius. | |
| EMSTATUS | GLIB_drawCircleFilled ( GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius) | 
| Draws a filled circle with center at x, y, and a radius. | |
| EMSTATUS | GLIB_drawPartialCircle ( GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius, uint8_t bitMask) | 
| Draws a partial circle with center at x, y, and a radius. | |
| static EMSTATUS | GLIB_drawPartialCirclePoints ( GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, int32_t x, int32_t y, uint8_t bitMask) | 
| Draws circle points using 8-way symmetry. | |
Function Documentation
| 
 | static | 
Draws circle points using 8-way symmetry.
Example: bitMask = 4 draws only pixels in 3. octant (00000100). bitMask = 5 draws only pixels in 3. and 1. octant (00000101).
- Parameters
- 
         pContextPointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenterCenter x-coordinate yCenterCenter y-coordinate xx-coordinate of circle point yy-coordinate of circle point bitMaskBitmask which decides which octants pixels should be drawn The LSB is 1. octant, and the MSB is 8. octant. The octants are ordered from 1 to 8 in counterclockwise order. 
- Returns
- 
         - Returns GLIB_OK on succes.
- Returns GLIB_ERROR_NOTHING_TO_DRAW if none of the points were drawn
- Returns error code otherwise
 
        Definition at line
        
         246
        
        of file
        
         glib_circle.c
        
        .
       
References GLIB_drawPixel() , GLIB_ERROR_NOTHING_TO_DRAW , and GLIB_OK .
Referenced by GLIB_drawPartialCircle() .