CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
       Definition at line
       
        2135
       
       of file
       
        em_cmu.h
       
       .
      
      
       #include <
       
     
        em_cmu.h
       
       >
      
| Data Fields | |
| bool | autoSelEm01 | 
| bool | autoStartEm01 | 
| bool | autoStartSelOnRacWakeup | 
| uint16_t | ctuneStartup | 
| uint16_t | ctuneSteadyState | 
| bool | lowPowerMode | 
| CMU_OscMode_TypeDef | mode | 
| uint8_t | regIshSteadyState | 
| uint8_t | thresholdPeakDetect | 
| uint8_t | timeoutPeakDetect | 
| uint8_t | timeoutShuntOptimization | 
| uint8_t | timeoutStartup | 
| uint8_t | timeoutSteady | 
| uint8_t | xoCoreBiasTrimStartup | 
| uint8_t | xoCoreBiasTrimSteadyState | 
Field Documentation
| bool CMU_HFXOInit_TypeDef::autoSelEm01 | 
- 
         
          Deprecated:
- Use CMU_HFXOAutostartEnable instead.
        Definition at line
        
         2147
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::autoStartEm01 | 
- 
         
          Deprecated:
- Use CMU_HFXOAutostartEnable instead.
        Definition at line
        
         2146
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup | 
- 
         
          Deprecated:
- Use CMU_HFXOAutostartEnable instead.
        Definition at line
        
         2148
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint16_t CMU_HFXOInit_TypeDef::ctuneStartup | 
Startup phase CTUNE (load capacitance) value
        Definition at line
        
         2149
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState | 
Steady-state phase CTUNE (load capacitance) value
        Definition at line
        
         2150
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::lowPowerMode | 
| CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode | 
| uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState | 
Shunt steady-state current
        Definition at line
        
         2151
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect | 
| uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect | 
| uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization | 
Timeout - shunt optimization
        Definition at line
        
         2155
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::timeoutStartup | 
| uint8_t CMU_HFXOInit_TypeDef::timeoutSteady | 
| uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup | 
Startup XO core bias current trim
        Definition at line
        
         2152
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState | 
Steady-state XO core bias current trim
        Definition at line
        
         2153
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_cmu.h