CRYOTIMER_TypeDef Struct ReferenceDevices > CRYOTIMER
CRYOTIMER Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32mg14p_cryotimer.h
       
       .
      
      
       #include <
       
     
        efr32mg14p_cryotimer.h
       
       >
      
| Data Fields | |
| __IM uint32_t | CNT | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | EM4WUEN | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | PERIODSEL | 
Field Documentation
| __IM uint32_t CRYOTIMER_TypeDef::CNT | 
Counter Value
        Definition at line
        
         52
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::EM4WUEN | 
Wake Up Enable
        Definition at line
        
         53
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         57
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IM uint32_t CRYOTIMER_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         54
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         56
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         55
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
| __IOM uint32_t CRYOTIMER_TypeDef::PERIODSEL | 
Interrupt Duration
        Definition at line
        
         51
        
        of file
        
         efr32mg14p_cryotimer.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/
       efr32mg14p_cryotimer.h