VDAC_InitChannel_TypeDef Struct ReferenceEMLIB > VDAC

VDAC channel initialization structure.

Definition at line 209 of file em_vdac.h .

#include < em_vdac.h >

Data Fields

bool enable
bool prsAsync
VDAC_PrsSel_TypeDef prsSel
bool sampleOffMode
VDAC_TrigMode_TypeDef trigMode

Field Documentation

bool VDAC_InitChannel_TypeDef::enable

Enable channel.

Definition at line 211 of file em_vdac.h .

Referenced by VDAC_InitChannel() .

bool VDAC_InitChannel_TypeDef::prsAsync

Treat the PRS signal asynchronously.

Definition at line 219 of file em_vdac.h .

Referenced by VDAC_InitChannel() .

VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if trigMode is set to vdacTrigModePrs or vdacTrigModeSwPrs .

Definition at line 216 of file em_vdac.h .

Referenced by VDAC_InitChannel() .

bool VDAC_InitChannel_TypeDef::sampleOffMode

Set channel conversion mode to sample/shut-off mode. Default is continuous.

Definition at line 226 of file em_vdac.h .

Referenced by VDAC_InitChannel() .

VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode

Channel conversion trigger mode.

Definition at line 222 of file em_vdac.h .

Referenced by VDAC_InitChannel() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_vdac.h