IDACEMLIB
Detailed Description
Current Digital-to-Analog Converter (IDAC) Peripheral API.
IDAC can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. Current is configurable with several ranges of various step sizes. IDAC can be used with PRS and can operate down to EM3.
The following steps are necessary for basic operation:
Clock enable:
Initialize peripheral with default settings and modify selected fields, such as output select:
Set output:
Data Structures | |
struct | IDAC_Init_TypeDef |
Macros | |
#define | IDAC_INIT_DEFAULT |
Enumerations | |
enum | IDAC_OutMode_TypeDef { idacOutputPin = IDAC_CTRL_OUTMODE_PIN, idacOutputADC = IDAC_CTRL_OUTMODE_ADC } |
enum | IDAC_PRSSEL_TypeDef { idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0, idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1, idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2, idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3, idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4, idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5 } |
enum | IDAC_Range_TypeDef { idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0, idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1, idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2, idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3 } |
Functions | |
void | IDAC_Enable (IDAC_TypeDef *idac, bool enable) |
Enable/disable IDAC. | |
void | IDAC_Init (IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init) |
Initialize IDAC. | |
void | IDAC_MinimalOutputTransitionMode (IDAC_TypeDef *idac, bool enable) |
Enable/disable Minimal Output Transition mode. | |
void | IDAC_OutEnable (IDAC_TypeDef *idac, bool enable) |
Enable/disable the IDAC OUT pin. | |
void | IDAC_RangeSet (IDAC_TypeDef *idac, const IDAC_Range_TypeDef range) |
Set the current range of the IDAC output. | |
void | IDAC_Reset (IDAC_TypeDef *idac) |
Reset IDAC to the same state that it was in after a hardware reset. | |
void | IDAC_StepSet (IDAC_TypeDef *idac, const uint32_t step) |
Set the current step of the IDAC output. | |
Macro Definition Documentation
#define IDAC_INIT_DEFAULT |
Default configuration for IDAC initialization structure.
Definition at line 193
of file em_idac.h
.
Enumeration Type Documentation
enum IDAC_OutMode_TypeDef |
enum IDAC_PRSSEL_TypeDef |
Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.
Enumerator | |
---|---|
idacPRSSELCh0 |
PRS channel 0. |
idacPRSSELCh1 |
PRS channel 1. |
idacPRSSELCh2 |
PRS channel 2. |
idacPRSSELCh3 |
PRS channel 3. |
idacPRSSELCh4 |
PRS channel 4. |
idacPRSSELCh5 |
PRS channel 5. |
Definition at line 135
of file em_idac.h
.
enum IDAC_Range_TypeDef |
Function Documentation
void IDAC_Enable | ( | IDAC_TypeDef * | idac, |
bool | enable |
||
) |
Enable/disable IDAC.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] enable
True to enable IDAC, false to disable.
Definition at line 115
of file em_idac.c
.
References _IDAC_CTRL_EN_SHIFT, BUS_RegBitWrite(), and IDAC_TypeDef::CTRL.
void IDAC_Init | ( | IDAC_TypeDef * | idac, |
const IDAC_Init_TypeDef * | init |
||
) |
Initialize IDAC.
Initializes IDAC according to the initialization structure parameter and sets the default calibration value stored in the DEVINFO structure.
- Note
- This function will disable IDAC prior to configuration.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] init
A pointer to the IDAC initialization structure.
Definition at line 78
of file em_idac.c
.
References IDAC_TypeDef::CTRL, IDAC_Init_TypeDef::enable, IDAC_CTRL_CURSINK, IDAC_CTRL_EN, IDAC_CTRL_OUTENPRS, IDAC_Init_TypeDef::outMode, IDAC_Init_TypeDef::prsEnable, IDAC_Init_TypeDef::prsSel, and IDAC_Init_TypeDef::sinkEnable.
void IDAC_MinimalOutputTransitionMode | ( | IDAC_TypeDef * | idac, |
bool | enable |
||
) |
Enable/disable Minimal Output Transition mode.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] enable
True to enable Minimal Output Transition mode, false to disable.
Definition at line 166
of file em_idac.c
.
References _IDAC_CTRL_MINOUTTRANS_SHIFT, BUS_RegBitWrite(), and IDAC_TypeDef::CTRL.
void IDAC_OutEnable | ( | IDAC_TypeDef * | idac, |
bool | enable |
||
) |
Enable/disable the IDAC OUT pin.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] enable
True to enable the IDAC OUT pin, false to disable.
Definition at line 331
of file em_idac.c
.
References _IDAC_CTRL_OUTEN_SHIFT, BUS_RegBitWrite(), and IDAC_TypeDef::CTRL.
void IDAC_RangeSet | ( | IDAC_TypeDef * | idac, |
const IDAC_Range_TypeDef | range |
||
) |
Set the current range of the IDAC output.
This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] range
The current range value.
Definition at line 188
of file em_idac.c
.
References _DEVINFO_IDAC0CAL0_RANGE0_MASK, _DEVINFO_IDAC0CAL0_RANGE0_SHIFT, _DEVINFO_IDAC0CAL0_RANGE1_MASK, _DEVINFO_IDAC0CAL0_RANGE1_SHIFT, _DEVINFO_IDAC0CAL0_RANGE2_MASK, _DEVINFO_IDAC0CAL0_RANGE2_SHIFT, _DEVINFO_IDAC0CAL0_RANGE3_MASK, _DEVINFO_IDAC0CAL0_RANGE3_SHIFT, _IDAC_CURPROG_RANGESEL_MASK, _IDAC_CURPROG_RANGESEL_SHIFT, IDAC_TypeDef::CAL, IDAC_TypeDef::CTRL, IDAC_TypeDef::CURPROG, DEVINFO, IDAC0, IDAC_CTRL_CURSINK, idacCurrentRange0, idacCurrentRange1, idacCurrentRange2, and idacCurrentRange3.
void IDAC_Reset | ( | IDAC_TypeDef * | idac | ) |
Reset IDAC to the same state that it was in after a hardware reset.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block.
Definition at line 128
of file em_idac.c
.
References _IDAC_CAL_RESETVALUE, _IDAC_CTRL_RESETVALUE, _IDAC_CURPROG_RESETVALUE, _IDAC_CURPROG_STEPSEL_SHIFT, _IDAC_DUTYCONFIG_RESETVALUE, IDAC_TypeDef::CAL, IDAC_TypeDef::CTRL, IDAC_TypeDef::CURPROG, IDAC_TypeDef::DUTYCONFIG, IDAC_CTRL_EN, IDAC_CURPROG_RANGESEL_RANGE0, and IDAC_DUTYCONFIG_DUTYCYCLEEN.
void IDAC_StepSet | ( | IDAC_TypeDef * | idac, |
const uint32_t | step |
||
) |
Set the current step of the IDAC output.
- Parameters
-
[in] idac
A pointer to the IDAC peripheral register block. [in] step
A step value for the IDAC output. A valid range is 0-31.
Definition at line 308
of file em_idac.c
.
References _IDAC_CURPROG_STEPSEL_MASK, _IDAC_CURPROG_STEPSEL_SHIFT, and IDAC_TypeDef::CURPROG.