IDAC_TypeDef Struct ReferenceDevices > EZR32HG_IDAC
       Definition at line
       
        48
       
       of file
       
        ezr32hg_idac.h
       
       .
      
| Data Fields | |
| __IOM uint32_t | CAL | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | CURPROG | 
| __IOM uint32_t | DUTYCONFIG | 
Field Documentation
| __IOM uint32_t IDAC_TypeDef::CAL | 
Calibration Register
        Definition at line
        
         51
        
        of file
        
         ezr32hg_idac.h
        
        .
       
Referenced by IDAC_RangeSet() , and IDAC_Reset() .
| __IOM uint32_t IDAC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32hg_idac.h
        
        .
       
Referenced by IDAC_Enable() , IDAC_Init() , IDAC_MinimalOutputTransitionMode() , IDAC_OutEnable() , IDAC_RangeSet() , and IDAC_Reset() .
| __IOM uint32_t IDAC_TypeDef::CURPROG | 
Current Programming Register
        Definition at line
        
         50
        
        of file
        
         ezr32hg_idac.h
        
        .
       
Referenced by IDAC_RangeSet() , IDAC_Reset() , and IDAC_StepSet() .
| __IOM uint32_t IDAC_TypeDef::DUTYCONFIG | 
Duty Cycle Configauration Register
        Definition at line
        
         52
        
        of file
        
         ezr32hg_idac.h
        
        .
       
Referenced by IDAC_Reset() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
       ezr32hg_idac.h