LEUARTEMLIB
Detailed Description
Low Energy Universal Asynchronous Receiver/Transmitter (LEUART) Peripheral API.
This module contains functions to control the LEUART peripheral of Silicon Labs 32-bit MCUs and SoCs. The LEUART module provides the full UART communication using a low frequency 32.768 kHz clock and has special features for communication without the CPU intervention.
| Data Structures | |
| struct | LEUART_Init_TypeDef | 
| Macros | |
| #define | LEUART_INIT_DEFAULT | 
| Enumerations | |
| enum | LEUART_Databits_TypeDef
         
         { leuartDatabits8 = LEUART_CTRL_DATABITS_EIGHT, leuartDatabits9 = LEUART_CTRL_DATABITS_NINE } | 
| enum | LEUART_Enable_TypeDef
         
         { leuartDisable = 0x0, leuartEnableRx = LEUART_CMD_RXEN, leuartEnableTx = LEUART_CMD_TXEN, leuartEnable = (LEUART_CMD_RXEN | LEUART_CMD_TXEN) } | 
| enum | LEUART_Parity_TypeDef
         
         { leuartNoParity = LEUART_CTRL_PARITY_NONE, leuartEvenParity = LEUART_CTRL_PARITY_EVEN, leuartOddParity = LEUART_CTRL_PARITY_ODD } | 
| enum | LEUART_Stopbits_TypeDef
         
         { leuartStopbits1 = LEUART_CTRL_STOPBITS_ONE, leuartStopbits2 = LEUART_CTRL_STOPBITS_TWO } | 
| Functions | |
| uint32_t | LEUART_BaudrateCalc (uint32_t refFreq, uint32_t clkdiv) | 
| Calculate the baudrate for the LEUART given reference frequency and clock division. | |
| uint32_t | LEUART_BaudrateGet ( LEUART_TypeDef *leuart) | 
| Get the current baudrate for LEUART. | |
| void | LEUART_BaudrateSet ( LEUART_TypeDef *leuart, uint32_t refFreq, uint32_t baudrate) | 
| Configure the baudrate (or as close as possible to a specified baudrate). | |
| void | LEUART_Enable ( LEUART_TypeDef *leuart, LEUART_Enable_TypeDef enable) | 
| Enable/disable the LEUART receiver and/or transmitter. | |
| void | LEUART_FreezeEnable ( LEUART_TypeDef *leuart, bool enable) | 
| LEUART register synchronization freeze control. | |
| void | LEUART_Init ( LEUART_TypeDef *leuart, LEUART_Init_TypeDef const *init) | 
| Initialize LEUART. | |
| __STATIC_INLINE void | LEUART_IntClear ( LEUART_TypeDef *leuart, uint32_t flags) | 
| Clear one or more pending LEUART interrupts. | |
| __STATIC_INLINE void | LEUART_IntDisable ( LEUART_TypeDef *leuart, uint32_t flags) | 
| Disable one or more LEUART interrupts. | |
| __STATIC_INLINE void | LEUART_IntEnable ( LEUART_TypeDef *leuart, uint32_t flags) | 
| Enable one or more LEUART interrupts. | |
| __STATIC_INLINE uint32_t | LEUART_IntGet ( LEUART_TypeDef *leuart) | 
| Get pending LEUART interrupt flags. | |
| __STATIC_INLINE uint32_t | LEUART_IntGetEnabled ( LEUART_TypeDef *leuart) | 
| Get enabled and pending LEUART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
| __STATIC_INLINE void | LEUART_IntSet ( LEUART_TypeDef *leuart, uint32_t flags) | 
| Set one or more pending LEUART interrupts from SW. | |
| void | LEUART_Reset ( LEUART_TypeDef *leuart) | 
| Reset LEUART to the same state that it was in after a hardware reset. | |
| uint8_t | LEUART_Rx ( LEUART_TypeDef *leuart) | 
| Receive one 8 bit frame, (or part of 9 bit frame). | |
| __STATIC_INLINE uint8_t | LEUART_RxDataGet ( LEUART_TypeDef *leuart) | 
| Receive one 8 bit frame, (or part of a 9 bit frame). | |
| __STATIC_INLINE uint16_t | LEUART_RxDataXGet ( LEUART_TypeDef *leuart) | 
| Receive one 8-9 bit frame, with extended information. | |
| void | LEUART_RxDmaInEM2Enable ( LEUART_TypeDef *leuart, bool enable) | 
| Enables handling of LEUART RX by DMA in EM2. | |
| uint16_t | LEUART_RxExt ( LEUART_TypeDef *leuart) | 
| Receive one 8-9 bit frame with extended information. | |
| __STATIC_INLINE uint32_t | LEUART_StatusGet ( LEUART_TypeDef *leuart) | 
| Get LEUART STATUS register. | |
| void | LEUART_Tx ( LEUART_TypeDef *leuart, uint8_t data) | 
| Transmit one frame. | |
| void | LEUART_TxDmaInEM2Enable ( LEUART_TypeDef *leuart, bool enable) | 
| Enables handling of LEUART TX by DMA in EM2. | |
| void | LEUART_TxExt ( LEUART_TypeDef *leuart, uint16_t data) | 
| Transmit one 8-9 bit frame with extended control. | |
Macro Definition Documentation
| #define LEUART_INIT_DEFAULT | 
Default configuration for LEUART initialization structure.
        Definition at line
        
         123
        
        of file
        
         em_leuart.h
        
        .
       
Referenced by BSP_BccInit() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
Enumeration Type Documentation
Function Documentation
| uint32_t LEUART_BaudrateCalc | ( | uint32_t | 
            refFreq,
            | 
| uint32_t | 
            clkdiv
            | ||
| ) | 
Calculate the baudrate for the LEUART given reference frequency and clock division.
This function returns the baudrate that a LEUART module will use if configured with the given frequency and clock divisor. Notice that this function will not use the hardware configuration. It can be used to determine if a given configuration is sufficiently accurate for the application.
- Parameters
- 
         [in] refFreqThe LEUART peripheral frequency used. [in] clkdivThe clock division factor to be used. 
- Returns
- A baudrate with given settings.
        Definition at line
        
         132
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_CLKDIV_MASK .
Referenced by LEUART_BaudrateGet() .
| uint32_t LEUART_BaudrateGet | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Get the current baudrate for LEUART.
This function returns the actual baudrate (not considering the oscillator inaccuracies) used by the LEUART peripheral.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. 
- Returns
- The current baudrate.
        Definition at line
        
         209
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_TypeDef::CLKDIV , CMU_ClockFreqGet() , cmuClock_LEUART0 , LEUART0 , and LEUART_BaudrateCalc() .
| void LEUART_BaudrateSet | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint32_t | 
            refFreq,
            | ||
| uint32_t | 
            baudrate
            | ||
| ) | 
Configure the baudrate (or as close as possible to a specified baudrate).
- Note
- The baudrate setting requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] refFreqThe LEUART reference clock frequency in Hz that will be used. If set to 0, the currently configured reference clock is assumed. [in] baudrateA baudrate to try to achieve for LEUART. 
        Definition at line
        
         253
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_CLKDIV_MASK , LEUART_TypeDef::CLKDIV , CMU_ClockFreqGet() , cmuClock_LEUART0 , LEUART0 , and LEUART_SYNCBUSY_CLKDIV .
Referenced by LEUART_Init() .
| void LEUART_Enable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| LEUART_Enable_TypeDef | 
            enable
            | ||
| ) | 
Enable/disable the LEUART receiver and/or transmitter.
Notice that this function does not do any configuration. Enabling should normally be done after the initialization is done (if not enabled as part of initialization).
- Note
- Enabling/disabling requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] enableSelect status for receiver/transmitter. 
        Definition at line
        
         345
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_CMD_RXEN_MASK , _LEUART_CMD_TXEN_MASK , LEUART_TypeDef::CMD , and LEUART_SYNCBUSY_CMD .
Referenced by RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| void LEUART_FreezeEnable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| bool | 
            enable
            | ||
| ) | 
LEUART register synchronization freeze control.
Some LEUART registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
- Note
- When enabling freeze mode, this function will wait for all current ongoing LEUART synchronization to the LF domain to complete (Normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] enable- True - enable freeze, modified registers are not propagated to the LF domain
- False - disables freeze, modified registers are propagated to the LF domain
 
        Definition at line
        
         392
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_TypeDef::FREEZE , LEUART_FREEZE_REGFREEZE , and LEUART_TypeDef::SYNCBUSY .
Referenced by LEUART_Init() , and LEUART_Reset() .
| void LEUART_Init | ( | LEUART_TypeDef * | 
            leuart,
            | 
| LEUART_Init_TypeDef const * | 
            init
            | ||
| ) | 
Initialize LEUART.
        This function will configure basic settings to operate in normal asynchronous mode. Consider using
        
         LEUART_Reset()
        
        prior to this function if the state of configuration is not known, since only configuration settings specified by
        
         init
        
        are set.
       
Special control setup not covered by this function may be done either before or after using this function (but normally before enabling) by direct modification of the CTRL register.
Notice that pins used by the LEUART module must be properly configured by the user explicitly for the LEUART to work as intended. (When configuring pins consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Note
- Initializing requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] initA pointer to the initialization structure used to configure basic async setup. 
        Definition at line
        
         444
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_CTRL_PARITY_MASK , _LEUART_CTRL_STOPBITS_MASK , LEUART_Init_TypeDef::baudrate , LEUART_TypeDef::CMD , LEUART_TypeDef::CTRL , LEUART_Init_TypeDef::databits , LEUART_Init_TypeDef::enable , LEUART_BaudrateSet() , LEUART_CMD_RXDIS , LEUART_CMD_TXDIS , LEUART_FreezeEnable() , LEUART_SYNCBUSY_CMD , LEUART_Init_TypeDef::parity , LEUART_Init_TypeDef::refFreq , and LEUART_Init_TypeDef::stopbits .
Referenced by BSP_BccInit() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| __STATIC_INLINE void LEUART_IntClear | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Clear one or more pending LEUART interrupts.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. [in] flagsPending LEUART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for LEUART module (LEUART_IF_nnn). 
        Definition at line
        
         159
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IFC .
Referenced by RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| __STATIC_INLINE void LEUART_IntDisable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Disable one or more LEUART interrupts.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. [in] flagsLEUART interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for LEUART module (LEUART_IF_nnn). 
        Definition at line
        
         175
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IEN .
Referenced by disableRxInterrupt() .
| __STATIC_INLINE void LEUART_IntEnable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Enable one or more LEUART interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LEUART_IntClear() prior to enabling the interrupt.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. [in] flagsLEUART interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for LEUART module (LEUART_IF_nnn). 
        Definition at line
        
         196
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IEN .
Referenced by enableRxInterrupt() , and RETARGET_SerialInit() .
| __STATIC_INLINE uint32_t LEUART_IntGet | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Get pending LEUART interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. 
- Returns
- LEUART interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for LEUART module (LEUART_IF_nnn).
        Definition at line
        
         215
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IF .
| __STATIC_INLINE uint32_t LEUART_IntGetEnabled | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Get enabled and pending LEUART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. 
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled LEUART interrupt sources. The return value is the bitwise AND combination of
         - the OR combination of enabled interrupt sources in LEUARTx_IEN_nnn register (LEUARTx_IEN_nnn) and
- the OR combination of valid interrupt flags of LEUART module (LEUARTx_IF_nnn).
 
        Definition at line
        
         239
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IEN , and LEUART_TypeDef::IF .
| __STATIC_INLINE void LEUART_IntSet | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Set one or more pending LEUART interrupts from SW.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. [in] flagsLEUART interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for LEUART module (LEUART_IF_nnn). 
        Definition at line
        
         262
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::IFS .
| void LEUART_Reset | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Reset LEUART to the same state that it was in after a hardware reset.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. 
        Definition at line
        
         482
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_CLKDIV_RESETVALUE , _LEUART_CTRL_RESETVALUE , _LEUART_IEN_RESETVALUE , _LEUART_IFC_MASK , _LEUART_PULSECTRL_RESETVALUE , _LEUART_ROUTE_RESETVALUE , _LEUART_SIGFRAME_RESETVALUE , _LEUART_STARTFRAME_RESETVALUE , LEUART_TypeDef::CLKDIV , LEUART_TypeDef::CMD , LEUART_TypeDef::CTRL , LEUART_TypeDef::IEN , LEUART_TypeDef::IFC , LEUART_CMD_CLEARRX , LEUART_CMD_CLEARTX , LEUART_CMD_RXBLOCKDIS , LEUART_CMD_RXDIS , LEUART_CMD_TXDIS , LEUART_FreezeEnable() , LEUART_TypeDef::PULSECTRL , LEUART_TypeDef::ROUTE , LEUART_TypeDef::SIGFRAME , and LEUART_TypeDef::STARTFRAME .
Referenced by BSP_BccDeInit() , and UARTDRV_DeInit() .
| uint8_t LEUART_Rx | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Receive one 8 bit frame, (or part of 9 bit frame).
This function is normally used to receive one frame when operating with frame length 8 bits. See LEUART_RxExt() for reception of 9 bit frames.
Notice that possible parity/stop bits are not considered a part of the specified frame bit length.
- Note
- This function will stall if the buffer is empty until data is received.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. 
- Returns
- Data received.
        Definition at line
        
         532
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_STATUS_RXDATAV , LEUART_TypeDef::RXDATA , and LEUART_TypeDef::STATUS .
| __STATIC_INLINE uint8_t LEUART_RxDataGet | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Receive one 8 bit frame, (or part of a 9 bit frame).
Used to quickly receive one 8 bit frame by reading RXDATA register directly, without checking STATUS register for RXDATAV flag. This can be useful from RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read received data. Please refer to LEUART_RxDataXGet() for reception of 9 bit frames.
- Note
- Since this function does not check if the RXDATA register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The LEUART_Rx() is normally a better choice if the validity of the RXDATA register is not certain.
- Notice that possible parity/stop bits are not considered part of specified frame bit length.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. 
- Returns
- Data received.
        Definition at line
        
         317
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::RXDATA .
| __STATIC_INLINE uint16_t LEUART_RxDataXGet | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Receive one 8-9 bit frame, with extended information.
Used to quickly receive one 8-9 bit frame with extended information by reading RXDATAX register directly, without checking STATUS register for RXDATAV flag. This can be useful from RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read received data.
- Note
- Since this function does not check if the RXDATAX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The LEUART_RxExt() is normally a better choice if the validity of the RXDATAX register is not certain.
- Notice that possible parity/stop bits are not considered part of specified frame bit length.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. 
- Returns
- Data received.
        Definition at line
        
         350
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::RXDATAX .
| void LEUART_RxDmaInEM2Enable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| bool | 
            enable
            | ||
| ) | 
Enables handling of LEUART RX by DMA in EM2.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] enableTrue - enables functionality False - disables functionality 
        Definition at line
        
         691
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_STATUS_RXENS_MASK , LEUART_TypeDef::CMD , LEUART_TypeDef::CTRL , LEUART_CMD_RXDIS , LEUART_CMD_RXEN , LEUART_CTRL_RXDMAWU , LEUART_SYNCBUSY_CMD , LEUART_SYNCBUSY_CTRL , and LEUART_TypeDef::STATUS .
| uint16_t LEUART_RxExt | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Receive one 8-9 bit frame with extended information.
This function is normally used to receive one frame and additional RX status information is required.
- Note
- This function will stall if buffer is empty until data is received.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. 
- Returns
- Data received.
        Definition at line
        
         557
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_STATUS_RXDATAV , LEUART_TypeDef::RXDATAX , and LEUART_TypeDef::STATUS .
| __STATIC_INLINE uint32_t LEUART_StatusGet | ( | LEUART_TypeDef * | 
            leuart
            | ) | 
Get LEUART STATUS register.
- Parameters
- 
         [in] leuartPointer to LEUART peripheral register block. 
- Returns
- STATUS register value.
        Definition at line
        
         278
        
        of file
        
         em_leuart.h
        
        .
       
References LEUART_TypeDef::STATUS .
| void LEUART_Tx | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint8_t | 
            data
            | ||
| ) | 
Transmit one frame.
        Depending on the frame length configuration, 8 (least significant) bits from
        
         data
        
        are transmitted. If the frame length is 9, 8 bits are transmitted from
        
         data
        
        and one bit as specified by the CTRL register, BIT8DV field. See
        
         LEUART_TxExt()
        
        for transmitting 9 bit frame with full control of all 9 bits.
       
Notice that possible parity/stop bits in asynchronous mode are not considered a part of the specified frame bit length.
- Note
- This function will stall if buffer is full until the buffer becomes available.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] dataData to transmit. See details above for more info. 
        Definition at line
        
         588
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_STATUS_TXBL , LEUART_SYNCBUSY_TXDATA , LEUART_TypeDef::STATUS , and LEUART_TypeDef::TXDATA .
Referenced by UARTDRV_ForceTransmit() .
| void LEUART_TxDmaInEM2Enable | ( | LEUART_TypeDef * | 
            leuart,
            | 
| bool | 
            enable
            | ||
| ) | 
Enables handling of LEUART TX by DMA in EM2.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] enableTrue - enables functionality False - disables functionality 
        Definition at line
        
         643
        
        of file
        
         em_leuart.c
        
        .
       
References _LEUART_STATUS_TXENS_MASK , LEUART_TypeDef::CMD , LEUART_TypeDef::CTRL , LEUART_CMD_TXDIS , LEUART_CMD_TXEN , LEUART_CTRL_TXDMAWU , LEUART_SYNCBUSY_CMD , LEUART_SYNCBUSY_CTRL , and LEUART_TypeDef::STATUS .
| void LEUART_TxExt | ( | LEUART_TypeDef * | 
            leuart,
            | 
| uint16_t | 
            data
            | ||
| ) | 
Transmit one 8-9 bit frame with extended control.
Notice that possible parity/stop bits in asynchronous mode are not considered a part of the specified frame bit length.
- Note
- This function will stall if the buffer is full until the buffer becomes available.
- Parameters
- 
         [in] leuartA pointer to the LEUART peripheral register block. [in] dataData to transmit with extended control. Least significant bit contains frame bits and additional control bits are available as documented in the reference manual (set to 0 if not used). 
        Definition at line
        
         619
        
        of file
        
         em_leuart.c
        
        .
       
References LEUART_STATUS_TXBL , LEUART_SYNCBUSY_TXDATAX , LEUART_TypeDef::STATUS , and LEUART_TypeDef::TXDATAX .