EZRADIODRV_PacketRxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Receive_Plugin
EzRadio receive plug-in instance initialization and handler structure.
       Definition at line
       
        65
       
       of file
       
        ezradio_receive_plugin.h
       
       .
      
      
       #include <
       
     
        ezradio_receive_plugin.h
       
       >
      
| Data Fields | |
| uint8_t | channel | 
| Reception channel. | |
| uint8_t * | pktBuf | 
| Pointer to the receive buffer. | |
| EZRADIODRV_Callback_t | userCallback | 
| User callback. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emdrv/ezradiodrv/plugins/inc/
       ezradio_receive_plugin.h