CMU_TypeDef Struct ReferenceDevices > EZR32HG_CMU
Definition at line
48
of file
ezr32hg_cmu.h
.
Data Fields |
|
| __IOM uint32_t | AUXHFRCOCTRL |
| __IOM uint32_t | CALCNT |
| __IOM uint32_t | CALCTRL |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FREEZE |
| __IOM uint32_t | HFCORECLKDIV |
| __IOM uint32_t | HFCORECLKEN0 |
| __IOM uint32_t | HFPERCLKDIV |
| __IOM uint32_t | HFPERCLKEN0 |
| __IOM uint32_t | HFRCOCTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LFACLKEN0 |
| __IOM uint32_t | LFAPRESC0 |
| __IOM uint32_t | LFBCLKEN0 |
| __IOM uint32_t | LFBPRESC0 |
| __IOM uint32_t | LFCCLKEN0 |
| __IOM uint32_t | LFCLKSEL |
| __IOM uint32_t | LFRCOCTRL |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | OSCENCMD |
| __IOM uint32_t | PCNTCTRL |
| uint32_t | RESERVED0 [2U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED2 [1U] |
| uint32_t | RESERVED3 [1U] |
| uint32_t | RESERVED4 [1U] |
| uint32_t | RESERVED5 [18U] |
| __IOM uint32_t | ROUTE |
| __IM uint32_t | STATUS |
| __IM uint32_t | SYNCBUSY |
| __IOM uint32_t | USBCRCTRL |
| __IOM uint32_t | USHFRCOCONF |
| __IOM uint32_t | USHFRCOCTRL |
| __IOM uint32_t | USHFRCOTUNE |
Field Documentation
| __IOM uint32_t CMU_TypeDef::AUXHFRCOCTRL |
AUXHFRCO Control Register
Definition at line
54
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::CALCNT |
Calibration Counter Register
Definition at line
56
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::CALCTRL |
Calibration Control Register
Definition at line
55
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::CMD |
Command Register
Definition at line
58
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::CTRL |
CMU Control Register
Definition at line
49
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::FREEZE |
Freeze Register
Definition at line
69
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::HFCORECLKDIV |
High Frequency Core Clock Division Register
Definition at line
50
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::HFCORECLKEN0 |
High Frequency Core Clock Enable Register 0
Definition at line
65
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::HFPERCLKDIV |
High Frequency Peripheral Clock Division Register
Definition at line
51
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::HFPERCLKEN0 |
High Frequency Peripheral Clock Enable Register 0
Definition at line
66
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::HFRCOCTRL |
HFRCO Control Register
Definition at line
52
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line
64
of file
ezr32hg_cmu.h
.
| __IM uint32_t CMU_TypeDef::IF |
Interrupt Flag Register
Definition at line
61
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
63
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
62
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFACLKEN0 |
Low Frequency A Clock Enable Register 0 (Async Reg)
Definition at line
70
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFAPRESC0 |
Low Frequency A Prescaler Register 0 (Async Reg)
Definition at line
74
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFBCLKEN0 |
Low Frequency B Clock Enable Register 0 (Async Reg)
Definition at line
72
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFBPRESC0 |
Low Frequency B Prescaler Register 0 (Async Reg)
Definition at line
76
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFCCLKEN0 |
Low Frequency C Clock Enable Register 0 (Async Reg)
Definition at line
73
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFCLKSEL |
Low Frequency Clock Select Register
Definition at line
59
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LFRCOCTRL |
LFRCO Control Register
Definition at line
53
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line
82
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::OSCENCMD |
Oscillator Enable/Disable Command Register
Definition at line
57
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::PCNTCTRL |
PCNT Control Register
Definition at line
78
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line
67
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
71
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line
75
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED3[1U] |
Reserved for future use
Definition at line
77
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED4[1U] |
Reserved for future use
Definition at line
80
of file
ezr32hg_cmu.h
.
| uint32_t CMU_TypeDef::RESERVED5[18U] |
Reserved for future use
Definition at line
84
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::ROUTE |
I/O Routing Register
Definition at line
81
of file
ezr32hg_cmu.h
.
| __IM uint32_t CMU_TypeDef::STATUS |
Status Register
Definition at line
60
of file
ezr32hg_cmu.h
.
| __IM uint32_t CMU_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
68
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::USBCRCTRL |
USB Clock Recovery Control
Definition at line
85
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::USHFRCOCONF |
USHFRCO Configuration
Definition at line
88
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::USHFRCOCTRL |
USHFRCO Control
Definition at line
86
of file
ezr32hg_cmu.h
.
| __IOM uint32_t CMU_TypeDef::USHFRCOTUNE |
USHFRCO Frequency Tune
Definition at line
87
of file
ezr32hg_cmu.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32HG/Include/
ezr32hg_cmu.h