EZRADIODRV_FieldLength Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin

EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.

Definition at line 84 of file ezradio_transmit_plugin.h .

#include < ezradio_transmit_plugin.h >

Data Fields

uint8_t f1
Field 1 length.
uint8_t f2
Field 2 length.
uint8_t f3
Field 3 length.
uint8_t f4
Field 4 length.
uint8_t f5
Field 5 length.

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/ezradiodrv/plugins/inc/ ezradio_transmit_plugin.h