CapSenseKit Drivers
Functions | |
uint32_t | CAPLESENSE_getNormalizedVal (uint8_t channel) |
Get the current normalized channelValue for a channel. | |
uint8_t | CAPLESENSE_getSegmentChannel (uint8_t capSegment) |
Get the channelValue for a sensor segment. | |
int32_t | CAPLESENSE_getSliderPosition (void) |
Get the position of the slider. | |
uint32_t | CAPLESENSE_getVal (uint8_t channel) |
Get the current channelValue for a channel. | |
void | CAPLESENSE_Init (bool sleep) |
Initializes the capacative sense system without LESENSE. | |
void | CAPLESENSE_setupCallbacks (void(*scanCb)(void), void(*chCb)(void)) |
LESENSE callback setup. | |
void | CAPLESENSE_setupLESENSE (bool sleep) |
Setup the LESENSE for capavitive sensing. | |
void | CAPLESENSE_Sleep (void) |
Send the capacative sense system to sleep mode. | |
uint32_t | CAPSENSE_getNormalizedVal (uint8_t channel) |
Get the current normalized channelValue for a channel. | |
bool | CAPSENSE_getPressed (uint8_t channel) |
Get the state of the Gecko Button. | |
int32_t | CAPSENSE_getSliderPosition (void) |
Get the position of the slider. | |
uint32_t | CAPSENSE_getVal (uint8_t channel) |
Get the current channelValue for a channel. | |
void | CAPSENSE_Init (void) |
Initializes the capacitive sense system. | |
void | CAPSENSE_Sense (void) |
This function iterates through all the capsensors and reads and initiates a reading. Uses EM1 while waiting for the result from each sensor. | |
Function Documentation
uint32_t CAPLESENSE_getNormalizedVal | ( | uint8_t | channel | ) |
Get the current normalized channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channel value in range (0-256).
Definition at line 425
of file caplesense.c
.
References channelMaxValues, and channelValues.
uint8_t CAPLESENSE_getSegmentChannel | ( | uint8_t | capSegment | ) |
Get the channelValue for a sensor segment.
- Parameters
-
capSegment
- Returns
- channel
Definition at line 389
of file caplesense.c
.
int32_t CAPLESENSE_getSliderPosition | ( | void |
| ) |
Get the position of the slider.
- Returns
- The position of the slider if it can be determined, -1 otherwise.
Definition at line 436
of file caplesense.c
.
References channelMaxValues, and channelValues.
uint32_t CAPLESENSE_getVal | ( | uint8_t | channel | ) |
Get the current channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channelValue.
Definition at line 415
of file caplesense.c
.
References channelValues.
void CAPLESENSE_Init | ( | bool | sleep | ) |
Initializes the capacative sense system without LESENSE.
- Parameters
-
sleep
If true, go into sleep mode.
Definition at line 501
of file caplesense.c
.
References CAPLESENSE_setupACMP(), CAPLESENSE_setupCMU(), CAPLESENSE_setupGPIO(), CAPLESENSE_setupLESENSE(), CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, and CORE_EXIT_ATOMIC.
void CAPLESENSE_setupCallbacks | ( | void(*)(void) | scanCb, |
void(*)(void) | chCb |
||
) |
LESENSE callback setup.
- Parameters
-
scanCb
Scan callback chCb
Channel callback
Definition at line 330
of file caplesense.c
.
References lesenseChCb, and lesenseScanCb.
void CAPLESENSE_setupLESENSE | ( | bool | sleep | ) |
Setup the LESENSE for capavitive sensing.
- Parameters
-
sleep
If true, go into sleep mode.
Definition at line 163
of file caplesense.c
.
References channelsInUse, LESENSE_Init_TypeDef::coreCtrl, LESENSE, LESENSE_ChannelAllConfig(), LESENSE_ChannelThresSet(), LESENSE_ClkDivSet(), LESENSE_Init(), LESENSE_IntClear(), LESENSE_IntDisable(), LESENSE_IntEnable(), LESENSE_IRQn, LESENSE_ResultBufferClear(), LESENSE_ScanFreqSet(), LESENSE_ScanResultDataBufferGet(), LESENSE_ScanStart(), LESENSE_ScanStop(), LESENSE_STATUS_BUFHALFFULL, LESENSE_STATUS_SCANACTIVE, LESENSE_StatusGet(), lesenseACMPModeMuxThres, lesenseBiasModeDutyCycle, lesenseBufTrigHalf, lesenseClkDiv_1, lesenseClkDiv_8, lesenseClkLF, lesenseDACConvModeDisable, lesenseDACIfData, lesenseDACOutModeDisable, lesenseDACRefBandGap, lesenseDecInputSensorSt, lesenseDMAWakeUpDisable, lesensePRSCh0, lesensePRSCh1, lesensePRSCh2, lesensePRSCh3, lesenseScanConfDirMap, lesenseScanStartPeriodic, lesenseWarmupModeNormal, and LESENSE_CoreCtrlDesc_TypeDef::scanStart.
Referenced by CAPLESENSE_Init().
uint32_t CAPSENSE_getNormalizedVal | ( | uint8_t | channel | ) |
Get the current normalized channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channel value in range (0-256).
Definition at line 132
of file capsense.c
.
References channelMaxValues, and channelValues.
bool CAPSENSE_getPressed | ( | uint8_t | channel | ) |
Get the state of the Gecko Button.
- Parameters
-
channel
The channel.
- Returns
- true if the button is "pressed" false otherwise.
Definition at line 144
of file capsense.c
.
References channelMaxValues, and channelValues.
int32_t CAPSENSE_getSliderPosition | ( | void |
| ) |
Get the position of the slider.
- Returns
- The position of the slider if it can be determined, -1 otherwise.
Definition at line 164
of file capsense.c
.
References channelMaxValues, and channelValues.
uint32_t CAPSENSE_getVal | ( | uint8_t | channel | ) |
Get the current channelValue for a channel.
- Parameters
-
channel
The channel.
- Returns
- The channelValue.
Definition at line 122
of file capsense.c
.
References channelValues.
void CAPSENSE_Init | ( | void |
| ) |
Initializes the capacitive sense system.
Capacitive sensing uses two timers: TIMER0 and TIMER1 as well as ACMP. ACMP is set up in cap-sense (oscillator mode). TIMER1 counts the number of pulses generated by ACMP_CAPSENSE. When TIMER0 expires it generates an interrupt. The number of pulses counted by TIMER1 is then stored in channelValues
Definition at line 284
of file capsense.c
.
References ACMP_CAPSENSE_INIT_DEFAULT, ACMP_CapsenseInit(), CMU, CMU_ClockEnable(), cmuClock_HFPER, cmuClock_PRS, cmuClock_TIMER0, cmuClock_TIMER1, PRS, PRS_CH_CTRL_EDSEL_POSEDGE, TIMER0, TIMER0_IRQn, TIMER1, TIMER_CC_CTRL_ICEDGE_BOTH, TIMER_CC_CTRL_ICEVCTRL_RISING, TIMER_CC_CTRL_INSEL_PRS, TIMER_CC_CTRL_MODE_INPUTCAPTURE, TIMER_CC_CTRL_PRSSEL_PRSCH0, TIMER_CTRL_CLKSEL_CC1, TIMER_CTRL_PRESC_DIV1024, TIMER_CTRL_PRESC_DIV512, and TIMER_IEN_OF.