USB_DIEP_TypeDef Struct ReferenceDevices
USB_DIEP EZR32LG USB DIEP.
Definition at line
46
of file
ezr32lg_usb_diep.h
.
#include <
ezr32lg_usb_diep.h
>
Data Fields |
|
| __IOM uint32_t | CTL |
| __IOM uint32_t | DMAADDR |
| __IOM uint32_t | INT |
| uint32_t | RESERVED0 [1] |
| uint32_t | RESERVED1 [1] |
| uint32_t | RESERVED2 [1] |
| __IOM uint32_t | TSIZ |
| __IM uint32_t | TXFSTS |
Field Documentation
| __IOM uint32_t USB_DIEP_TypeDef::CTL |
Device IN Endpoint x+1 Control Register
Definition at line
47
of file
ezr32lg_usb_diep.h
.
| __IOM uint32_t USB_DIEP_TypeDef::DMAADDR |
Device IN Endpoint x+1 DMA Address Register
Definition at line
52
of file
ezr32lg_usb_diep.h
.
| __IOM uint32_t USB_DIEP_TypeDef::INT |
Device IN Endpoint x+1 Interrupt Register
Definition at line
49
of file
ezr32lg_usb_diep.h
.
| uint32_t USB_DIEP_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line
48
of file
ezr32lg_usb_diep.h
.
| uint32_t USB_DIEP_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line
50
of file
ezr32lg_usb_diep.h
.
| uint32_t USB_DIEP_TypeDef::RESERVED2[1] |
Reserved future
Definition at line
54
of file
ezr32lg_usb_diep.h
.
| __IOM uint32_t USB_DIEP_TypeDef::TSIZ |
Device IN Endpoint x+1 Transfer Size Register
Definition at line
51
of file
ezr32lg_usb_diep.h
.
| __IM uint32_t USB_DIEP_TypeDef::TXFSTS |
Device IN Endpoint x+1 Transmit FIFO Status Register
Definition at line
53
of file
ezr32lg_usb_diep.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
ezr32lg_usb_diep.h