USB_HC_TypeDef Struct ReferenceDevices
USB_HC EZR32LG USB HC.
Definition at line
46
of file
ezr32lg_usb_hc.h
.
#include <
ezr32lg_usb_hc.h
>
Data Fields |
|
| __IOM uint32_t | CHAR |
| __IOM uint32_t | DMAADDR |
| __IOM uint32_t | INT |
| __IOM uint32_t | INTMSK |
| uint32_t | RESERVED0 [1] |
| uint32_t | RESERVED1 [2] |
| __IOM uint32_t | TSIZ |
Field Documentation
| __IOM uint32_t USB_HC_TypeDef::CHAR |
Host Channel x Characteristics Register
Definition at line
47
of file
ezr32lg_usb_hc.h
.
| __IOM uint32_t USB_HC_TypeDef::DMAADDR |
Host Channel x DMA Address Register
Definition at line
52
of file
ezr32lg_usb_hc.h
.
| __IOM uint32_t USB_HC_TypeDef::INT |
Host Channel x Interrupt Register
Definition at line
49
of file
ezr32lg_usb_hc.h
.
| __IOM uint32_t USB_HC_TypeDef::INTMSK |
Host Channel x Interrupt Mask Register
Definition at line
50
of file
ezr32lg_usb_hc.h
.
| uint32_t USB_HC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line
48
of file
ezr32lg_usb_hc.h
.
| uint32_t USB_HC_TypeDef::RESERVED1[2] |
Reserved future
Definition at line
53
of file
ezr32lg_usb_hc.h
.
| __IOM uint32_t USB_HC_TypeDef::TSIZ |
Host Channel x Transfer Size Register
Definition at line
51
of file
ezr32lg_usb_hc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
ezr32lg_usb_hc.h