WDOGEMLIB
Detailed Description
Watchdog (WDOG) Peripheral API.
This module contains functions to control the WDOG peripheral of Silicon Labs 32-bit MCUs and SoCs. The WDOG resets the system in case of a fault condition.
Data Structures |
|
| struct | WDOG_Init_TypeDef |
Macros |
|
| #define | DEFAULT_WDOG WDOG |
| #define | WDOG_INIT_DEFAULT |
Enumerations |
|
| enum |
WDOG_ClkSel_TypeDef
{
wdogClkSelULFRCO = _WDOG_CTRL_CLKSEL_ULFRCO, wdogClkSelLFRCO = _WDOG_CTRL_CLKSEL_LFRCO, wdogClkSelLFXO = _WDOG_CTRL_CLKSEL_LFXO } |
| enum |
WDOG_PeriodSel_TypeDef
{
wdogPeriod_9 = 0x0, wdogPeriod_17 = 0x1, wdogPeriod_33 = 0x2, wdogPeriod_65 = 0x3, wdogPeriod_129 = 0x4, wdogPeriod_257 = 0x5, wdogPeriod_513 = 0x6, wdogPeriod_1k = 0x7, wdogPeriod_2k = 0x8, wdogPeriod_4k = 0x9, wdogPeriod_8k = 0xA, wdogPeriod_16k = 0xB, wdogPeriod_32k = 0xC, wdogPeriod_64k = 0xD, wdogPeriod_128k = 0xE, wdogPeriod_256k = 0xF } |
Functions |
|
| __STATIC_INLINE void | WDOG_Enable (bool enable) |
|
Enable/disable the watchdog timer.
|
|
| __STATIC_INLINE void | WDOG_Feed (void) |
|
Feed the watchdog.
|
|
| __STATIC_INLINE void | WDOG_Init (const WDOG_Init_TypeDef *init) |
|
Initialize watchdog (assuming the watchdog configuration has not been locked).
|
|
| __STATIC_INLINE void | WDOG_Lock (void) |
|
Lock the watchdog configuration.
|
|
| void | WDOGn_Enable ( WDOG_TypeDef *wdog, bool enable) |
|
Enable/disable the watchdog timer.
|
|
| void | WDOGn_Feed ( WDOG_TypeDef *wdog) |
|
Feed the watchdog.
|
|
| void | WDOGn_Init ( WDOG_TypeDef *wdog, const WDOG_Init_TypeDef *init) |
|
Initialize watchdog (assuming the watchdog configuration has not been locked).
|
|
| void | WDOGn_Lock ( WDOG_TypeDef *wdog) |
|
Lock the watchdog configuration.
|
|
Macro Definition Documentation
| #define DEFAULT_WDOG WDOG |
Default WDOG instance for deprecated functions.
Definition at line
321
of file
em_wdog.h
.
Referenced by WDOG_Enable() , WDOG_Feed() , WDOG_Init() , and WDOG_Lock() .
| #define WDOG_INIT_DEFAULT |
Suggested default config for WDOG init structure.
Definition at line
180
of file
em_wdog.h
.
Enumeration Type Documentation
| enum WDOG_ClkSel_TypeDef |
Watchdog period selection.
Definition at line
67
of file
em_wdog.h
.
Function Documentation
| __STATIC_INLINE void WDOG_Enable | ( | bool |
enable
|
) |
Enable/disable the watchdog timer.
-
Deprecated: - Deprecated function. New code should use WDOGn_Enable() . This function uses DEFAULT_WDOG .
- Parameters
-
[in] enabletrue to enable watchdog, false to disable. Watchdog cannot be disabled if watchdog has been locked.
Definition at line
339
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Enable() .
| __STATIC_INLINE void WDOG_Feed | ( | void |
|
) |
Feed the watchdog.
-
Deprecated: - Deprecated function. New code should use WDOGn_Feed() . This function uses DEFAULT_WDOG .
Definition at line
352
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Feed() .
| __STATIC_INLINE void WDOG_Init | ( | const WDOG_Init_TypeDef * |
init
|
) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
-
Deprecated: - Deprecated function. New code should use Use WDOGn_Init() . This function uses DEFAULT_WDOG .
- Parameters
-
[in] initStructure holding watchdog configuration. A default setting WDOG_INIT_DEFAULT is available for init.
Definition at line
370
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Init() .
| __STATIC_INLINE void WDOG_Lock | ( | void |
|
) |
Lock the watchdog configuration.
-
Deprecated: - Deprecated function. New code should use WDOGn_Lock() . This function uses DEFAULT_WDOG .
Definition at line
383
of file
em_wdog.h
.
References DEFAULT_WDOG , and WDOGn_Lock() .
| void WDOGn_Enable | ( | WDOG_TypeDef * |
wdog,
|
| bool |
enable
|
||
| ) |
Enable/disable the watchdog timer.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdogPointer to WDOG peripheral register block. [in] enabletrue to enable watchdog, false to disable. Watchdog cannot be disabled if watchdog has been locked.
Definition at line
75
of file
em_wdog.c
.
References _WDOG_CTRL_EN_SHIFT , BUS_RegBitRead() , BUS_RegBitWrite() , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , WDOG_CTRL_LOCK , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Enable() .
| void WDOGn_Feed | ( | WDOG_TypeDef * |
wdog
|
) |
Feed the watchdog.
When the watchdog is activated, it must be fed (ie clearing the counter) before it reaches the defined timeout period. Otherwise, the watchdog will generate a reset.
- Parameters
-
[in] wdogPointer to WDOG peripheral register block.
Definition at line
109
of file
em_wdog.c
.
References WDOG_TypeDef::CMD , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , WDOG_CMD_CLEAR , WDOG_CTRL_EN , WDOG_SYNCBUSY_CMD , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Feed() .
| void WDOGn_Init | ( | WDOG_TypeDef * |
wdog,
|
| const WDOG_Init_TypeDef * |
init
|
||
| ) |
Initialize watchdog (assuming the watchdog configuration has not been locked).
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdogPointer to WDOG peripheral register block. [in] initStructure holding watchdog configuration. A default setting WDOG_INIT_DEFAULT is available for init.
Definition at line
149
of file
em_wdog.c
.
References _WDOG_CTRL_CLKSEL_SHIFT , _WDOG_CTRL_PERSEL_SHIFT , WDOG_Init_TypeDef::clkSel , WDOG_TypeDef::CTRL , WDOG_Init_TypeDef::debugRun , WDOG_Init_TypeDef::em2Run , WDOG_Init_TypeDef::em3Run , WDOG_Init_TypeDef::em4Block , WDOG_Init_TypeDef::enable , WDOG_Init_TypeDef::lock , WDOG_Init_TypeDef::perSel , WDOG_Init_TypeDef::swoscBlock , WDOG_TypeDef::SYNCBUSY , WDOG_CTRL_DEBUGRUN , WDOG_CTRL_EM2RUN , WDOG_CTRL_EM3RUN , WDOG_CTRL_EM4BLOCK , WDOG_CTRL_EN , WDOG_CTRL_LOCK , WDOG_CTRL_SWOSCBLOCK , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Init() .
| void WDOGn_Lock | ( | WDOG_TypeDef * |
wdog
|
) |
Lock the watchdog configuration.
This prevents errors from overwriting the watchdog configuration, possibly disabling it. Only a reset can unlock the watchdog config, once locked.
If the LFRCO or LFXO clocks are used to clock the watchdog, one should consider using the option of inhibiting those clocks to be disabled, please see the WDOG_Enable() init structure.
- Note
- This function modifies the WDOG CTRL register which requires synchronization into the low frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed.
- Parameters
-
[in] wdogPointer to WDOG peripheral register block.
Definition at line
223
of file
em_wdog.c
.
References _WDOG_CTRL_LOCK_SHIFT , BUS_RegBitWrite() , WDOG_TypeDef::CTRL , WDOG_TypeDef::SYNCBUSY , and WDOG_SYNCBUSY_CTRL .
Referenced by WDOG_Lock() .