USB Status FlagsPlatform Middleware > USBXpress

Detailed Description

These constant values are returned by USBX_blockRead() and USBX_blockWrite() .

Macros

#define USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED
Failed because the device is not configured.
#define USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY
Failed because the endpoint is busy.
#define USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED
Failed because the endpoint is stalled.
#define USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL
Failed due to an illegal parameter.
#define USBX_STATUS_OK USB_STATUS_OK
Success.