LESENSE_DecStCond_TypeDef Struct ReferenceEMLIB > LESENSE

Decoder state condition descriptor structure.

Definition at line 1022 of file em_lesense.h.

#include <em_lesense.h>

Data Fields

uint8_t compMask
 
uint8_t compVal
 
uint8_t nextState
 
LESENSE_StTransAct_TypeDef prsAct
 
bool setInt
 

Field Documentation

uint8_t LESENSE_DecStCond_TypeDef::compMask

Configure compare mask. Set bit X to exclude sensor X from evaluation. Note: decoder can handle sensor inputs from up to 4 sensors, therefore this mask is 4 bit long.

Definition at line 1030 of file em_lesense.h.

Referenced by LESENSE_DecoderStateConfig().

uint8_t LESENSE_DecStCond_TypeDef::compVal

Configure compare value. State transition is triggered when sensor state equals to this value. Valid range: 0-15 (4 bits).

Definition at line 1025 of file em_lesense.h.

Referenced by LESENSE_DecoderStateConfig().

uint8_t LESENSE_DecStCond_TypeDef::nextState

Configure index of state to be entered if the sensor state equals to compVal. Valid range: 0-15 (4 bits).

Definition at line 1034 of file em_lesense.h.

Referenced by LESENSE_DecoderStateConfig().

LESENSE_StTransAct_TypeDef LESENSE_DecStCond_TypeDef::prsAct

Configure which PRS action to perform when sensor state equals to compVal.

Definition at line 1038 of file em_lesense.h.

Referenced by LESENSE_DecoderStateConfig().

bool LESENSE_DecStCond_TypeDef::setInt

If enabled, interrupt flag is set when sensor state equals to compVal.

Definition at line 1041 of file em_lesense.h.

Referenced by LESENSE_DecoderStateConfig().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_lesense.h