ADC_InitScanInput_TypeDef Struct ReferenceEMLIB > ADC
Scan input configuration
       Definition at line
       
        850
       
       of file
       
        em_adc.h
       
       .
      
      
       #include <
       
     
        em_adc.h
       
       >
      
         Data Fields | 
       |
| uint32_t | scanInputEn | 
| uint32_t | scanInputSel | 
| uint32_t | scanNegSel | 
Field Documentation
| uint32_t ADC_InitScanInput_TypeDef::scanInputEn | 
Input enable mask
        Definition at line
        
         855
        
        of file
        
         em_adc.h
        
        .
       
| uint32_t ADC_InitScanInput_TypeDef::scanInputSel | 
Input range select to be applied to ADC_SCANINPUTSEL.
        Definition at line
        
         852
        
        of file
        
         em_adc.h
        
        .
       
| uint32_t ADC_InitScanInput_TypeDef::scanNegSel | 
Alternative negative input
        Definition at line
        
         858
        
        of file
        
         em_adc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_adc.h