USB_TypeDef Struct ReferenceDevices > EZR32LG_USB

Definition at line 48 of file ezr32lg_usb.h .

Data Fields

__IOM uint32_t CTRL
__IM uint32_t DAINT
__IOM uint32_t DAINTMSK
__IOM uint32_t DCFG
__IOM uint32_t DCTL
USB_DIEP_TypeDef DIEP [6]
__IOM uint32_t DIEP0CTL
__IOM uint32_t DIEP0DMAADDR
__IOM uint32_t DIEP0INT
__IOM uint32_t DIEP0TSIZ
__IM uint32_t DIEP0TXFSTS
__IOM uint32_t DIEPEMPMSK
__IOM uint32_t DIEPMSK
__IOM uint32_t DIEPTXF1
__IOM uint32_t DIEPTXF2
__IOM uint32_t DIEPTXF3
__IOM uint32_t DIEPTXF4
__IOM uint32_t DIEPTXF5
__IOM uint32_t DIEPTXF6
USB_DOEP_TypeDef DOEP [6]
__IOM uint32_t DOEP0CTL
__IOM uint32_t DOEP0DMAADDR
__IOM uint32_t DOEP0INT
__IOM uint32_t DOEP0TSIZ
__IOM uint32_t DOEPMSK
__IM uint32_t DSTS
__IOM uint32_t DVBUSDIS
__IOM uint32_t DVBUSPULSE
__IOM uint32_t FIFO0D [512]
__IOM uint32_t FIFO10D [512]
__IOM uint32_t FIFO11D [512]
__IOM uint32_t FIFO12D [512]
__IOM uint32_t FIFO13D [512]
__IOM uint32_t FIFO1D [512]
__IOM uint32_t FIFO2D [512]
__IOM uint32_t FIFO3D [512]
__IOM uint32_t FIFO4D [512]
__IOM uint32_t FIFO5D [512]
__IOM uint32_t FIFO6D [512]
__IOM uint32_t FIFO7D [512]
__IOM uint32_t FIFO8D [512]
__IOM uint32_t FIFO9D [512]
__IOM uint32_t FIFORAM [512]
__IOM uint32_t GAHBCFG
__IOM uint32_t GDFIFOCFG
__IOM uint32_t GINTMSK
__IOM uint32_t GINTSTS
__IOM uint32_t GNPTXFSIZ
__IM uint32_t GNPTXSTS
__IOM uint32_t GOTGCTL
__IOM uint32_t GOTGINT
__IOM uint32_t GRSTCTL
__IOM uint32_t GRXFSIZ
__IM uint32_t GRXSTSP
__IM uint32_t GRXSTSR
__IOM uint32_t GUSBCFG
__IM uint32_t HAINT
__IOM uint32_t HAINTMSK
USB_HC_TypeDef HC [14]
__IOM uint32_t HCFG
__IOM uint32_t HFIR
__IM uint32_t HFNUM
__IOM uint32_t HPRT
__IOM uint32_t HPTXFSIZ
__IM uint32_t HPTXSTS
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t PCGCCTL
uint32_t RESERVED0 [61433]
uint32_t RESERVED1 [11]
uint32_t RESERVED10 [1]
uint32_t RESERVED11 [50]
uint32_t RESERVED12 [1]
uint32_t RESERVED13 [1]
uint32_t RESERVED14 [1]
uint32_t RESERVED15 [72]
uint32_t RESERVED16 [1]
uint32_t RESERVED17 [1]
uint32_t RESERVED18 [2]
uint32_t RESERVED19 [136]
uint32_t RESERVED2 [40]
uint32_t RESERVED20 [127]
uint32_t RESERVED21 [512]
uint32_t RESERVED22 [512]
uint32_t RESERVED23 [512]
uint32_t RESERVED24 [512]
uint32_t RESERVED25 [512]
uint32_t RESERVED26 [512]
uint32_t RESERVED27 [512]
uint32_t RESERVED28 [512]
uint32_t RESERVED29 [512]
uint32_t RESERVED3 [185]
uint32_t RESERVED30 [512]
uint32_t RESERVED31 [512]
uint32_t RESERVED32 [512]
uint32_t RESERVED33 [512]
uint32_t RESERVED34 [17920]
uint32_t RESERVED4 [1]
uint32_t RESERVED5 [9]
uint32_t RESERVED6 [47]
uint32_t RESERVED7 [80]
uint32_t RESERVED8 [1]
uint32_t RESERVED9 [2]
__IOM uint32_t ROUTE
__IM uint32_t STATUS

Field Documentation

__IOM uint32_t USB_TypeDef::CTRL

System Control Register

Definition at line 49 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::DAINT

Device All Endpoints Interrupt Register

Definition at line 103 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DAINTMSK

Device All Endpoints Interrupt Mask Register

Definition at line 104 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DCFG

Device Configuration Register

Definition at line 97 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DCTL

Device Control Register

Definition at line 98 of file ezr32lg_usb.h .

USB_DIEP_TypeDef USB_TypeDef::DIEP[6]

Device IN Endpoint x+1 Registers

Definition at line 122 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEP0CTL

Device IN Endpoint 0 Control Register

Definition at line 113 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEP0DMAADDR

Device IN Endpoint 0 DMA Address Register

Definition at line 118 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEP0INT

Device IN Endpoint 0 Interrupt Register

Definition at line 115 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEP0TSIZ

Device IN Endpoint 0 Transfer Size Register

Definition at line 117 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::DIEP0TXFSTS

Device IN Endpoint 0 Transmit FIFO Status Register

Definition at line 119 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPEMPMSK

Device IN Endpoint FIFO Empty Interrupt Mask Register

Definition at line 110 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPMSK

Device IN Endpoint Common Interrupt Mask Register

Definition at line 101 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF1

Device IN Endpoint Transmit FIFO 1 Size Register

Definition at line 75 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF2

Device IN Endpoint Transmit FIFO 2 Size Register

Definition at line 76 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF3

Device IN Endpoint Transmit FIFO 3 Size Register

Definition at line 77 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF4

Device IN Endpoint Transmit FIFO 4 Size Register

Definition at line 78 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF5

Device IN Endpoint Transmit FIFO 5 Size Register

Definition at line 79 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DIEPTXF6

Device IN Endpoint Transmit FIFO 6 Size Register

Definition at line 80 of file ezr32lg_usb.h .

USB_DOEP_TypeDef USB_TypeDef::DOEP[6]

Device OUT Endpoint x+1 Registers

Definition at line 133 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DOEP0CTL

Device OUT Endpoint 0 Control Register

Definition at line 125 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DOEP0DMAADDR

Device OUT Endpoint 0 DMA Address Register

Definition at line 130 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DOEP0INT

Device OUT Endpoint 0 Interrupt Register

Definition at line 127 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DOEP0TSIZ

Device OUT Endpoint 0 Transfer Size Register

Definition at line 129 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DOEPMSK

Device OUT Endpoint Common Interrupt Mask Register

Definition at line 102 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::DSTS

Device Status Register

Definition at line 99 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DVBUSDIS

Device VBUS Discharge Time Register

Definition at line 106 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::DVBUSPULSE

Device VBUS Pulsing Time Register

Definition at line 107 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO0D[512]

Device EP 0/Host Channel 0 FIFO

Definition at line 139 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO10D[512]

Host Channel 10 FIFO

Definition at line 169 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO11D[512]

Host Channel 11 FIFO

Definition at line 172 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO12D[512]

Host Channel 12 FIFO

Definition at line 175 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO13D[512]

Host Channel 13 FIFO

Definition at line 178 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO1D[512]

Device EP 1/Host Channel 1 FIFO

Definition at line 142 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO2D[512]

Device EP 2/Host Channel 2 FIFO

Definition at line 145 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO3D[512]

Device EP 3/Host Channel 3 FIFO

Definition at line 148 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO4D[512]

Device EP 4/Host Channel 4 FIFO

Definition at line 151 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO5D[512]

Device EP 5/Host Channel 5 FIFO

Definition at line 154 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO6D[512]

Device EP 6/Host Channel 6 FIFO

Definition at line 157 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO7D[512]

Host Channel 7 FIFO

Definition at line 160 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO8D[512]

Host Channel 8 FIFO

Definition at line 163 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFO9D[512]

Host Channel 9 FIFO

Definition at line 166 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::FIFORAM[512]

Direct Access to Data FIFO RAM for Debugging (2 KB)

Definition at line 181 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GAHBCFG

AHB Configuration Register

Definition at line 60 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GDFIFOCFG

Global DFIFO Configuration Register

Definition at line 71 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GINTMSK

Interrupt Mask Register

Definition at line 64 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GINTSTS

Interrupt Register

Definition at line 63 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GNPTXFSIZ

Non-periodic Transmit FIFO Size Register

Definition at line 68 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::GNPTXSTS

Non-periodic Transmit FIFO/Queue Status Register

Definition at line 69 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GOTGCTL

OTG Control and Status Register

Definition at line 58 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GOTGINT

OTG Interrupt Register

Definition at line 59 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GRSTCTL

Reset Register

Definition at line 62 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GRXFSIZ

Receive FIFO Size Register

Definition at line 67 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::GRXSTSP

Receive Status Read and Pop Register

Definition at line 66 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::GRXSTSR

Receive Status Debug Read Register

Definition at line 65 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::GUSBCFG

USB Configuration Register

Definition at line 61 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::HAINT

Host All Channels Interrupt Register

Definition at line 88 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::HAINTMSK

Host All Channels Interrupt Mask Register

Definition at line 89 of file ezr32lg_usb.h .

USB_HC_TypeDef USB_TypeDef::HC[14]

Host Channel Registers

Definition at line 94 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::HCFG

Host Configuration Register

Definition at line 83 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::HFIR

Host Frame Interval Register

Definition at line 84 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::HFNUM

Host Frame Number/Frame Time Remaining Register

Definition at line 85 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::HPRT

Host Port Control and Status Register

Definition at line 91 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::HPTXFSIZ

Host Periodic Transmit FIFO Size Register

Definition at line 74 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::HPTXSTS

Host Periodic Transmit FIFO/Queue Status Register

Definition at line 87 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::IF

Interrupt Flag Register

Definition at line 51 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 53 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 52 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::PCGCCTL

Power and Clock Gating Control Register

Definition at line 136 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED0[61433]

Reserved for future use

Definition at line 57 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED1[11]

Reserved for future use

Definition at line 70 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED10[1]

Reserved for future use

Definition at line 109 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED11[50]

Reserved for future use

Definition at line 112 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED12[1]

Reserved for future use

Definition at line 114 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED13[1]

Reserved for future use

Definition at line 116 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED14[1]

Reserved registers

Definition at line 121 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED15[72]

Reserved for future use

Definition at line 124 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED16[1]

Reserved for future use

Definition at line 126 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED17[1]

Reserved for future use

Definition at line 128 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED18[2]

Reserved registers

Definition at line 132 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED19[136]

Reserved for future use

Definition at line 135 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED2[40]

Reserved for future use

Definition at line 73 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED20[127]

Reserved registers

Definition at line 138 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED21[512]

Reserved registers

Definition at line 141 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED22[512]

Reserved registers

Definition at line 144 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED23[512]

Reserved registers

Definition at line 147 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED24[512]

Reserved registers

Definition at line 150 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED25[512]

Reserved registers

Definition at line 153 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED26[512]

Reserved registers

Definition at line 156 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED27[512]

Reserved registers

Definition at line 159 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED28[512]

Reserved registers

Definition at line 162 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED29[512]

Reserved registers

Definition at line 165 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED3[185]

Reserved for future use

Definition at line 82 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED30[512]

Reserved registers

Definition at line 168 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED31[512]

Reserved registers

Definition at line 171 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED32[512]

Reserved registers

Definition at line 174 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED33[512]

Reserved registers

Definition at line 177 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED34[17920]

Reserved registers

Definition at line 180 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED4[1]

Reserved for future use

Definition at line 86 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED5[9]

Reserved for future use

Definition at line 90 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED6[47]

Reserved registers

Definition at line 93 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED7[80]

Reserved for future use

Definition at line 96 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED8[1]

Reserved for future use

Definition at line 100 of file ezr32lg_usb.h .

uint32_t USB_TypeDef::RESERVED9[2]

Reserved for future use

Definition at line 105 of file ezr32lg_usb.h .

__IOM uint32_t USB_TypeDef::ROUTE

I/O Routing Register

Definition at line 55 of file ezr32lg_usb.h .

__IM uint32_t USB_TypeDef::STATUS

System Status Register

Definition at line 50 of file ezr32lg_usb.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/ ezr32lg_usb.h