OPAMPEMLIB
Detailed Description
Operational Amplifier (OPAMP) peripheral API.
This module contains functions to:
- OPAMP_Enable() Configure and enable OPAMP.
- OPAMP_Disable() Disable OPAMP.
All OPAMP functions assume that the DAC clock is running. If DAC is not used, the clock can be turned off when OPAMPs are configured.
If the available gain values don't suit the application at hand, the resistor ladders can be disabled and external gain programming resistors used.
A number of predefined OPAMP setup macros are available for configuration of the most common OPAMP topologies (see figures below).
- Note
- The terms POSPAD and NEGPAD in the figures are used to indicate that these pads should be connected to a suitable signal ground.
Unity gain voltage follower.
Use predefined macros OPA_INIT_UNITY_GAIN and OPA_INIT_UNITY_GAIN_OPA2.
|\ ___________|+\ | \_______ ___|_ / | | | / | | |/ | |___________|
Non-inverting amplifier.
Use predefined macros OPA_INIT_NON_INVERTING and OPA_INIT_NON_INVERTING_OPA2.
|\ ___________|+\ | \_______ ___|_ / | | | / | | |/ | |_____R2____| | R1 | NEGPAD
Inverting amplifier.
Use predefined macros OPA_INIT_INVERTING and OPA_INIT_INVERTING_OPA2.
_____R2____ | | | |\ | ____R1_|___|_\ | | \____|___ ___| / | |+/ | |/ | POSPAD
Cascaded non-inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_NON_INVERTING_OPA0, OPA_INIT_CASCADED_NON_INVERTING_OPA1 and OPA_INIT_CASCADED_NON_INVERTING_OPA2.
|\ |\ |\ ___________|+\ OPA0 ___________|+\ OPA1 ___________|+\ OPA2 | \_________| | \_________| | \_______ ___|_ / | ___|_ / | ___|_ / | | | / | | | / | | | / | | |/ | | |/ | | |/ | |_____R2____| |_____R2____| |_____R2____| | | | R1 R1 R1 | | | NEGPAD NEGPAD NEGPAD
Cascaded inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_INVERTING_OPA0, OPA_INIT_CASCADED_INVERTING_OPA1 and OPA_INIT_CASCADED_INVERTING_OPA2.
_____R2____ _____R2____ _____R2____ | | | | | | | |\ | | |\ | | |\ | ____R1_|___|_\ | ____R1_|___|_\ | ____R1_|___|_\ | | \____|____| | \____|___| | \____|__ ___| / ___| / ___| / | |+/ OPA0 | |+/ OPA1 | |+/ OPA2 | |/ | |/ | |/ | | | POSPAD POSPAD POSPAD
Differential driver with two opamp's.
Use predefined macros OPA_INIT_DIFF_DRIVER_OPA0 and OPA_INIT_DIFF_DRIVER_OPA1.
__________________________ | + | _____R2____ |\ | | | ___________|+\ OPA0 | | |\ OPA1 | | \_________|____R1_|___|_\ | _ ___|_ / | | \____|______ | | / | ___| / | |/ | | |+/ |________________| | |/ | POSPAD
Differential receiver with three opamp's.
Use predefined macros OPA_INIT_DIFF_RECEIVER_OPA0, OPA_INIT_DIFF_RECEIVER_OPA1 and OPA_INIT_DIFF_RECEIVER_OPA2.
|\ __________|+\ OPA1 _ | \_________ ___|_ / | | _____R2____ | | / | | | | | |/ | | | |\ | |___________| |____R1_|___|_\ | | \____|___ |\ ____R1_ ___| / +__________|+\ OPA0 | | |+/ OPA2 | \_________| | |/ ___|_ / | R2 | | / | | | |/ | NEGPAD OPA0 |___________|
Data Structures | |
struct | OPAMP_Init_TypeDef |
Macros | |
#define | OPA_INIT_CASCADED_INVERTING_OPA0 |
#define | OPA_INIT_CASCADED_INVERTING_OPA1 |
#define | OPA_INIT_CASCADED_INVERTING_OPA2 |
#define | OPA_INIT_CASCADED_NON_INVERTING_OPA0 |
#define | OPA_INIT_CASCADED_NON_INVERTING_OPA1 |
#define | OPA_INIT_CASCADED_NON_INVERTING_OPA2 |
#define | OPA_INIT_DIFF_DRIVER_OPA0 |
#define | OPA_INIT_DIFF_DRIVER_OPA1 |
#define | OPA_INIT_DIFF_RECEIVER_OPA0 |
#define | OPA_INIT_DIFF_RECEIVER_OPA1 |
#define | OPA_INIT_DIFF_RECEIVER_OPA2 |
#define | OPA_INIT_INVERTING |
#define | OPA_INIT_INVERTING_OPA2 |
#define | OPA_INIT_NON_INVERTING |
#define | OPA_INIT_NON_INVERTING_OPA2 |
#define | OPA_INIT_UNITY_GAIN |
#define | OPA_INIT_UNITY_GAIN_OPA2 |
Enumerations | |
enum | OPAMP_NegSel_TypeDef { opaNegSelDisable = DAC_OPA0MUX_NEGSEL_DISABLE, opaNegSelUnityGain = DAC_OPA0MUX_NEGSEL_UG, opaNegSelResTap = DAC_OPA0MUX_NEGSEL_OPATAP, opaNegSelNegPad = DAC_OPA0MUX_NEGSEL_NEGPAD } |
enum | OPAMP_OutMode_TypeDef { opaOutModeDisable = DAC_OPA0MUX_OUTMODE_DISABLE, opaOutModeMain = DAC_OPA0MUX_OUTMODE_MAIN, opaOutModeAlt = DAC_OPA0MUX_OUTMODE_ALT, opaOutModeAll = DAC_OPA0MUX_OUTMODE_ALL } |
enum | OPAMP_PosSel_TypeDef { opaPosSelDisable = DAC_OPA0MUX_POSSEL_DISABLE, opaPosSelDac = DAC_OPA0MUX_POSSEL_DAC, opaPosSelPosPad = DAC_OPA0MUX_POSSEL_POSPAD, opaPosSelOpaIn = DAC_OPA0MUX_POSSEL_OPA0INP, opaPosSelResTapOpa0 = DAC_OPA0MUX_POSSEL_OPATAP } |
enum | OPAMP_ResInMux_TypeDef { opaResInMuxDisable = DAC_OPA0MUX_RESINMUX_DISABLE, opaResInMuxOpaIn = DAC_OPA0MUX_RESINMUX_OPA0INP, opaResInMuxNegPad = DAC_OPA0MUX_RESINMUX_NEGPAD, opaResInMuxPosPad = DAC_OPA0MUX_RESINMUX_POSPAD, opaResInMuxVss = DAC_OPA0MUX_RESINMUX_VSS } |
enum | OPAMP_ResSel_TypeDef { opaResSelDefault = DAC_OPA0MUX_RESSEL_DEFAULT, opaResSelR2eq0_33R1 = DAC_OPA0MUX_RESSEL_RES0, opaResSelR2eqR1 = DAC_OPA0MUX_RESSEL_RES1, opaResSelR1eq1_67R1 = DAC_OPA0MUX_RESSEL_RES2, opaResSelR2eq2R1 = DAC_OPA0MUX_RESSEL_RES3, opaResSelR2eq3R1 = DAC_OPA0MUX_RESSEL_RES4, opaResSelR2eq4_33R1 = DAC_OPA0MUX_RESSEL_RES5, opaResSelR2eq7R1 = DAC_OPA0MUX_RESSEL_RES6, opaResSelR2eq15R1 = DAC_OPA0MUX_RESSEL_RES7 } |
enum | OPAMP_TypeDef { OPA0 = 0, OPA1 = 1, OPA2 = 2 } |
Functions | |
void | OPAMP_Disable (DAC_TypeDef *dac, OPAMP_TypeDef opa) |
Disable an Operational Amplifier. | |
void | OPAMP_Enable (DAC_TypeDef *dac, OPAMP_TypeDef opa, const OPAMP_Init_TypeDef *init) |
Configure and enable an Operational Amplifier. | |
Macro Definition Documentation
#define OPA_INIT_CASCADED_INVERTING_OPA0 |
Configuration of OPA0 in cascaded inverting amplifier mode.
Definition at line 729
of file em_opamp.h
.
#define OPA_INIT_CASCADED_INVERTING_OPA1 |
Configuration of OPA1 in cascaded inverting amplifier mode.
Definition at line 751
of file em_opamp.h
.
#define OPA_INIT_CASCADED_INVERTING_OPA2 |
Configuration of OPA2 in cascaded inverting amplifier mode.
Definition at line 773
of file em_opamp.h
.
#define OPA_INIT_CASCADED_NON_INVERTING_OPA0 |
Configuration of OPA0 in cascaded non-inverting amplifier mode.
Definition at line 663
of file em_opamp.h
.
#define OPA_INIT_CASCADED_NON_INVERTING_OPA1 |
Configuration of OPA1 in cascaded non-inverting amplifier mode.
Definition at line 685
of file em_opamp.h
.
#define OPA_INIT_CASCADED_NON_INVERTING_OPA2 |
Configuration of OPA2 in cascaded non-inverting amplifier mode.
Definition at line 707
of file em_opamp.h
.
#define OPA_INIT_DIFF_DRIVER_OPA0 |
Configuration of OPA0 in two-opamp differential driver mode.
Definition at line 795
of file em_opamp.h
.
#define OPA_INIT_DIFF_DRIVER_OPA1 |
Configuration of OPA1 in two-opamp differential driver mode.
Definition at line 817
of file em_opamp.h
.
#define OPA_INIT_DIFF_RECEIVER_OPA0 |
Configuration of OPA0 in three-opamp differential receiver mode.
Definition at line 839
of file em_opamp.h
.
#define OPA_INIT_DIFF_RECEIVER_OPA1 |
Configuration of OPA1 in three-opamp differential receiver mode.
Definition at line 861
of file em_opamp.h
.
#define OPA_INIT_DIFF_RECEIVER_OPA2 |
Configuration of OPA2 in three-opamp differential receiver mode.
Definition at line 883
of file em_opamp.h
.
#define OPA_INIT_INVERTING |
Configuration of OPA0/1 in inverting amplifier mode.
Definition at line 619
of file em_opamp.h
.
#define OPA_INIT_INVERTING_OPA2 |
Configuration of OPA2 in inverting amplifier mode.
Definition at line 641
of file em_opamp.h
.
#define OPA_INIT_NON_INVERTING |
Configuration of OPA0/1 in non-inverting amplifier mode.
Definition at line 575
of file em_opamp.h
.
#define OPA_INIT_NON_INVERTING_OPA2 |
Configuration of OPA2 in non-inverting amplifier mode.
Definition at line 597
of file em_opamp.h
.
#define OPA_INIT_UNITY_GAIN |
Configuration of OPA0/1 in unity gain voltage follower mode.
Definition at line 531
of file em_opamp.h
.
#define OPA_INIT_UNITY_GAIN_OPA2 |
Configuration of OPA2 in unity gain voltage follower mode.
Definition at line 553
of file em_opamp.h
.
Enumeration Type Documentation
enum OPAMP_NegSel_TypeDef |
enum OPAMP_PosSel_TypeDef |
OPAMP positive terminal input selection values.
Definition at line 181
of file em_opamp.h
.
OPAMP resistor ladder input selector values.
Definition at line 366
of file em_opamp.h
.
enum OPAMP_ResSel_TypeDef |
OPAMP gain values.
Definition at line 341
of file em_opamp.h
.
enum OPAMP_TypeDef |
Function Documentation
void OPAMP_Disable | ( | DAC_TypeDef * | dac, |
OPAMP_TypeDef | opa |
||
) |
Disable an Operational Amplifier.
- Parameters
-
[in] dac
A pointer to the DAC peripheral register block. [in] opa
Selects an OPA, valid values are OPA0, OPA1, and OPA2.
Definition at line 259
of file em_opamp.c
.
References DAC_CH0CTRL_EN, DAC_CH1CTRL_EN, DAC_OPACTRL_OPA0EN, DAC_OPACTRL_OPA1EN, DAC_OPACTRL_OPA2EN, OPA0, OPA1, and OPA2.
Referenced by OPAMP_Enable().
void OPAMP_Enable | ( | DAC_TypeDef * | dac, |
OPAMP_TypeDef | opa, |
||
const OPAMP_Init_TypeDef * | init |
||
) |
Configure and enable an Operational Amplifier.
- Note
- The value of the alternate output enable bit mask in the OPAMP_Init_TypeDef structure should consist of one or more of the DAC_OPA[opa#]MUX_OUTPEN_OUT[output#] flags (defined in <part_name>_dac.h) OR'ed together.
For OPA0:- DAC_OPA0MUX_OUTPEN_OUT0
- DAC_OPA0MUX_OUTPEN_OUT1
- DAC_OPA0MUX_OUTPEN_OUT2
- DAC_OPA0MUX_OUTPEN_OUT3
- DAC_OPA0MUX_OUTPEN_OUT4
- DAC_OPA1MUX_OUTPEN_OUT0
- DAC_OPA1MUX_OUTPEN_OUT1
- DAC_OPA1MUX_OUTPEN_OUT2
- DAC_OPA1MUX_OUTPEN_OUT3
- DAC_OPA1MUX_OUTPEN_OUT4
- DAC_OPA2MUX_OUTPEN_OUT0
- DAC_OPA2MUX_OUTPEN_OUT1
init.outPen = DAC_OPA0MUX_OUTPEN_OUT0 | DAC_OPA0MUX_OUTPEN_OUT4;
- Parameters
-
[in] dac
A pointer to the DAC peripheral register block. [in] opa
Selects an OPA, valid values are OPA0, OPA1, and OPA2. [in] init
A pointer to a structure containing OPAMP initialization information.
Definition at line 370
of file em_opamp.c
.
References _DAC_BIASPROG_BIASPROG_MASK, _DAC_BIASPROG_BIASPROG_SHIFT, _DAC_BIASPROG_OPA2BIASPROG_MASK, _DAC_BIASPROG_OPA2BIASPROG_SHIFT, _DAC_CAL_CH0OFFSET_MASK, _DAC_CAL_CH0OFFSET_SHIFT, _DAC_CAL_CH1OFFSET_MASK, _DAC_CAL_CH1OFFSET_SHIFT, _DAC_CAL_GAIN_MASK, _DAC_OPA0MUX_OUTPEN_MASK, _DAC_OPA1MUX_OUTPEN_MASK, _DAC_OPA2MUX_OUTPEN_MASK, _DAC_OPACTRL_OPA0LPFDIS_MASK, _DAC_OPACTRL_OPA1LPFDIS_MASK, _DAC_OPACTRL_OPA2LPFDIS_MASK, _DAC_OPAOFFSET_OPA2OFFSET_MASK, _DAC_OPAOFFSET_OPA2OFFSET_SHIFT, OPAMP_Init_TypeDef::bias, DAC_BIASPROG_HALFBIAS, DAC_BIASPROG_OPA2HALFBIAS, DAC_CH0CTRL_EN, DAC_CH1CTRL_EN, DAC_OPA0MUX_NEXTOUT, DAC_OPA0MUX_NPEN, DAC_OPA0MUX_PPEN, DAC_OPA1MUX_NEXTOUT, DAC_OPA1MUX_NPEN, DAC_OPA1MUX_PPEN, DAC_OPA2MUX_NEXTOUT, DAC_OPA2MUX_NPEN, DAC_OPA2MUX_OUTMODE, DAC_OPA2MUX_POSSEL_DISABLE, DAC_OPA2MUX_POSSEL_OPA1INP, DAC_OPA2MUX_POSSEL_OPATAP, DAC_OPA2MUX_POSSEL_POSPAD, DAC_OPA2MUX_PPEN, DAC_OPACTRL_OPA0EN, DAC_OPACTRL_OPA0HCMDIS, DAC_OPACTRL_OPA0LPFDIS_NLPFDIS, DAC_OPACTRL_OPA0LPFDIS_PLPFDIS, DAC_OPACTRL_OPA0SHORT, DAC_OPACTRL_OPA1EN, DAC_OPACTRL_OPA1HCMDIS, DAC_OPACTRL_OPA1LPFDIS_NLPFDIS, DAC_OPACTRL_OPA1LPFDIS_PLPFDIS, DAC_OPACTRL_OPA1SHORT, DAC_OPACTRL_OPA2EN, DAC_OPACTRL_OPA2HCMDIS, DAC_OPACTRL_OPA2LPFDIS_NLPFDIS, DAC_OPACTRL_OPA2LPFDIS_PLPFDIS, DAC_OPACTRL_OPA2SHORT, OPAMP_Init_TypeDef::defaultOffset, DEVINFO, OPAMP_Init_TypeDef::halfBias, OPAMP_Init_TypeDef::hcmDisable, OPAMP_Init_TypeDef::lpfNegPadDisable, OPAMP_Init_TypeDef::lpfPosPadDisable, OPAMP_Init_TypeDef::negSel, OPAMP_Init_TypeDef::nextOut, OPAMP_Init_TypeDef::npEn, OPAMP_Init_TypeDef::offset, OPA0, OPA1, OPA2, OPAMP_Disable(), opaNegSelResTap, OPAMP_Init_TypeDef::outMode, OPAMP_Init_TypeDef::outPen, OPAMP_Init_TypeDef::posSel, OPAMP_Init_TypeDef::ppEn, OPAMP_Init_TypeDef::resInMux, OPAMP_Init_TypeDef::resSel, OPAMP_Init_TypeDef::shortInputs, and SYSTEM_GetCalibrationValue().