LESENSE_DecStAll_TypeDef Struct ReferenceEMLIB > LESENSE

Configuration structure for decoder.

Definition at line 1068 of file em_lesense.h.

#include <em_lesense.h>

Data Fields

LESENSE_DecStDesc_TypeDef St [LESENSE_NUM_DECODER_STATES]
 

Field Documentation

Descriptor of the 16 or 32 decoder states depending on the device.

Definition at line 1070 of file em_lesense.h.

Referenced by LESENSE_DecoderStateAllConfig().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/em_lesense.h