USB_COMMONPlatform Middleware > USB
Detailed Description
Common parts for both HOST and DEVICE USB stacks, see USB device stack library and USB host stack library pages for device and host library documentation.
Data Structures | |
struct | USB_ConfigurationDescriptor_TypeDef |
USB Configuration Descriptor. | |
struct | USB_DeviceDescriptor_TypeDef |
USB Device Descriptor. | |
struct | USB_EndpointDescriptor_TypeDef |
USB Endpoint Descriptor. | |
struct | USB_InterfaceDescriptor_TypeDef |
USB Interface Descriptor. | |
struct | USB_Setup_TypeDef |
USB Setup request package. | |
struct | USB_StringDescriptor_TypeDef |
USB String Descriptor. | |
Typedefs | |
typedef unsigned short | char16_t |
typedef int(* | USB_XferCompleteCb_TypeDef) (USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining) |
USB transfer callback function. | |
typedef void(* | USBTIMER_Callback_TypeDef) (void) |
USBTIMER callback function. | |
Enumerations | |
enum | USB_Status_TypeDef { USB_STATUS_OK = 0, USB_STATUS_REQ_ERR = -1, USB_STATUS_EP_BUSY = -2, USB_STATUS_REQ_UNHANDLED = -3, USB_STATUS_ILLEGAL = -4, USB_STATUS_EP_STALLED = -5, USB_STATUS_EP_ABORTED = -6, USB_STATUS_EP_ERROR = -7, USB_STATUS_EP_NAK = -8, USB_STATUS_DEVICE_UNCONFIGURED = -9, USB_STATUS_DEVICE_SUSPENDED = -10, USB_STATUS_DEVICE_RESET = -11, USB_STATUS_TIMEOUT = -12, USB_STATUS_DEVICE_REMOVED = -13, USB_STATUS_HC_BUSY = -14, USB_STATUS_DEVICE_MALFUNCTION = -15, USB_STATUS_PORT_OVERCURRENT = -16 } |
USB transfer status enumerator. | |
Functions | |
char * | USB_GetErrorMsgString (int error) |
Return an error message string for a given error code. | |
void | USB_PrintErrorMsgString (char *pre, int error) |
Format and print a text string given an error code, prepends an optional user supplied leader string. | |
int | USB_PRINTF (const char *format,...) |
Transmit "printf" formated data on the debug serial port. | |
int | USB_PUTCHAR (char c) |
Transmit a single char on the debug serial port. | |
void | USB_PUTS (const char *p) |
Transmit a zero terminated string on the debug serial port. | |
void | USBTIMER_DelayMs (uint32_t msec) |
Active wait millisecond delay function. Can also be used inside interrupt handlers. | |
void | USBTIMER_DelayUs (uint32_t usec) |
Active wait microsecond delay function. Can also be used inside interrupt handlers. | |
void | USBTIMER_Init (void) |
Activate the hardware timer used to pace the 1 millisecond timer system. | |
void | USBTIMER_Start (uint32_t id, uint32_t timeout, USBTIMER_Callback_TypeDef callback) |
Start a timer. | |
void | USBTIMER_Stop (uint32_t id) |
Stop a timer. | |
Macro Definition Documentation
#define CLEAR_FEATURE 1 |
Standard setup request CLEAR_FEATURE.
Definition at line 90
of file em_usb.h
.
Referenced by MSDD_SetupCmd(), and USBH_UnStallEpB().
#define CONFIG_DESC_BM_REMOTEWAKEUP 0x20 |
Configuration descriptor attribute macro.
Definition at line 193
of file em_usb.h
.
#define CONFIG_DESC_BM_RESERVED_D7 0x80 |
Configuration descriptor attribute macro.
Definition at line 195
of file em_usb.h
.
#define CONFIG_DESC_BM_SELFPOWERED 0x40 |
Configuration descriptor attribute macro.
Definition at line 194
of file em_usb.h
.
#define CONFIG_DESC_BM_TRANSFERTYPE 0x03 |
Configuration descriptor transfer type bitmask.
Definition at line 196
of file em_usb.h
.
Referenced by USBD_Init(), and USBH_AssignHostChannel().
#define CONFIG_DESC_MAXPOWER_mA | ( | x | ) | (((x) + 1) / 2) |
Configuration descriptor power macro.
Definition at line 197
of file em_usb.h
.
#define DEVICE_IS_SELFPOWERED 0x0001 |
Standard request GET_STATUS bitmask.
Definition at line 199
of file em_usb.h
.
#define GET_CONFIGURATION 8 |
Standard setup request GET_CONFIGURATION.
Definition at line 95
of file em_usb.h
.
#define GET_DESCRIPTOR 6 |
Standard setup request GET_DESCRIPTOR.
Definition at line 93
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd(), USBH_GetConfigurationDescriptorB(), USBH_GetDeviceDescriptorB(), USBH_GetStringB(), and USBX_SetupCmdCb().
#define GET_INTERFACE 10 |
Standard setup request GET_INTERFACE.
Definition at line 97
of file em_usb.h
.
#define GET_STATUS 0 |
Standard setup request GET_STATUS.
Definition at line 89
of file em_usb.h
.
#define HUB_FEATURE_C_PORT_CONNECTION 16 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
Definition at line 206
of file em_usb.h
.
#define HUB_FEATURE_C_PORT_RESET 20 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
Definition at line 207
of file em_usb.h
.
#define HUB_FEATURE_PORT_INDICATOR 22 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
Definition at line 208
of file em_usb.h
.
#define HUB_FEATURE_PORT_POWER 8 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
Definition at line 205
of file em_usb.h
.
#define HUB_FEATURE_PORT_RESET 4 |
HUB class request CLEAR/SET_PORT_FEATURE feature selector.
Definition at line 204
of file em_usb.h
.
#define PORT_FULL_SPEED 1 |
Full speed return value for USBH_GetPortSpeed().
Definition at line 241
of file em_usb.h
.
Referenced by MSDBOT_Init().
#define PORT_LOW_SPEED 2 |
Low speed return value for USBH_GetPortSpeed().
Definition at line 242
of file em_usb.h
.
#define REMOTE_WAKEUP_ENABLED 0x0002 |
Standard request GET_STATUS bitmask.
Definition at line 200
of file em_usb.h
.
#define SET_ADDRESS 5 |
Standard setup request SET_ADDRESS.
Definition at line 92
of file em_usb.h
.
Referenced by USBH_SetAddressB().
#define SET_CONFIGURATION 9 |
Standard setup request SET_CONFIGURATION.
Definition at line 96
of file em_usb.h
.
Referenced by USBH_SetConfigurationB().
#define SET_DESCRIPTOR 7 |
Standard setup request SET_DESCRIPTOR.
Definition at line 94
of file em_usb.h
.
#define SET_FEATURE 3 |
Standard setup request SET_FEATURE.
Definition at line 91
of file em_usb.h
.
Referenced by USBH_StallEpB().
#define SET_INTERFACE 11 |
Standard setup request SET_INTERFACE.
Definition at line 98
of file em_usb.h
.
Referenced by USBH_SetAltInterfaceB().
#define SILABS_USB_VID 0x10C4 |
Silicon Labs Vendor ID, supplied by USB-IF.
Definition at line 65
of file em_usb.h
.
#define STATIC_CONST_STRING_DESC | ( | _name, |
|
... |
|||
) |
em_common.h:179
em_common.h:190
em_common.h:172
em_common.h:182
em_common.h:165
Macro for creating USB compliant UTF-16LE UNICODE string descriptors.
Example: STATIC_CONST_STRING_DESC(iManufacturer, 'E','n','e','r','g','y',' ','M','i','c','r','o',' ','A','S');
- Note
- The size of the resulting struct will be two byte larger than a USB string descriptor. This is to accommodate a terminating null char for the string. The value assigned to the 'len' member does not take this into account and is therefore correct usb wise.
Definition at line 268
of file em_usb.h
.
#define STATIC_CONST_STRING_DESC_LANGID | ( | _name, |
|
x, |
|||
y |
|||
) |
em_common.h:179
em_common.h:190
em_common.h:172
em_common.h:182
em_common.h:165
Macro for creating USB compliant language string descriptors.
Example: STATIC_CONST_STRING_DESC_LANGID(langID, 0x04, 0x09);
Definition at line 291
of file em_usb.h
.
#define STATIC_UBUF | ( | x, |
|
y |
|||
) | SL_ALIGN(4) static uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
Macro for creating WORD (4 byte) aligned static uint8_t arrays with size which is a multiple of WORD size.
Example:
STATIC_UBUF(rxBuffer, 37); => static uint8_t rxBuffer[40];
Definition at line 320
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define SYNCH_FRAME 12 |
Standard setup request SYNCH_FRAME.
Definition at line 99
of file em_usb.h
.
#define UBUF | ( | x, |
|
y |
|||
) | SL_ALIGN(4) uint8_t x[((y) + 3) & ~3] SL_ATTRIBUTE_ALIGN(4) |
Macro for creating WORD (4 byte) aligned uint8_t array with size which is a multiple of WORD size.
Example:
UBUF(rxBuffer, 37); => uint8_t rxBuffer[40];
Definition at line 314
of file em_usb.h
.
#define USB_AUDIO_GET_CUR 0x81 |
Audio class setup request GET_CUR.
Definition at line 114
of file em_usb.h
.
#define USB_AUDIO_GET_CUR 0x81 |
Audio class setup request GET_CUR.
Definition at line 114
of file em_usb.h
.
#define USB_AUDIO_GET_MAX 0x83 |
Audio class setup request GET_MAX.
Definition at line 118
of file em_usb.h
.
#define USB_AUDIO_GET_MEM 0x85 |
Audio class setup request GET_MEM.
Definition at line 122
of file em_usb.h
.
#define USB_AUDIO_GET_MIN 0x82 |
Audio class setup request GET_MIN.
Definition at line 116
of file em_usb.h
.
#define USB_AUDIO_GET_RES 0x84 |
Audio class setup request GET_RES.
Definition at line 120
of file em_usb.h
.
#define USB_AUDIO_GET_STAT 0xFF |
Audio class setup request GET_STAT.
Definition at line 123
of file em_usb.h
.
#define USB_AUDIO_SET_CUR 0x01 |
Audio class setup request SET_CUR.
Definition at line 113
of file em_usb.h
.
#define USB_AUDIO_SET_MAX 0x03 |
Audio class setup request SET_MAX.
Definition at line 117
of file em_usb.h
.
#define USB_AUDIO_SET_MEM 0x05 |
Audio class setup request SET_MEM.
Definition at line 121
of file em_usb.h
.
#define USB_AUDIO_SET_MIN 0x02 |
Audio class setup request SET_MIN.
Definition at line 115
of file em_usb.h
.
#define USB_AUDIO_SET_RES 0x04 |
Audio class setup request SET_RES.
Definition at line 119
of file em_usb.h
.
#define USB_CA_AS_GENERAL_DESCRIPTOR 1 |
Audio Class-Specific AS Interface General descriptor.
Definition at line 151
of file em_usb.h
.
#define USB_CA_AS_GENERAL_DESCSIZE 7 |
Audio Class-Specific AS Interface General desc size.
Definition at line 169
of file em_usb.h
.
#define USB_CA_EP_GENERAL_DESCRIPTOR 1 |
Audio Class-Specific general descriptor subtype code.
Definition at line 150
of file em_usb.h
.
#define USB_CA_EP_GENERAL_DESCSIZE 7 |
Audio Class-Specific general descriptor subtype size.
Definition at line 168
of file em_usb.h
.
#define USB_CA_EXTENSION_UNIT_DESCRIPTOR 8 |
Audio Class-Specific AC Interface Extension desc.
Definition at line 149
of file em_usb.h
.
#define USB_CA_FEATURE_UNIT_DESCRIPTOR 6 |
Audio Class-Specific AC Interface Feature desc.
Definition at line 147
of file em_usb.h
.
#define USB_CA_FORMAT_TYPE_DESCRIPTOR 2 |
Audio Class-Specific AS Interface Format Type desc.
Definition at line 152
of file em_usb.h
.
#define USB_CA_HEADER_DESCRIPTOR 1 |
Audio Class-Specific AC Interface Header descriptor.
Definition at line 142
of file em_usb.h
.
#define USB_CA_INPUT_TERMINAL_DESCRIPTOR 2 |
Audio Class-Specific AC Interface Input Terminal desc.
Definition at line 143
of file em_usb.h
.
#define USB_CA_INPUT_TERMINAL_DESCSIZE 12 |
Audio Input Terminal descriptor size.
Definition at line 166
of file em_usb.h
.
#define USB_CA_MIXER_UNIT_DESCRIPTOR 4 |
Audio Class-Specific AC Interface Mixer descriptor.
Definition at line 145
of file em_usb.h
.
#define USB_CA_OUTPUT_TERMINAL_DESCRIPTOR 3 |
Audio Class-Specific AC Interface Output Terminal desc.
Definition at line 144
of file em_usb.h
.
#define USB_CA_OUTPUT_TERMINAL_DESCSIZE 9 |
Audio Output Terminal descriptor size.
Definition at line 167
of file em_usb.h
.
#define USB_CA_PROCESSING_UNIT_DESCRIPTOR 7 |
Audio Class-Specific AC Interface Processing desc.
Definition at line 148
of file em_usb.h
.
#define USB_CA_SELECTOR_UNIT_DESCRIPTOR 5 |
Audio Class-Specific AC Interface Selector desc.
Definition at line 146
of file em_usb.h
.
#define USB_CA_STD_AS_ENDPOINT_DESCSZIE 9 |
Audio-class standard audio stream descriptor size.
Definition at line 170
of file em_usb.h
.
#define USB_CDC_ACM_FND_DESCSIZE 4 |
CDC Abstract Control Management functional descriptor size.
Definition at line 165
of file em_usb.h
.
#define USB_CDC_CALLMNG_FND_DESCSIZE 5 |
CDC Call Management functional descriptor size.
Definition at line 164
of file em_usb.h
.
#define USB_CDC_GETLINECODING 0x21 |
CDC class setup request GET_LINE_CODING.
Definition at line 108
of file em_usb.h
.
Referenced by CDC_SetupCmd().
#define USB_CDC_HEADER_FND_DESCSIZE 5 |
CDC Header functional descriptor size.
Definition at line 163
of file em_usb.h
.
#define USB_CDC_SETCTRLLINESTATE 0x22 |
CDC class setup request SET_CONTROL_LINE_STATE.
Definition at line 109
of file em_usb.h
.
Referenced by CDC_SetupCmd().
#define USB_CDC_SETLINECODING 0x20 |
CDC class setup request SET_LINE_CODING.
Definition at line 107
of file em_usb.h
.
Referenced by CDC_SetupCmd().
#define USB_CLASS_AUDIO 1 |
Audio interface class code.
Definition at line 231
of file em_usb.h
.
#define USB_CLASS_AUDIO_CONTROL 1 |
Audio subclass code for control interface.
Definition at line 232
of file em_usb.h
.
#define USB_CLASS_AUDIO_MIDISTREAMING 3 |
Audio subclass code for midi streaming interface.
Definition at line 234
of file em_usb.h
.
#define USB_CLASS_AUDIO_STREAMING 2 |
Audio subclass code for streaming interface.
Definition at line 233
of file em_usb.h
.
#define USB_CLASS_CDC 2 |
CDC device/interface class code.
Definition at line 210
of file em_usb.h
.
#define USB_CLASS_CDC_ACM 2 |
CDC Abstract Control Model interface subclass code.
Definition at line 212
of file em_usb.h
.
#define USB_CLASS_CDC_ACMFN 2 |
CDC class Abstract Control Management Functional Descriptor subtype.
Definition at line 215
of file em_usb.h
.
#define USB_CLASS_CDC_CMNGFN 1 |
CDC class Call Management Functional Descriptor subtype.
Definition at line 214
of file em_usb.h
.
#define USB_CLASS_CDC_DATA 0x0A |
CDC Data interface class code.
Definition at line 211
of file em_usb.h
.
#define USB_CLASS_CDC_HFN 0 |
CDC class Header Functional Descriptor subtype.
Definition at line 213
of file em_usb.h
.
#define USB_CLASS_CDC_UNIONFN 6 |
CDC class Union Functional Descriptor subtype.
Definition at line 216
of file em_usb.h
.
#define USB_CLASS_HID 3 |
HID device/interface class code.
Definition at line 218
of file em_usb.h
.
#define USB_CLASS_HID_KEYBOARD 1 |
HID keyboard interface protocol code.
Definition at line 219
of file em_usb.h
.
#define USB_CLASS_HID_MOUSE 2 |
HID mouse interface protocol code.
Definition at line 220
of file em_usb.h
.
#define USB_CLASS_HUB 9 |
HUB device/interface class code.
Definition at line 222
of file em_usb.h
.
#define USB_CLASS_MISC_COMMON_SUBCLASS 2 |
MISCELLANEOUS Common sub class code.
Definition at line 238
of file em_usb.h
.
#define USB_CLASS_MISC_IAD_PROTOCOL 1 |
MISCELLANEOUS Interface Association Descriptor protocol code.
Definition at line 239
of file em_usb.h
.
#define USB_CLASS_MISCELLANEOUS 0xEF |
MISCELLANEOUS device class code.
Definition at line 237
of file em_usb.h
.
#define USB_CLASS_MSD 8 |
MSD device/interface class code.
Definition at line 224
of file em_usb.h
.
#define USB_CLASS_MSD_BOT_TRANSPORT 0x50 |
MSD Bulk Only Transport protocol.
Definition at line 225
of file em_usb.h
.
#define USB_CLASS_MSD_CSW_CMDFAILED 1 |
MSD BOT Command status wrapper command failed code.
Definition at line 228
of file em_usb.h
.
#define USB_CLASS_MSD_CSW_CMDPASSED 0 |
MSD BOT Command status wrapper command passed code.
Definition at line 227
of file em_usb.h
.
Referenced by MSDBOT_Xfer().
#define USB_CLASS_MSD_CSW_PHASEERROR 2 |
MSD BOT Command status wrapper cmd phase error code.
Definition at line 229
of file em_usb.h
.
#define USB_CLASS_MSD_SCSI_CMDSET 6 |
MSD Subclass SCSI transparent command set.
Definition at line 226
of file em_usb.h
.
#define USB_CONFIG_DESCRIPTOR 2 |
CONFIGURATION descriptor value.
Definition at line 127
of file em_usb.h
.
Referenced by USBH_GetConfigurationDescriptorB(), and USBH_QGetConfigurationDescriptor().
#define USB_CONFIG_DESCSIZE 9 |
Configuration descriptor size.
Definition at line 155
of file em_usb.h
.
Referenced by USBH_InitDeviceData(), USBH_QGetConfigurationDescriptor(), USBH_QGetInterfaceDescriptor(), and USBH_QueryDeviceB().
#define USB_CS_ENDPOINT_DESCRIPTOR 0x25 |
Audio Class-specific endpoint Descriptor Type.
Definition at line 140
of file em_usb.h
.
#define USB_CS_INTERFACE_DESCRIPTOR 0x24 |
Audio Class-specific interface Descriptor Type.
Definition at line 139
of file em_usb.h
.
#define USB_DEVICE_DESCRIPTOR 1 |
DEVICE descriptor value.
Definition at line 126
of file em_usb.h
.
Referenced by USBH_GetDeviceDescriptorB(), and USBH_QGetDeviceDescriptor().
#define USB_DEVICE_DESCSIZE 18 |
Device descriptor size.
Definition at line 154
of file em_usb.h
.
Referenced by USBH_InitDeviceData(), USBH_QGetDeviceDescriptor(), and USBH_QueryDeviceB().
#define USB_DEVICE_QUALIFIER_DESCRIPTOR 6 |
DEVICE_QUALIFIER descriptor value.
Definition at line 132
of file em_usb.h
.
#define USB_DEVICE_QUALIFIER_DESCSIZE 10 |
Device qualifier descriptor size.
Definition at line 158
of file em_usb.h
.
#define USB_DPLL_SRC_HFXO 2 |
Use HFXO as DPLL clock source.
Definition at line 245
of file em_usb.h
.
#define USB_DPLL_SRC_LFXO 1 |
Use LFXO as DPLL clock source.
Definition at line 244
of file em_usb.h
.
#define USB_ENDPOINT_DESCRIPTOR 5 |
ENDPOINT descriptor value.
Definition at line 131
of file em_usb.h
.
Referenced by USBD_Init(), and USBH_QGetEndpointDescriptor().
#define USB_ENDPOINT_DESCSIZE 7 |
Endpoint descriptor size.
Definition at line 157
of file em_usb.h
.
Referenced by USBH_InitDeviceData(), and USBH_QGetEndpointDescriptor().
#define USB_EP_DIR_IN 0x80 |
Endpoint direction mask.
Definition at line 187
of file em_usb.h
.
#define USB_EPNUM_MASK 0x0F |
#define USB_EPSYNC_ADAPTIVE (2 << 2) |
Endpoint synchronization type, adaptive.
Definition at line 185
of file em_usb.h
.
#define USB_EPSYNC_ASYNC (1 << 2) |
Endpoint synchronization type, asynchronous.
Definition at line 184
of file em_usb.h
.
#define USB_EPSYNC_NO (0 << 2) |
Endpoint synchronization type, none.
Definition at line 183
of file em_usb.h
.
#define USB_EPSYNC_SYNC (3 << 2) |
Endpoint synchronization type, synchronous.
Definition at line 186
of file em_usb.h
.
#define USB_EPTYPE_BULK 2 |
Endpoint type bulk.
Definition at line 181
of file em_usb.h
.
#define USB_EPTYPE_CTRL 0 |
Endpoint type control.
Definition at line 179
of file em_usb.h
.
Referenced by USBD_Init(), and USBH_InitDeviceData().
#define USB_EPTYPE_INTR 3 |
Endpoint type interrupt.
Definition at line 182
of file em_usb.h
.
Referenced by USBH_Read(), and USBH_Write().
#define USB_EPTYPE_ISOC 1 |
Endpoint type isochron.
Definition at line 180
of file em_usb.h
.
#define USB_FEATURE_DEVICE_REMOTE_WAKEUP 1 |
Standard request CLEAR/SET_FEATURE bitmask.
Definition at line 202
of file em_usb.h
.
#define USB_FEATURE_ENDPOINT_HALT 0 |
Standard request CLEAR/SET_FEATURE bitmask.
Definition at line 201
of file em_usb.h
.
Referenced by MSDD_SetupCmd(), USBH_StallEpB(), and USBH_UnStallEpB().
#define USB_FS_BULK_EP_MAXSIZE 64 |
The max size of full speed bulk endpoints.
Definition at line 177
of file em_usb.h
.
Referenced by USBX_inXferCompleteCb().
#define USB_FS_CTRL_EP_MAXSIZE 64 |
The max size of full speed control endpoints.
Definition at line 175
of file em_usb.h
.
#define USB_FS_INTR_EP_MAXSIZE 64 |
The max size of full speed interrupt endpoints.
Definition at line 176
of file em_usb.h
.
#define USB_FS_ISOC_EP_MAXSIZE 1023 |
The max size of full speed isochronous endpoints.
Definition at line 178
of file em_usb.h
.
#define USB_HID_DESCRIPTOR 0x21 |
#define USB_HID_DESCSIZE 9 |
#define USB_HID_GET_IDLE 0x02 |
HID class setup request GET_IDLE.
Definition at line 103
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define USB_HID_GET_REPORT 0x01 |
HID class setup request GET_REPORT.
Definition at line 102
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define USB_HID_REPORT_DESCRIPTOR 0x22 |
HID REPORT descriptor value.
Definition at line 138
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define USB_HID_SET_IDLE 0x0A |
HID class setup request SET_IDLE.
Definition at line 105
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define USB_HID_SET_PROTOCOL 0x0B |
HID class setup request SET_PROTOCOL.
Definition at line 106
of file em_usb.h
.
#define USB_HID_SET_REPORT 0x09 |
HID class setup request SET_REPORT.
Definition at line 104
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd().
#define USB_HUB_DESCRIPTOR 0x29 |
HUB descriptor value.
Definition at line 141
of file em_usb.h
.
#define USB_INTERFACE_ASSOCIATION_DESCRIPTOR 11 |
INTERFACE_ASSOCIATION descriptor value.
Definition at line 135
of file em_usb.h
.
#define USB_INTERFACE_ASSOCIATION_DESCSIZE 8 |
INTERFACE_ASSOCIATION descriptor size.
Definition at line 160
of file em_usb.h
.
#define USB_INTERFACE_DESCRIPTOR 4 |
INTERFACE descriptor value.
Definition at line 130
of file em_usb.h
.
Referenced by USBD_Init(), and USBH_QGetInterfaceDescriptor().
#define USB_INTERFACE_DESCSIZE 9 |
Interface descriptor size.
Definition at line 156
of file em_usb.h
.
Referenced by USBH_InitDeviceData(), USBH_QGetEndpointDescriptor(), USBH_QGetInterfaceDescriptor(), and USBH_QueryDeviceB().
#define USB_INTERFACE_POWER_DESCRIPTOR 8 |
INTERFACE_POWER descriptor value.
Definition at line 134
of file em_usb.h
.
#define USB_LANGID_ENUS 0x0409 |
English-United States language id.
Definition at line 190
of file em_usb.h
.
#define USB_LS_CTRL_EP_MAXSIZE 8 |
The max size of low speed control endpoints.
Definition at line 173
of file em_usb.h
.
#define USB_LS_INTR_EP_MAXSIZE 8 |
The max size of low speed interrupt endpoints.
Definition at line 174
of file em_usb.h
.
#define USB_MAX_DEVICE_ADDRESS 127 |
Maximum allowable device address.
Definition at line 191
of file em_usb.h
.
Referenced by USBH_SetAddressB().
#define USB_MAX_STRING_DESCRIPTOR_CHARS 126 |
Maximum STRING descriptor bString length.
Definition at line 129
of file em_usb.h
.
#define USB_MSD_BOTRESET 0xFF |
MSD class setup request Bulk only transfer reset.
Definition at line 110
of file em_usb.h
.
Referenced by MSDD_SetupCmd().
#define USB_MSD_GETMAXLUN 0xFE |
MSD class setup request Get Max LUN.
Definition at line 111
of file em_usb.h
.
Referenced by MSDD_SetupCmd().
#define USB_OTHER_SPEED_CONFIG_DESCRIPTOR 7 |
OTHER_SPEED_CONFIGURATION descriptor value.
Definition at line 133
of file em_usb.h
.
#define USB_OTHER_SPEED_CONFIG_DESCSIZE 9 |
Device other speed configuration descriptor size.
Definition at line 159
of file em_usb.h
.
#define USB_SETUP_DIR_D2H 0x80 |
Setup request data stage IN direction mask.
Definition at line 71
of file em_usb.h
.
Referenced by USBH_GetConfigurationDescriptorB(), USBH_GetDeviceDescriptorB(), USBH_GetStringB(), and USBX_SetupCmdCb().
#define USB_SETUP_DIR_H2D 0x00 |
Setup request data stage OUT direction mask.
Definition at line 72
of file em_usb.h
.
Referenced by USBH_SetAddressB(), USBH_SetAltInterfaceB(), USBH_SetConfigurationB(), USBH_StallEpB(), and USBH_UnStallEpB().
#define USB_SETUP_DIR_IN 1 |
Setup request data stage IN direction value.
Definition at line 69
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), and MSDD_SetupCmd().
#define USB_SETUP_DIR_MASK 0x80 |
Setup request data stage direction mask.
Definition at line 70
of file em_usb.h
.
Referenced by USBD_Init(), and USBH_AssignHostChannel().
#define USB_SETUP_DIR_OUT 0 |
Setup request data stage OUT direction value.
Definition at line 68
of file em_usb.h
.
Referenced by MSDD_SetupCmd().
#define USB_SETUP_PKT_SIZE 8 |
Setup request packet size.
Definition at line 188
of file em_usb.h
.
#define USB_SETUP_RECIPIENT_DEVICE 0 |
Setup request device recipient value.
Definition at line 83
of file em_usb.h
.
Referenced by USBH_GetConfigurationDescriptorB(), USBH_GetDeviceDescriptorB(), USBH_GetStringB(), USBH_SetAddressB(), USBH_SetConfigurationB(), and USBX_SetupCmdCb().
#define USB_SETUP_RECIPIENT_ENDPOINT 2 |
Setup request endpoint recipient value.
Definition at line 85
of file em_usb.h
.
Referenced by MSDD_SetupCmd(), USBH_StallEpB(), and USBH_UnStallEpB().
#define USB_SETUP_RECIPIENT_INTERFACE 1 |
Setup request interface recipient value.
Definition at line 84
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), USBH_SetAltInterfaceB(), and USBX_SetupCmdCb().
#define USB_SETUP_RECIPIENT_OTHER 3 |
Setup request other recipient value.
Definition at line 86
of file em_usb.h
.
#define USB_SETUP_TYPE_CLASS 1 |
Class setup request value.
Definition at line 76
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), and MSDD_SetupCmd().
#define USB_SETUP_TYPE_CLASS_MASK 0x20 |
Class setup request mask.
Definition at line 79
of file em_usb.h
.
#define USB_SETUP_TYPE_STANDARD 0 |
Standard setup request value.
Definition at line 75
of file em_usb.h
.
Referenced by HIDKBD_SetupCmd(), MSDD_SetupCmd(), and USBX_SetupCmdCb().
#define USB_SETUP_TYPE_STANDARD_MASK 0x00 |
Standard setup request mask.
Definition at line 78
of file em_usb.h
.
Referenced by USBH_GetConfigurationDescriptorB(), USBH_GetDeviceDescriptorB(), USBH_GetStringB(), USBH_SetAddressB(), USBH_SetAltInterfaceB(), USBH_SetConfigurationB(), USBH_StallEpB(), and USBH_UnStallEpB().
#define USB_SETUP_TYPE_VENDOR 2 |
Vendor setup request value.
Definition at line 77
of file em_usb.h
.
Referenced by USBX_SetupCmdCb().
#define USB_SETUP_TYPE_VENDOR_MASK 0x40 |
#define USB_SMARTCARD_DESCRIPTOR 0x21 |
Smartcard usb-ccid-specific Descriptor Type.
Definition at line 137
of file em_usb.h
.
#define USB_SMARTCARD_DESCSIZE 54 |
CCID descriptor size.
Definition at line 162
of file em_usb.h
.
#define USB_STRING_DESCRIPTOR 3 |
STRING descriptor value.
Definition at line 128
of file em_usb.h
.
Referenced by USBH_GetStringB(), and USBX_SetupCmdCb().
Typedef Documentation
typedef unsigned short char16_t |
Data type used for UTF-16LE formatted USB string descriptors.
Definition at line 251
of file em_usb.h
.
typedef int(* USB_XferCompleteCb_TypeDef) (USB_Status_TypeDef status, uint32_t xferred, uint32_t remaining) |
USB transfer callback function.
The callback function is called when a transfer has completed. An application should check the status, xferred and optionally the remaining parameters before deciding if the transfer is usable. In the case where the transfer is part of a control request data stage, the callback function should return an appropriate USB_Status_TypeDef status.
- Parameters
-
[in] status
The transfer status. See USB_Status_TypeDef. [in] xferred
Number of bytes actually transferred. [in] remaining
Number of bytes not transferred.
- Returns
- USB_STATUS_OK on success, else an appropriate error code.
Definition at line 652
of file em_usb.h
.
typedef void(* USBTIMER_Callback_TypeDef) (void) |
USBTIMER callback function.
The callback function is called when an USBTIMER has expired. The callback is done with interrupts disabled.
Definition at line 662
of file em_usb.h
.
Enumeration Type Documentation
enum USB_Status_TypeDef |
USB transfer status enumerator.
Definition at line 323
of file em_usb.h
.
Function Documentation
char* USB_GetErrorMsgString | ( | int | error | ) |
Return an error message string for a given error code.
- Parameters
-
[in] error
Error code, see USB_Status_TypeDef.
- Returns
- Error message string pointer.
Definition at line 73
of file em_usbhal.c
.
Referenced by USB_PrintErrorMsgString().
void USB_PrintErrorMsgString | ( | char * | pre, |
int | error |
||
) |
Format and print a text string given an error code, prepends an optional user supplied leader string.
- Parameters
-
[in] pre
Optional leader string to prepend to error message string. [in] error
Error code, see USB_Status_TypeDef.
Definition at line 94
of file em_usbhal.c
.
References USB_GetErrorMsgString(), USB_PRINTF(), and USB_STATUS_OK.
int USB_PRINTF | ( | const char * | format, |
... |
|||
) |
Transmit "printf" formated data on the debug serial port.
- Note
- This function is enabled with #define USB_USE_PRINTF when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] format
Format string (as in printf). No floating point format support.
- Returns
- Number of chars transmitted.
Referenced by MSDH_Init(), USB_PrintErrorMsgString(), USBH_PrintConfigurationDescriptor(), USBH_PrintDeviceDescriptor(), USBH_PrintEndpointDescriptor(), and USBH_PrintInterfaceDescriptor().
int USB_PUTCHAR | ( | char | c | ) |
Transmit a single char on the debug serial port.
- Note
- This function is enabled with #define DEBUG_USB_API when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] c
Char to transmit.
- Returns
- The char transmitted.
Referenced by USBH_PrintConfigurationDescriptor(), and USBH_PrintString().
void USB_PUTS | ( | const char * | p | ) |
Transmit a zero terminated string on the debug serial port.
- Note
- This function is enabled with #define DEBUG_USB_API when configuring the protocol stack in "usbconfig.h". This is convenient when debugging code, no need to remove use of this function when debugging has completed.
- Parameters
-
[in] p
Pointer to string to transmit.
Referenced by USBH_PrintString().
void USBTIMER_DelayMs | ( | uint32_t | msec | ) |
Active wait millisecond delay function. Can also be used inside interrupt handlers.
- Parameters
-
[in] msec
Number of milliseconds to wait.
Definition at line 154
of file em_usbtimer.c
.
Referenced by MSDH_Init(), USBH_PortReset(), USBH_PortResume(), USBH_PortSuspend(), and USBH_WaitForDeviceConnectionB().
void USBTIMER_DelayUs | ( | uint32_t | usec | ) |
Active wait microsecond delay function. Can also be used inside interrupt handlers.
- Parameters
-
[in] usec
Number of microseconds to wait.
Definition at line 174
of file em_usbtimer.c
.
void USBTIMER_Init | ( | void |
| ) |
Activate the hardware timer used to pace the 1 millisecond timer system.
Call this function whenever the HFPERCLK frequency is changed. This function is initially called by HOST and DEVICE stack xxxx_Init() functions.
Definition at line 205
of file em_usbtimer.c
.
References CMU_ClockEnable(), CMU_ClockFreqGet(), cmuClock_HFPER, TIMER_InitCC_TypeDef::mode, TIMER_CompareSet(), TIMER_CounterGet(), TIMER_IEN_CC0, TIMER_Init(), TIMER_INIT_DEFAULT, TIMER_InitCC(), TIMER_INITCC_DEFAULT, TIMER_IntClear(), TIMER_IntEnable(), TIMER_TopSet(), and timerCCModeCompare.
Referenced by USBD_Init(), and USBH_Init().
void USBTIMER_Start | ( | uint32_t | id, |
uint32_t | timeout, |
||
USBTIMER_Callback_TypeDef | callback |
||
) |
Start a timer.
If the timer is already running, it will be restarted with new timeout.
- Parameters
-
[in] id
Timer id (0..). [in] timeout
Number of milliseconds before timer will elapse. [in] callback
Function to be called on timer elapse, ref. USBTIMER_Callback_TypeDef.
Definition at line 249
of file em_usbtimer.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, CORE_EXIT_ATOMIC, and USBTIMER_Stop().
Referenced by CDC_StateChangeEvent(), HIDKBD_StateChangeEvent(), USBH_ControlMsg(), USBH_Read(), and USBH_Write().
void USBTIMER_Stop | ( | uint32_t | id | ) |
Stop a timer.
- Parameters
-
[in] id
Timer id (0..).
Definition at line 311
of file em_usbtimer.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_ATOMIC, and CORE_EXIT_ATOMIC.
Referenced by CDC_StateChangeEvent(), HIDKBD_SetupCmd(), HIDKBD_StateChangeEvent(), USBH_Stop(), USBH_WaitForDeviceConnectionB(), and USBTIMER_Start().