USBH_Init_TypeDef Struct ReferencePlatform Middleware > USB > USB_HOST
USB Host stack initialization structure.
This structure is passed to USBH_Init() when starting up the device. Max accumulated FIFO size is 2K bytes.
Definition at line
881
of file
em_usb.h
.
#include <
em_usb.h
>
Data Fields |
|
| uint32_t | nptxFifoSize |
| uint32_t | ptxFifoSize |
| uint32_t | reserved |
| uint32_t | rxFifoSize |
Field Documentation
| uint32_t USBH_Init_TypeDef::nptxFifoSize |
Number of FIFO bytes set aside for OUT CTRL/BULK endoints.
Definition at line
883
of file
em_usb.h
.
Referenced by USBH_Init() .
| uint32_t USBH_Init_TypeDef::ptxFifoSize |
Number of FIFO bytes set aside for OUT INTR/ISO endoints.
Definition at line
884
of file
em_usb.h
.
Referenced by USBH_Init() .
| uint32_t USBH_Init_TypeDef::reserved |
Reserved for future use.
Definition at line
885
of file
em_usb.h
.
| uint32_t USBH_Init_TypeDef::rxFifoSize |
Number of FIFO bytes set aside for IN endpoints.
Definition at line
882
of file
em_usb.h
.
Referenced by USBH_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/middleware/usb_gecko/inc/
em_usb.h