TouchKit Drivers
Detailed Description
Touch panel driver for DK3650, DK3750 and DK3850 Development Kits.
Data Structures | |
struct | TOUCH_Config_TypeDef |
struct | TOUCH_Pos_TypeDef |
Macros | |
#define | ADC_X adcSingleInpCh1 |
#define | ADC_Y adcSingleInpCh4 |
#define | TOUCH_INIT_DEFAULT |
#define | TOUCH_X1_PIN 5 |
#define | TOUCH_X1_PORT gpioPortD |
#define | TOUCH_X2_PIN 4 |
#define | TOUCH_X2_PORT gpioPortD |
#define | TOUCH_Y1_PIN 3 |
#define | TOUCH_Y1_PORT gpioPortD |
#define | TOUCH_Y2_PIN 1 |
#define | TOUCH_Y2_PORT gpioPortD |
Typedefs | |
typedef void( | TOUCH_Upcall_TypeDef) (TOUCH_Pos_TypeDef *) |
Enumerations | |
enum | TOUCH_State_TypeDef { TOUCH_INIT, TOUCH_CHECK_PRESS, TOUCH_MEASURE_X, TOUCH_MEASURE_Y } |
Functions | |
void | ADC0_IRQHandler (void) |
Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second. | |
int | TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr) |
Set calibration table. | |
void | TOUCH_CallUpcall (void) |
Function that calls registered upcall. | |
TOUCH_Pos_TypeDef * | TOUCH_GetPos (void) |
Returns current touch position and state. | |
void | TOUCH_Init (TOUCH_Config_TypeDef *config) |
Initialize touch panel driver. | |
int | TOUCH_IsBusy (void) |
Check status of the touch panel. | |
void | TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos) |
Convert ADC readings into XY position. | |
void | TOUCH_RegisterUpcall (TOUCH_Upcall_TypeDef *new_upcall) |
Register upcall which will be call every position or state change. | |
int | TOUCH_StateChanged (void) |
Check if cursor state changed (down or move) | |
Variables | |
MATRIX | calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Macro Definition Documentation
#define ADC_X adcSingleInpCh1 |
#define ADC_Y adcSingleInpCh4 |
Input channel 4
Definition at line 51
of file touch.c
.
Referenced by ADC0_IRQHandler(), and TOUCH_Init().
#define TOUCH_INIT_DEFAULT |
Initializes Touch default values
Definition at line 63
of file touch.h
.
#define TOUCH_X1_PIN 5 |
#define TOUCH_X1_PORT gpioPortD |
#define TOUCH_X2_PIN 4 |
#define TOUCH_X2_PORT gpioPortD |
#define TOUCH_Y1_PIN 3 |
#define TOUCH_Y1_PORT gpioPortD |
#define TOUCH_Y2_PIN 1 |
#define TOUCH_Y2_PORT gpioPortD |
Typedef Documentation
typedef void( TOUCH_Upcall_TypeDef) (TOUCH_Pos_TypeDef *) |
touch panel upcall type definition
Definition at line 70
of file touch.h
.
Enumeration Type Documentation
enum TOUCH_State_TypeDef |
touch driver states
Definition at line 64
of file touch.c
.
Function Documentation
void ADC0_IRQHandler | ( | void |
| ) |
Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second.
ADC0 IRQ Handler
Definition at line 242
of file touch.c
.
References ADC_InitSingle_TypeDef::acqTime, ADC0, ADC_DataSingleGet(), ADC_IF_SINGLE, ADC_InitSingle(), ADC_IntClear(), ADC_Start(), ADC_X, ADC_Y, adcAcqTime128, adcAcqTime16, adcRefVDD, adcResOVS, adcStartSingle, TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, GPIO_PinInGet(), GPIO_PinModeSet(), gpioModeInput, gpioModeInputPullFilter, gpioModePushPull, ADC_InitSingle_TypeDef::input, TOUCH_Pos_TypeDef::pen, ADC_InitSingle_TypeDef::reference, ADC_InitSingle_TypeDef::resolution, TOUCH_CallUpcall(), TOUCH_RecalculatePosition(), TOUCH_StateChanged(), TOUCH_X1_PIN, TOUCH_X1_PORT, TOUCH_X2_PIN, TOUCH_X2_PORT, TOUCH_Y1_PIN, TOUCH_Y1_PORT, TOUCH_Y2_PIN, TOUCH_Y2_PORT, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
int TOUCH_CalibrationTable | ( | POINT * | displayPtr, |
POINT * | screenPtr |
||
) |
Set calibration table.
- Parameters
-
[in] displayPtr
Table of display points [in] screenPtr
Table of adc values reflecting display points
- Returns
- Returns OK if calibration table is set.
Definition at line 420
of file touch.c
.
References calibrationMatrix.
TOUCH_Pos_TypeDef * TOUCH_GetPos | ( | void |
| ) |
Returns current touch position and state.
- Returns
- Current touch position and state
Definition at line 383
of file touch.c
.
References ADC0, ADC_IF_SINGLE, ADC_IntDisable(), ADC_IntEnable(), TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
void TOUCH_Init | ( | TOUCH_Config_TypeDef * | config | ) |
Initialize touch panel driver.
- Parameters
-
config
Driver configuration data.
Definition at line 351
of file touch.c
.
References _ADC_IF_MASK, ADC0, ADC0_IRQn, ADC_IF_SINGLE, ADC_Init(), ADC_INIT_DEFAULT, ADC_InitSingle(), ADC_IntClear(), ADC_IntDisable(), ADC_IntEnable(), ADC_PrescaleCalc(), ADC_Start(), ADC_Y, adcRefVDD, adcResOVS, adcStartSingle, BSP_PeripheralAccess(), BSP_TOUCH, CMU_ClockEnable(), cmuClock_ADC0, TOUCH_Config_TypeDef::frequency, TOUCH_Config_TypeDef::ignore, ADC_InitSingle_TypeDef::input, TOUCH_Config_TypeDef::oversampling, ADC_Init_TypeDef::ovsRateSel, ADC_Init_TypeDef::prescale, ADC_InitSingle_TypeDef::reference, and ADC_InitSingle_TypeDef::resolution.
int TOUCH_IsBusy | ( | void |
| ) |
Check status of the touch panel.
- Returns
- 0 if panel is idle (not touched).
Definition at line 331
of file touch.c
.
References GPIO_PinInGet(), TOUCH_X2_PIN, and TOUCH_X2_PORT.
void TOUCH_RecalculatePosition | ( | volatile TOUCH_Pos_TypeDef * | pos | ) |
Convert ADC readings into XY position.
- Parameters
-
[in] pos
Pointer to position structure
Definition at line 172
of file touch.c
.
References TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, calibrationMatrix, TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
Referenced by ADC0_IRQHandler().
void TOUCH_RegisterUpcall | ( | TOUCH_Upcall_TypeDef * | new_upcall | ) |
Register upcall which will be call every position or state change.
- Parameters
-
[in] new_upcall
Pointer to upcall function
Definition at line 403
of file touch.c
.
int TOUCH_StateChanged | ( | void |
| ) |
Check if cursor state changed (down or move)
- Returns
- 1 if the cursor state has changed
Definition at line 215
of file touch.c
.
References TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.
Referenced by ADC0_IRQHandler().
Variable Documentation
MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Calibration table
Definition at line 84
of file touch.c
.
Referenced by TOUCH_CalibrationTable(), and TOUCH_RecalculatePosition().