USB_Setup_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB Setup request package.
Definition at line 381
of file em_usb.h
.
#include <
em_usb.h
>
Data Fields | |
union { | |
struct { | |
union { | |
struct { | |
uint8_t Direction: 1 | |
uint8_t Recipient: 5 | |
uint8_t Type: 2 | |
} | |
uint8_t bmRequestType | |
} | |
uint8_t bRequest | |
uint16_t wIndex | |
uint16_t wLength | |
uint16_t wValue | |
} | |
uint32_t dw [2] | |
}; | |
Field Documentation
uint8_t USB_Setup_TypeDef::bmRequestType |
Request characteristics.
Definition at line 390
of file em_usb.h
.
Referenced by USBH_ControlMsg(), and USBX_SetupCmdCb().
uint8_t USB_Setup_TypeDef::bRequest |
Request code.
Definition at line 392
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), USBH_ControlMsg(), and USBX_SetupCmdCb().
uint8_t USB_Setup_TypeDef::Direction |
Transfer direction of SETUP data phase.
Definition at line 388
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), and MSDD_SetupCmd().
uint8_t USB_Setup_TypeDef::Recipient |
Request recipient (device, interface, endpoint or other).
Definition at line 386
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), and MSDD_SetupCmd().
uint8_t USB_Setup_TypeDef::Type |
Request type (standard, class or vendor).
Definition at line 387
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), and USBX_SetupCmdCb().
uint16_t USB_Setup_TypeDef::wIndex |
Index or offset, varies according to request.
Definition at line 394
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), USBH_ControlMsg(), and USBX_SetupCmdCb().
uint16_t USB_Setup_TypeDef::wLength |
Number of bytes to transfer if there is a data stage.
Definition at line 395
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), USBH_ControlMsg(), and USBX_SetupCmdCb().
uint16_t USB_Setup_TypeDef::wValue |
Varies according to request.
Definition at line 393
of file em_usb.h
.
Referenced by CDC_SetupCmd(), HIDKBD_SetupCmd(), MSDD_SetupCmd(), USBH_ControlMsg(), and USBX_SetupCmdCb().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/middleware/usb_gecko/inc/
em_usb.h