DACEMLIB
Detailed Description
Digital to Analog Converter (DAC) Peripheral API.
This module contains functions to control the DAC peripheral of Silicon Labs 32-bit MCUs and SoCs. The DAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. The DAC is designed for low-energy consumption and can also provide very good performance.
Data Structures |
|
| struct | DAC_Init_TypeDef |
| struct | DAC_InitChannel_TypeDef |
Macros |
|
| #define | DAC_INIT_DEFAULT |
| #define | DAC_INITCHANNEL_DEFAULT |
Enumerations |
|
| enum |
DAC_ConvMode_TypeDef
{
dacConvModeContinuous = _DAC_CTRL_CONVMODE_CONTINUOUS, dacConvModeSampleHold = _DAC_CTRL_CONVMODE_SAMPLEHOLD, dacConvModeSampleOff = _DAC_CTRL_CONVMODE_SAMPLEOFF } |
| enum |
DAC_Output_TypeDef
{
dacOutputDisable = _DAC_CTRL_OUTMODE_DISABLE, dacOutputPin = _DAC_CTRL_OUTMODE_PIN, dacOutputADC = _DAC_CTRL_OUTMODE_ADC, dacOutputPinADC = _DAC_CTRL_OUTMODE_PINADC } |
| enum |
DAC_PRSSEL_TypeDef
{
dacPRSSELCh0 = _DAC_CH0CTRL_PRSSEL_PRSCH0, dacPRSSELCh1 = _DAC_CH0CTRL_PRSSEL_PRSCH1, dacPRSSELCh2 = _DAC_CH0CTRL_PRSSEL_PRSCH2, dacPRSSELCh3 = _DAC_CH0CTRL_PRSSEL_PRSCH3, dacPRSSELCh4 = _DAC_CH0CTRL_PRSSEL_PRSCH4, dacPRSSELCh5 = _DAC_CH0CTRL_PRSSEL_PRSCH5, dacPRSSELCh6 = _DAC_CH0CTRL_PRSSEL_PRSCH6, dacPRSSELCh7 = _DAC_CH0CTRL_PRSSEL_PRSCH7, dacPRSSELCh8 = _DAC_CH0CTRL_PRSSEL_PRSCH8, dacPRSSELCh9 = _DAC_CH0CTRL_PRSSEL_PRSCH9, dacPRSSELCh10 = _DAC_CH0CTRL_PRSSEL_PRSCH10, dacPRSSELCh11 = _DAC_CH0CTRL_PRSSEL_PRSCH11 } |
| enum |
DAC_Ref_TypeDef
{
dacRef1V25 = _DAC_CTRL_REFSEL_1V25, dacRef2V5 = _DAC_CTRL_REFSEL_2V5, dacRefVDD = _DAC_CTRL_REFSEL_VDD } |
| enum |
DAC_Refresh_TypeDef
{
dacRefresh8 = _DAC_CTRL_REFRSEL_8CYCLES, dacRefresh16 = _DAC_CTRL_REFRSEL_16CYCLES, dacRefresh32 = _DAC_CTRL_REFRSEL_32CYCLES, dacRefresh64 = _DAC_CTRL_REFRSEL_64CYCLES } |
Functions |
|
| __STATIC_INLINE void | DAC_Channel0OutputSet ( DAC_TypeDef *dac, uint32_t value) |
|
Set the output signal of DAC channel 0 to a given value.
|
|
| __STATIC_INLINE void | DAC_Channel1OutputSet ( DAC_TypeDef *dac, uint32_t value) |
|
Set the output signal of DAC channel 1 to a given value.
|
|
| void | DAC_ChannelOutputSet ( DAC_TypeDef *dac, unsigned int channel, uint32_t value) |
|
Set the output signal of a DAC channel to a given value.
|
|
| void | DAC_Enable ( DAC_TypeDef *dac, unsigned int ch, bool enable) |
|
Enable/disable the DAC channel.
|
|
| void | DAC_Init ( DAC_TypeDef *dac, const DAC_Init_TypeDef *init) |
|
Initialize DAC.
|
|
| void | DAC_InitChannel ( DAC_TypeDef *dac, const DAC_InitChannel_TypeDef *init, unsigned int ch) |
|
Initialize DAC channel.
|
|
| __STATIC_INLINE void | DAC_IntClear ( DAC_TypeDef *dac, uint32_t flags) |
|
Clear one or more pending DAC interrupts.
|
|
| __STATIC_INLINE void | DAC_IntDisable ( DAC_TypeDef *dac, uint32_t flags) |
|
Disable one or more DAC interrupts.
|
|
| __STATIC_INLINE void | DAC_IntEnable ( DAC_TypeDef *dac, uint32_t flags) |
|
Enable one or more DAC interrupts.
|
|
| __STATIC_INLINE uint32_t | DAC_IntGet ( DAC_TypeDef *dac) |
|
Get pending DAC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | DAC_IntGetEnabled ( DAC_TypeDef *dac) |
|
Get enabled and pending DAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | DAC_IntSet ( DAC_TypeDef *dac, uint32_t flags) |
|
Set one or more pending DAC interrupts from SW.
|
|
| uint8_t | DAC_PrescaleCalc (uint32_t dacFreq, uint32_t hfperFreq) |
|
Calculate prescaler value used to determine the DAC clock.
|
|
| void | DAC_Reset ( DAC_TypeDef *dac) |
|
Reset DAC to the same state that it was in after a hardware reset.
|
|
Macro Definition Documentation
| #define DAC_INIT_DEFAULT |
Default configuration for DAC initialization structure.
Definition at line
170
of file
em_dac.h
.
| #define DAC_INITCHANNEL_DEFAULT |
Default configuration for DAC channel initialization structure.
Definition at line
210
of file
em_dac.h
.
Enumeration Type Documentation
| enum DAC_ConvMode_TypeDef |
| enum DAC_Output_TypeDef |
| enum DAC_PRSSEL_TypeDef |
Peripheral Reflex System signal used to trigger single sample.
Definition at line
83
of file
em_dac.h
.
| enum DAC_Ref_TypeDef |
| enum DAC_Refresh_TypeDef |
Function Documentation
| __STATIC_INLINE void DAC_Channel0OutputSet | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
value
|
||
| ) |
Set the output signal of DAC channel 0 to a given value.
This function sets the output signal of DAC channel 0 by writing
value
to the CH0DATA register.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] valueValue to write to the channel 0 output register CH0DATA.
Definition at line
245
of file
em_dac.h
.
References _DAC_CH0DATA_MASK , and DAC_TypeDef::CH0DATA .
Referenced by DAC_ChannelOutputSet() .
| __STATIC_INLINE void DAC_Channel1OutputSet | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
value
|
||
| ) |
Set the output signal of DAC channel 1 to a given value.
Sets the output signal of DAC channel 1 by writing
value
to the CH1DATA register.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] valueValue to write to the channel 1 output register CH1DATA.
Definition at line
266
of file
em_dac.h
.
References _DAC_CH1DATA_MASK , and DAC_TypeDef::CH1DATA .
Referenced by DAC_ChannelOutputSet() .
| void DAC_ChannelOutputSet | ( | DAC_TypeDef * |
dac,
|
| unsigned int |
channel,
|
||
| uint32_t |
value
|
||
| ) |
Set the output signal of a DAC channel to a given value.
This function sets the output signal of a DAC channel by writing
value
to the corresponding CHnDATA register.
- Parameters
-
[in] dacA pointer to the DAC peripheral register block. [in] channelA channel number to set the output. [in] valueA value to write to the channel output register CHnDATA.
Definition at line
229
of file
em_dac.c
.
References DAC_Channel0OutputSet() , and DAC_Channel1OutputSet() .
| void DAC_Enable | ( | DAC_TypeDef * |
dac,
|
| unsigned int |
ch,
|
||
| bool |
enable
|
||
| ) |
Enable/disable the DAC channel.
- Parameters
-
[in] dacA pointer to the DAC peripheral register block. [in] chA channel to enable/disable. [in] enabletrue to enable DAC channel, false to disable.
Definition at line
85
of file
em_dac.c
.
References _DAC_CH0CTRL_EN_SHIFT , BUS_RegBitWrite() , DAC_TypeDef::CH0CTRL , and DAC_TypeDef::CH1CTRL .
| void DAC_Init | ( | DAC_TypeDef * |
dac,
|
| const DAC_Init_TypeDef * |
init
|
||
| ) |
Initialize DAC.
Initializes common parts for both channels. In addition, channel control configuration must be done. See DAC_InitChannel() .
- Note
- This function will disable both channels prior to configuration.
- Parameters
-
[in] dacA pointer to the DAC peripheral register block. [in] initA pointer to the DAC initialization structure.
Definition at line
118
of file
em_dac.c
.
References _DAC_CH0CTRL_EN_SHIFT , _DAC_CTRL_CONVMODE_SHIFT , _DAC_CTRL_OUTMODE_SHIFT , _DAC_CTRL_PRESC_MASK , _DAC_CTRL_PRESC_SHIFT , _DAC_CTRL_REFRSEL_SHIFT , _DAC_CTRL_REFSEL_SHIFT , BUS_RegBitWrite() , DAC_TypeDef::CAL , DAC_TypeDef::CH0CTRL , DAC_Init_TypeDef::ch0ResetPre , DAC_TypeDef::CH1CTRL , DAC_Init_TypeDef::convMode , DAC_TypeDef::CTRL , DAC_CTRL_CH0PRESCRST , DAC_CTRL_DIFF , DAC_CTRL_OUTENPRS , DAC_CTRL_SINEMODE , dacRef2V5 , dacRefVDD , DEVINFO , DAC_Init_TypeDef::diff , DAC_Init_TypeDef::outEnablePRS , DAC_Init_TypeDef::outMode , DAC_Init_TypeDef::prescale , DAC_Init_TypeDef::reference , DAC_Init_TypeDef::refresh , and DAC_Init_TypeDef::sineEnable .
| void DAC_InitChannel | ( | DAC_TypeDef * |
dac,
|
| const DAC_InitChannel_TypeDef * |
init,
|
||
| unsigned int |
ch
|
||
| ) |
Initialize DAC channel.
- Parameters
-
[in] dacA pointer to the DAC peripheral register block. [in] initA pointer to the DAC initialization structure. [in] chA channel number to initialize.
Definition at line
182
of file
em_dac.c
.
References _DAC_CH0CTRL_PRSSEL_SHIFT , DAC_TypeDef::CH0CTRL , DAC_TypeDef::CH1CTRL , DAC_CH0CTRL_EN , DAC_CH0CTRL_PRSEN , DAC_CH0CTRL_REFREN , DAC_InitChannel_TypeDef::enable , DAC_InitChannel_TypeDef::prsEnable , DAC_InitChannel_TypeDef::prsSel , and DAC_InitChannel_TypeDef::refreshEnable .
| __STATIC_INLINE void DAC_IntClear | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending DAC interrupts.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] flagsPending DAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
Definition at line
284
of file
em_dac.h
.
References DAC_TypeDef::IFC .
| __STATIC_INLINE void DAC_IntDisable | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
flags
|
||
| ) |
Disable one or more DAC interrupts.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
Definition at line
300
of file
em_dac.h
.
References DAC_TypeDef::IEN .
| __STATIC_INLINE void DAC_IntEnable | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
flags
|
||
| ) |
Enable one or more DAC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using DAC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
Definition at line
321
of file
em_dac.h
.
References DAC_TypeDef::IEN .
| __STATIC_INLINE uint32_t DAC_IntGet | ( | DAC_TypeDef * |
dac
|
) |
Get pending DAC interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] dacPointer to DAC peripheral register block.
- Returns
- DAC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
Definition at line
340
of file
em_dac.h
.
References DAC_TypeDef::IF .
| __STATIC_INLINE uint32_t DAC_IntGetEnabled | ( | DAC_TypeDef * |
dac
|
) |
Get enabled and pending DAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] dacPointer to DAC peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled DAC interrupt sources. Return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in DACx_IEN_nnn register (DACx_IEN_nnn) and
- the OR combination of valid interrupt flags of the DAC module (DACx_IF_nnn).
Definition at line
364
of file
em_dac.h
.
References DAC_TypeDef::IEN , and DAC_TypeDef::IF .
| __STATIC_INLINE void DAC_IntSet | ( | DAC_TypeDef * |
dac,
|
| uint32_t |
flags
|
||
| ) |
Set one or more pending DAC interrupts from SW.
- Parameters
-
[in] dacPointer to DAC peripheral register block. [in] flagsDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
Definition at line
387
of file
em_dac.h
.
References DAC_TypeDef::IFS .
| uint8_t DAC_PrescaleCalc | ( | uint32_t |
dacFreq,
|
| uint32_t |
hfperFreq
|
||
| ) |
Calculate prescaler value used to determine the DAC clock.
The DAC clock is given by: HFPERCLK / (prescale ^ 2). If the requested DAC frequency is low and the maximum prescaler value can't adjust the actual DAC frequency lower than the requested DAC frequency, the maximum prescaler value is returned resulting in a higher DAC frequency than requested.
- Parameters
-
[in] dacFreqDAC frequency wanted. The frequency will automatically be adjusted to be below the maximum allowed DAC clock. [in] hfperFreqFrequency in Hz of the reference HFPER clock. Set to 0 to use the currently defined HFPER clock setting.
- Returns
-
Prescaler value to use for DAC to achieve a clock value <=
dacFreq.
Definition at line
267
of file
em_dac.c
.
References _DAC_CTRL_PRESC_MASK , _DAC_CTRL_PRESC_SHIFT , CMU_ClockFreqGet() , and cmuClock_HFPER .
| void DAC_Reset | ( | DAC_TypeDef * |
dac
|
) |
Reset DAC to the same state that it was in after a hardware reset.
- Parameters
-
[in] dacA pointer to the ADC peripheral register block.
Definition at line
306
of file
em_dac.c
.
References _DAC_BIASPROG_RESETVALUE , _DAC_CH0CTRL_RESETVALUE , _DAC_CH1CTRL_RESETVALUE , _DAC_CTRL_RESETVALUE , _DAC_IEN_RESETVALUE , _DAC_IFC_MASK , DAC_TypeDef::BIASPROG , DAC_TypeDef::CAL , DAC_TypeDef::CH0CTRL , DAC_TypeDef::CH1CTRL , DAC_TypeDef::CTRL , DEVINFO , DAC_TypeDef::IEN , and DAC_TypeDef::IFC .