ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line
733
of file
em_acmp.h
.
#include <
em_acmp.h
>
Data Fields |
|
uint32_t | biasProg |
bool | enable |
bool | fullBias |
bool | halfBias |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
bool | inactiveValue |
bool | interruptOnFallingEdge |
bool | interruptOnRisingEdge |
bool | lowPowerReferenceEnabled |
uint32_t | vddLevel |
ACMP_WarmTime_TypeDef | warmTime |
Field Documentation
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line
748
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line
823
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::fullBias |
Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
737
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::halfBias |
Half-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
Definition at line
743
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
Definition at line
804
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on the falling edge.
Definition at line
752
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on the rising edge.
Definition at line
756
of file
em_acmp.h
.
Referenced by ACMP_Init() .
bool ACMP_Init_TypeDef::lowPowerReferenceEnabled |
Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.
Definition at line
809
of file
em_acmp.h
.
Referenced by ACMP_Init() .
uint32_t ACMP_Init_TypeDef::vddLevel |
VDD reference value. VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.
Definition at line
819
of file
em_acmp.h
.
Referenced by ACMP_Init() .
ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime |
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
Definition at line
782
of file
em_acmp.h
.
Referenced by ACMP_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_acmp.h