LESENSE_DecCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE decoder control descriptor structure.
Definition at line
669
of file
em_lesense.h
.
#include <
em_lesense.h
>
Data Fields |
|
| bool | chkState |
| LESENSE_DecInput_TypeDef | decInput |
| bool | hystIRQ |
| bool | hystPRS0 |
| bool | hystPRS1 |
| bool | hystPRS2 |
| uint32_t | initState |
| bool | intMap |
| LESENSE_PRSSel_TypeDef | prsChSel0 |
| LESENSE_PRSSel_TypeDef | prsChSel1 |
| LESENSE_PRSSel_TypeDef | prsChSel2 |
| LESENSE_PRSSel_TypeDef | prsChSel3 |
| bool | prsCount |
Field Documentation
| bool LESENSE_DecCtrlDesc_TypeDef::chkState |
Set to enable decoder to check the present state in addition to the states defined in TCONF.
Definition at line
678
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput |
Select input to the LESENSE decoder.
Definition at line
671
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ |
Set to enable hysteresis in decoder for suppressing the interrupt requests.
Definition at line
698
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0 |
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.
Definition at line
686
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1 |
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.
Definition at line
690
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2 |
Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.
Definition at line
694
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| uint32_t LESENSE_DecCtrlDesc_TypeDef::initState |
Initial state of the LESENSE decoder.
Definition at line
674
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::intMap |
When set, a transition from state x in decoder will set the interrupt flag CHx.
Definition at line
682
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0 |
Select PRS channel input for bit 0 of LESENSE decoder.
Definition at line
705
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1 |
Select PRS channel input for bit 1 of LESENSE decoder.
Definition at line
708
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2 |
Select PRS channel input for bit 2 of LESENSE decoder.
Definition at line
711
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3 |
Select PRS channel input for bit 3 of LESENSE decoder.
Definition at line
714
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::prsCount |
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
Definition at line
702
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_lesense.h