ROMTABLE_TypeDef Struct ReferenceDevices > EFM32WG_ROMTABLE
Definition at line
47
of file
efm32wg_romtable.h
.
Data Fields |
|
| __IM uint32_t | CID0 |
| __IM uint32_t | PID0 |
| __IM uint32_t | PID1 |
| __IM uint32_t | PID2 |
| __IM uint32_t | PID3 |
| __IM uint32_t | PID4 |
| __IM uint32_t | PID5 |
| __IM uint32_t | PID6 |
| __IM uint32_t | PID7 |
Field Documentation
| __IM uint32_t ROMTABLE_TypeDef::CID0 |
Unused
Definition at line
56
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID0 |
Chip family LSB, chip major revision
Definition at line
52
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID1 |
JEP_106_NO, Chip family MSB
Definition at line
53
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID2 |
Chip minor rev MSB, JEP_106_PRESENT, JEP_106_NO
Definition at line
54
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID3 |
Chip minor rev LSB
Definition at line
55
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID4 |
JEP_106_BANK
Definition at line
48
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID5 |
Unused
Definition at line
49
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID6 |
Unused
Definition at line
50
of file
efm32wg_romtable.h
.
| __IM uint32_t ROMTABLE_TypeDef::PID7 |
Unused
Definition at line
51
of file
efm32wg_romtable.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32WG/Include/
efm32wg_romtable.h