DMAEMLIB
Detailed Description
Direct Memory Access (DMA) Peripheral API.
DMA access functions provide basic support for the following types of DMA cycles:
- Basic , used for transferring data between memory and peripherals.
- Auto-request , used for transferring data between memory locations.
- Ping-pong , used for for continuous transfer of data between memory and peripherals, automatically toggling between primary and alternate descriptors.
- Memory scatter-gather , used for transferring a number of buffers between memory locations.
- Peripheral scatter-gather , used for transferring a number of buffers between memory and peripherals.
A basic understanding of the DMA controller is assumed. See the reference manual for more details.
The term 'descriptor' is synonymous to the 'channel control data structure' term.
To use the DMA controller, the initialization function must have been executed once (normally during the system initialization):
* DMA_Init(); *
Normally, a DMA channel is configured:
* DMA_CfgChannel(); *
The channel configuration only has to be done once if reusing the channel for the same purpose later.
To set up a DMA cycle, the primary and/or alternate descriptor has to be set up as indicated below.
For basic or auto-request cycles, use once on either primary or alternate descriptor:
* DMA_CfgDescr(); *
For ping-pong cycles, configure both primary or alternate descriptors:
* DMA_CfgDescr(); // Primary descriptor config * DMA_CfgDescr(); // Alternate descriptor config *
For scatter-gather cycles, program the alternate descriptor array:
* // 'n' is the number of scattered buffers * // 'descr' points to the start of the alternate descriptor array * * // Fill in 'cfg' * DMA_CfgDescrScatterGather(descr, 0, cfg); * // Fill in 'cfg' * DMA_CfgDescrScatterGather(descr, 1, cfg); * : * // Fill in 'cfg' * DMA_CfgDescrScatterGather(descr, n - 1, cfg); *
In many cases, the descriptor configuration only has to be done once if re-using the channel for the same type of DMA cycles later.
To activate the DMA cycle, use the respective DMA_Activate...() function.
For ping-pong DMA cycles, use DMA_RefreshPingPong() from the callback to prepare the completed descriptor for reuse. Notice that the refresh must be done prior to the other active descriptor completes, otherwise the ping-pong DMA cycle will halt.
Data Structures |
|
| struct | DMA_CB_TypeDef |
|
Callback structure that can be used to define DMA complete actions.
|
|
| struct | DMA_CfgChannel_TypeDef |
| struct | DMA_CfgDescr_TypeDef |
| struct | DMA_CfgDescrSGAlt_TypeDef |
| struct | DMA_CfgLoop_TypeDef |
| struct | DMA_CfgRect_TypeDef |
| struct | DMA_Init_TypeDef |
Typedefs |
|
| typedef void(* | DMA_FuncPtr_TypeDef ) (unsigned int channel, bool primary, void *user) |
|
DMA interrupt callback function pointer.
|
|
Enumerations |
|
| enum |
DMA_ArbiterConfig_TypeDef
{
dmaArbitrate1 = _DMA_CTRL_R_POWER_1, dmaArbitrate2 = _DMA_CTRL_R_POWER_2, dmaArbitrate4 = _DMA_CTRL_R_POWER_4, dmaArbitrate8 = _DMA_CTRL_R_POWER_8, dmaArbitrate16 = _DMA_CTRL_R_POWER_16, dmaArbitrate32 = _DMA_CTRL_R_POWER_32, dmaArbitrate64 = _DMA_CTRL_R_POWER_64, dmaArbitrate128 = _DMA_CTRL_R_POWER_128, dmaArbitrate256 = _DMA_CTRL_R_POWER_256, dmaArbitrate512 = _DMA_CTRL_R_POWER_512, dmaArbitrate1024 = _DMA_CTRL_R_POWER_1024 } |
| enum |
DMA_CycleCtrl_TypeDef
{
dmaCycleCtrlBasic = _DMA_CTRL_CYCLE_CTRL_BASIC, dmaCycleCtrlAuto = _DMA_CTRL_CYCLE_CTRL_AUTO, dmaCycleCtrlPingPong = _DMA_CTRL_CYCLE_CTRL_PINGPONG, dmaCycleCtrlMemScatterGather = _DMA_CTRL_CYCLE_CTRL_MEM_SCATTER_GATHER, dmaCycleCtrlPerScatterGather = _DMA_CTRL_CYCLE_CTRL_PER_SCATTER_GATHER } |
| enum |
DMA_DataInc_TypeDef
{
dmaDataInc1 = _DMA_CTRL_SRC_INC_BYTE, dmaDataInc2 = _DMA_CTRL_SRC_INC_HALFWORD, dmaDataInc4 = _DMA_CTRL_SRC_INC_WORD, dmaDataIncNone = _DMA_CTRL_SRC_INC_NONE } |
| enum |
DMA_DataSize_TypeDef
{
dmaDataSize1 = _DMA_CTRL_SRC_SIZE_BYTE, dmaDataSize2 = _DMA_CTRL_SRC_SIZE_HALFWORD, dmaDataSize4 = _DMA_CTRL_SRC_SIZE_WORD } |
Functions |
|
| void | DMA_ActivateAuto (unsigned int channel, bool primary, void *dst, const void *src, unsigned int nMinus1) |
|
Activate the DMA auto-request cycle (used for memory-memory transfers).
|
|
| void | DMA_ActivateBasic (unsigned int channel, bool primary, bool useBurst, void *dst, const void *src, unsigned int nMinus1) |
|
Activate the DMA basic cycle (used for memory-peripheral transfers).
|
|
| void | DMA_ActivatePingPong (unsigned int channel, bool useBurst, void *primDst, const void *primSrc, unsigned int primNMinus1, void *altDst, const void *altSrc, unsigned int altNMinus1) |
|
Activate a DMA ping-pong cycle (used for memory-peripheral transfers).
|
|
| void | DMA_ActivateScatterGather (unsigned int channel, bool useBurst, DMA_DESCRIPTOR_TypeDef *altDescr, unsigned int count) |
|
Activate the DMA scatter-gather cycle (used for either memory-peripheral or memory-memory transfers).
|
|
| void | DMA_CfgChannel (unsigned int channel, DMA_CfgChannel_TypeDef *cfg) |
|
Configure a DMA channel.
|
|
| void | DMA_CfgDescr (unsigned int channel, bool primary, DMA_CfgDescr_TypeDef *cfg) |
|
Configure the DMA descriptor for auto-request, basic, or ping-pong DMA cycles.
|
|
| void | DMA_CfgDescrScatterGather ( DMA_DESCRIPTOR_TypeDef *descr, unsigned int indx, DMA_CfgDescrSGAlt_TypeDef *cfg) |
|
Configure an alternate DMA descriptor for use with scatter-gather DMA cycles.
|
|
| void | DMA_CfgLoop (unsigned int channel, DMA_CfgLoop_TypeDef *cfg) |
|
Configure the DMA channel for Loop mode or 2D transfer.
|
|
| void | DMA_CfgRect (unsigned int channel, DMA_CfgRect_TypeDef *cfg) |
|
Configure the DMA channel 2D transfer properties.
|
|
| void | DMA_ChannelEnable (unsigned int channel, bool enable) |
|
Enable or disable a DMA channel.
|
|
| bool | DMA_ChannelEnabled (unsigned int channel) |
|
Check if the DMA channel is enabled.
|
|
| void | DMA_ChannelRequestEnable (unsigned int channel, bool enable) |
|
Enable or disable a DMA channel request.
|
|
| void | DMA_Init ( DMA_Init_TypeDef *init) |
|
Initialize the DMA controller.
|
|
| __STATIC_INLINE void | DMA_IntClear (uint32_t flags) |
|
Clear one or more pending DMA interrupts.
|
|
| __STATIC_INLINE void | DMA_IntDisable (uint32_t flags) |
|
Disable one or more DMA interrupts.
|
|
| __STATIC_INLINE void | DMA_IntEnable (uint32_t flags) |
|
Enable one or more DMA interrupts.
|
|
| __STATIC_INLINE uint32_t | DMA_IntGet (void) |
|
Get pending DMA interrupt flags.
|
|
| __STATIC_INLINE uint32_t | DMA_IntGetEnabled (void) |
|
Get enabled and pending DMA interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | DMA_IntSet (uint32_t flags) |
|
Set one or more pending DMA interrupts.
|
|
| void | DMA_IRQHandler (void) |
|
Interrupt handler for the DMA cycle completion handling.
|
|
| void | DMA_RefreshPingPong (unsigned int channel, bool primary, bool useBurst, void *dst, const void *src, unsigned int nMinus1, bool stop) |
|
Refresh a descriptor used in a DMA ping-pong cycle.
|
|
| void | DMA_Reset (void) |
|
Reset the DMA controller.
|
|
| __STATIC_INLINE void | DMA_ResetLoop (unsigned int channel) |
|
Clear Loop configuration for channel.
|
|
| __STATIC_INLINE void | DMA_ResetRect (unsigned int channel) |
|
Clear Rect/2D DMA configuration for channel.
|
|
Typedef Documentation
| typedef void(* DMA_FuncPtr_TypeDef) (unsigned int channel, bool primary, void *user) |
DMA interrupt callback function pointer.
Parameters:
- channel - DMA channel the callback function is invoked for.
- primary - Indicates if callback is invoked for completion of primary (true) or alternate (false) descriptor. Mainly useful for ping-pong DMA cycles, to know which descriptor to refresh.
- user - User definable reference that may be used to pass information to be used by the callback handler. If used, referenced data must be valid at the point when the interrupt handler invokes callback. If callback changes any data in the provided user structure, remember that those changes are done in interrupt context and proper protection of data may be required.
Definition at line
126
of file
em_dma.h
.
Enumeration Type Documentation
Number of transfers before controller does new arbitration.
Definition at line
92
of file
em_dma.h
.
Types of DMA transfer.
Definition at line
78
of file
em_dma.h
.
| enum DMA_DataInc_TypeDef |
| enum DMA_DataSize_TypeDef |
Function Documentation
| void DMA_ActivateAuto | ( | unsigned int |
channel,
|
| bool |
primary,
|
||
| void * |
dst,
|
||
| const void * |
src,
|
||
| unsigned int |
nMinus1
|
||
| ) |
Activate the DMA auto-request cycle (used for memory-memory transfers).
Prior to activating the DMA cycle, the channel and descriptor to be used must have been properly configured.
- Note
- If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to activate the DMA cycle for. [in] primary- true - activate using the primary descriptor
- false - activate using an alternate descriptor
[in] dstAn ddress to a start location to transfer data to. If NULL, leave setting in descriptor as is from a previous activation. [in] srcAn address to a start location to transfer data from. If NULL, leave setting in descriptor as is from a previous activation. [in] nMinus1A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr() .
Definition at line
361
of file
em_dma.c
.
References _DMA_CTRL_N_MINUS_1_MASK , _DMA_CTRL_N_MINUS_1_SHIFT , DMA , DMA_CHAN_COUNT , and dmaCycleCtrlAuto .
| void DMA_ActivateBasic | ( | unsigned int |
channel,
|
| bool |
primary,
|
||
| bool |
useBurst,
|
||
| void * |
dst,
|
||
| const void * |
src,
|
||
| unsigned int |
nMinus1
|
||
| ) |
Activate the DMA basic cycle (used for memory-peripheral transfers).
Prior to activating the DMA cycle, the channel and descriptor to be used must have been properly configured.
- Note
- If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to activate the DMA cycle for. [in] primary- true - activate using the primary descriptor
- false - activate using an alternate descriptor
[in] useBurstThe burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage. [in] dstAn address to a start location to transfer data to. If NULL, leave setting in descriptor as is from a previous activation. [in] srcAn address to a start location to transfer data from. If NULL, leave setting in descriptor as is from a previous activation. [in] nMinus1A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr() .
Definition at line
423
of file
em_dma.c
.
References _DMA_CTRL_N_MINUS_1_MASK , _DMA_CTRL_N_MINUS_1_SHIFT , DMA , DMA_CHAN_COUNT , and dmaCycleCtrlBasic .
Referenced by CDC_StateChangeEvent() .
| void DMA_ActivatePingPong | ( | unsigned int |
channel,
|
| bool |
useBurst,
|
||
| void * |
primDst,
|
||
| const void * |
primSrc,
|
||
| unsigned int |
primNMinus1,
|
||
| void * |
altDst,
|
||
| const void * |
altSrc,
|
||
| unsigned int |
altNMinus1
|
||
| ) |
Activate a DMA ping-pong cycle (used for memory-peripheral transfers).
Prior to activating the DMA cycle, the channel and both descriptors must have been properly configured. The primary descriptor is always the first descriptor to be used by the DMA controller.
- Note
- If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to activate DMA cycle for. [in] useBurstThe burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptors. See the reference manual for more details on burst usage. Notice that this setting is used for both the primary and alternate descriptors. [in] primDstAn address to a start location to transfer data to, for the primary descriptor. If NULL, leave setting in descriptor as is from a previous activation. [in] primSrcAn address to a start location to transfer data from, for the primary descriptor. If NULL, leave setting in the descriptor as is from a previous activation. [in] primNMinus1A number of DMA transfer elements (minus 1) to transfer (<= 1023), for primary descriptor. The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr() . [in] altDstAn address to a start location to transfer data to, for an alternate descriptor. If NULL, leave setting in descriptor as is from a previous activation. [in] altSrcAn address to a start location to transfer data from, for an alternate descriptor. If NULL, leave setting in descriptor as is from a previous activation. [in] altNMinus1A number of DMA transfer elements (minus 1) to transfer (<= 1023), for an alternate descriptor. The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr() .
Definition at line
494
of file
em_dma.c
.
References _DMA_CTRL_N_MINUS_1_MASK , _DMA_CTRL_N_MINUS_1_SHIFT , DMA , DMA_CHAN_COUNT , and dmaCycleCtrlPingPong .
| void DMA_ActivateScatterGather | ( | unsigned int |
channel,
|
| bool |
useBurst,
|
||
| DMA_DESCRIPTOR_TypeDef * |
altDescr,
|
||
| unsigned int |
count
|
||
| ) |
Activate the DMA scatter-gather cycle (used for either memory-peripheral or memory-memory transfers).
Prior to activating the DMA cycle, the array with alternate descriptors must have been properly configured. This function can be reused without reconfiguring the alternate descriptors, as long as
count
is the same.
- Note
- If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to activate DMA cycle for. [in] useBurstThe burst feature is only used on peripherals supporting DMA bursts (this parameter is ignored for memory scatter-gather cycles). This parameter determines if bursts should be enabled during DMA transfers using the alternate descriptors. Bursts must not be used if the total length (as given by nMinus1 for the alternate descriptor) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage. [in,out] altDescrA pointer to a start of an array with prepared alternate descriptors. The last descriptor will have its cycle control type reprogrammed to a basic type. [in] countA number of alternate descriptors in altDescrarray. The maximum number of alternate descriptors is 256.
Definition at line
563
of file
em_dma.c
.
References _DMA_CTRL_CYCLE_CTRL_MASK , _DMA_CTRL_CYCLE_CTRL_SHIFT , _DMA_CTRL_DST_INC_SHIFT , _DMA_CTRL_DST_SIZE_SHIFT , _DMA_CTRL_N_MINUS_1_SHIFT , _DMA_CTRL_NEXT_USEBURST_SHIFT , _DMA_CTRL_R_POWER_SHIFT , _DMA_CTRL_SRC_INC_SHIFT , _DMA_CTRL_SRC_PROT_CTRL_MASK , _DMA_CTRL_SRC_SIZE_SHIFT , DMA_DESCRIPTOR_TypeDef::CTRL , DMA , DMA_CHAN_COUNT , dmaArbitrate4 , dmaCycleCtrlAuto , dmaCycleCtrlBasic , dmaCycleCtrlMemScatterGather , dmaCycleCtrlPerScatterGather , dmaDataInc4 , dmaDataSize4 , DMA_DESCRIPTOR_TypeDef::DSTEND , DMA_CB_TypeDef::primary , DMA_DESCRIPTOR_TypeDef::SRCEND , and DMA_DESCRIPTOR_TypeDef::USER .
| void DMA_CfgChannel | ( | unsigned int |
channel,
|
| DMA_CfgChannel_TypeDef * |
cfg
|
||
| ) |
Configure a DMA channel.
Configure miscellaneous issues for a DMA channel. This function is typically used once to set up a channel for a certain type of use.
- Note
- If using this function on a channel already in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to configure. [in] cfgThe configuration to use.
Definition at line
667
of file
em_dma.c
.
References BUS_RegBitWrite() , DMA_CfgChannel_TypeDef::cb , DMA , DMA_CHAN_COUNT , DMA_CfgChannel_TypeDef::enableInt , DMA_CfgChannel_TypeDef::highPri , DMA_CfgChannel_TypeDef::select , and DMA_DESCRIPTOR_TypeDef::USER .
Referenced by NANDFLASH_Init() .
| void DMA_CfgDescr | ( | unsigned int |
channel,
|
| bool |
primary,
|
||
| DMA_CfgDescr_TypeDef * |
cfg
|
||
| ) |
Configure the DMA descriptor for auto-request, basic, or ping-pong DMA cycles.
This function is used to configure a descriptor for the following DMA cycle types:
- auto-request - used for a memory/memory transfer
- basic - used for a peripheral/memory transfer
- ping-pong - used for a ping-pong-based peripheral/memory transfer style providing time to refresh one descriptor while the other is in use.
The DMA cycle is not activated. See DMA_ActivateAuto() , DMA_ActivateBasic() , or DMA_ActivatePingPong() to activate the DMA cycle. In many cases, the configuration only has to be done once, and all subsequent cycles may be activated with the activate function.
For ping-pong DMA cycles, this function must be used both on the primary and the alternate descriptor prior to activating the DMA cycle.
Notice that the DMA channel must also be configured. See DMA_CfgChannel() .
- Note
- If using this function on a descriptor already activated and in use by the DMA controller, the behavior is undefined.
- Parameters
-
[in] channelThe DMA channel to configure for. [in] primary- true - configure the primary descriptor
- false - configure an alternate descriptor
[in] cfgThe configuration to use.
Definition at line
735
of file
em_dma.c
.
References _DMA_CTRL_DST_INC_SHIFT , _DMA_CTRL_DST_SIZE_SHIFT , _DMA_CTRL_N_MINUS_1_SHIFT , _DMA_CTRL_NEXT_USEBURST_SHIFT , _DMA_CTRL_R_POWER_SHIFT , _DMA_CTRL_SRC_INC_SHIFT , _DMA_CTRL_SRC_PROT_CTRL_SHIFT , _DMA_CTRL_SRC_SIZE_SHIFT , DMA_CfgDescr_TypeDef::arbRate , DMA_DESCRIPTOR_TypeDef::CTRL , DMA , DMA_CHAN_COUNT , DMA_CTRL_CYCLE_CTRL_INVALID , DMA_CfgDescr_TypeDef::dstInc , DMA_CfgDescr_TypeDef::hprot , DMA_CfgDescr_TypeDef::size , and DMA_CfgDescr_TypeDef::srcInc .
| void DMA_CfgDescrScatterGather | ( | DMA_DESCRIPTOR_TypeDef * |
descr,
|
| unsigned int |
indx,
|
||
| DMA_CfgDescrSGAlt_TypeDef * |
cfg
|
||
| ) |
Configure an alternate DMA descriptor for use with scatter-gather DMA cycles.
In scatter-gather mode, the alternate descriptors are located in one contiguous memory area. Each of the alternate descriptors must be fully configured prior to starting the scatter-gather DMA cycle.
The DMA cycle is not activated by this function. See DMA_ActivateScatterGather() to activate the DMA cycle. In some cases, the alternate configuration only has to be done once and all subsequent transfers may be activated with the activate function.
Notice that the DMA channel must also be configured, see DMA_CfgChannel() .
- Parameters
-
[in] descrPoints to the start of a memory area holding the alternate descriptors. [in] indxAn alternate descriptor index number to configure (numbered from 0). [in] cfgThe configuration to use.
Definition at line
850
of file
em_dma.c
.
References _DMA_CTRL_CYCLE_CTRL_SHIFT , _DMA_CTRL_DST_INC_SHIFT , _DMA_CTRL_DST_SIZE_SHIFT , _DMA_CTRL_N_MINUS_1_SHIFT , _DMA_CTRL_NEXT_USEBURST_SHIFT , _DMA_CTRL_R_POWER_SHIFT , _DMA_CTRL_SRC_INC_SHIFT , _DMA_CTRL_SRC_PROT_CTRL_SHIFT , _DMA_CTRL_SRC_SIZE_SHIFT , DMA_CfgDescrSGAlt_TypeDef::arbRate , DMA_DESCRIPTOR_TypeDef::CTRL , dmaCycleCtrlMemScatterGather , dmaCycleCtrlPerScatterGather , dmaDataIncNone , DMA_CfgDescrSGAlt_TypeDef::dst , DMA_DESCRIPTOR_TypeDef::DSTEND , DMA_CfgDescrSGAlt_TypeDef::dstInc , DMA_CfgDescrSGAlt_TypeDef::hprot , DMA_CfgDescrSGAlt_TypeDef::nMinus1 , DMA_CfgDescrSGAlt_TypeDef::peripheral , DMA_CfgDescrSGAlt_TypeDef::size , DMA_CfgDescrSGAlt_TypeDef::src , DMA_DESCRIPTOR_TypeDef::SRCEND , DMA_CfgDescrSGAlt_TypeDef::srcInc , and DMA_DESCRIPTOR_TypeDef::USER .
| void DMA_CfgLoop | ( | unsigned int |
channel,
|
| DMA_CfgLoop_TypeDef * |
cfg
|
||
| ) |
Configure the DMA channel for Loop mode or 2D transfer.
For 2D transfer, set cfg->enable to "false" and only configure nMinus1 to the same width as the channel descriptor.
- Parameters
-
[in] channelThe DMA channel to configure for. [in] cfgThe configuration to use.
Definition at line
779
of file
em_dma.c
.
References _DMA_LOOP0_EN_SHIFT , _DMA_LOOP0_WIDTH_SHIFT , _DMA_LOOP1_EN_SHIFT , _DMA_LOOP1_WIDTH_SHIFT , DMA , DMA_CfgLoop_TypeDef::enable , and DMA_CfgLoop_TypeDef::nMinus1 .
| void DMA_CfgRect | ( | unsigned int |
channel,
|
| DMA_CfgRect_TypeDef * |
cfg
|
||
| ) |
Configure the DMA channel 2D transfer properties.
- Parameters
-
[in] channelThe DMA channel to configure for. [in] cfgThe configuration to use.
Definition at line
808
of file
em_dma.c
.
References _DMA_RECT0_DSTSTRIDE_SHIFT , _DMA_RECT0_HEIGHT_SHIFT , _DMA_RECT0_SRCSTRIDE_SHIFT , DMA , DMA_CfgRect_TypeDef::dstStride , DMA_CfgRect_TypeDef::height , and DMA_CfgRect_TypeDef::srcStride .
| void DMA_ChannelEnable | ( | unsigned int |
channel,
|
| bool |
enable
|
||
| ) |
Enable or disable a DMA channel.
Use this function to explicitly enable or disable a DMA channel. A DMA channel is automatically disabled when the DMA controller has finished a transaction.
- Parameters
-
[in] channelThe DMA channel to enable or disable. [in] enableIf 'true', the channel will be enabled. If 'false', the channel will be disabled.
Definition at line
916
of file
em_dma.c
.
References DMA , and DMA_CHAN_COUNT .
Referenced by DMADRV_StopTransfer() .
| bool DMA_ChannelEnabled | ( | unsigned int |
channel
|
) |
Check if the DMA channel is enabled.
The DMA channel is disabled when the DMA controller has finished a DMA cycle.
- Parameters
-
[in] channelThe DMA channel to check.
- Returns
- True if the channel is enabled, false if not.
Definition at line
941
of file
em_dma.c
.
References DMA , and DMA_CHAN_COUNT .
Referenced by DMADRV_TransferActive() .
| void DMA_ChannelRequestEnable | ( | unsigned int |
channel,
|
| bool |
enable
|
||
| ) |
Enable or disable a DMA channel request.
Use this function to enable or disable a DMA channel request. This will prevent the DMA from proceeding after its current transaction if disabled.
- Parameters
-
[in] channelThe DMA channel to enable or disable the request on. [in] enableIf 'true', the request will be enabled. If 'false', the request will be disabled.
Definition at line
962
of file
em_dma.c
.
References BUS_RegBitWrite() , DMA , and DMA_CHAN_COUNT .
Referenced by DMADRV_PauseTransfer() , and DMADRV_ResumeTransfer() .
| void DMA_Init | ( | DMA_Init_TypeDef * |
init
|
) |
Initialize the DMA controller.
This function resets and prepares the DMA controller for use. Although it may be used several times, it is normally only used during system initialization. If reused during a normal operation, any ongoing DMA transfers will be aborted. When complete, the DMA controller is in an enabled state.
- Note
- Must be invoked before using the DMA controller.
- Parameters
-
[in] initA pointer to a structure containing the DMA initialization information.
Definition at line
990
of file
em_dma.c
.
References _DMA_CONFIG_CHPROT_SHIFT , CMU_ClockEnable() , cmuClock_DMA , DMA_Init_TypeDef::controlBlock , DMA , DMA_CONFIG_EN , DMA_IEN_ERR , DMA_IRQn , DMA_Reset() , and DMA_Init_TypeDef::hprot .
Referenced by DMADRV_Init() , and NANDFLASH_Init() .
| __STATIC_INLINE void DMA_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending DMA interrupts.
- Parameters
-
[in] flagsPending DMA interrupt sources to clear. Use one or more valid interrupt flags for the DMA module (DMA_IFC_nnn).
Definition at line
436
of file
em_dma.h
.
References DMA .
| __STATIC_INLINE void DMA_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more DMA interrupts.
- Parameters
-
[in] flagsDMA interrupt sources to disable. Use one or more valid interrupt flags for the DMA module (DMA_IEN_nnn).
Definition at line
449
of file
em_dma.h
.
References DMA .
| __STATIC_INLINE void DMA_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more DMA interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using DMA_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flagsDMA interrupt sources to enable. Use one or more valid interrupt flags for the DMA module (DMA_IEN_nnn).
Definition at line
467
of file
em_dma.h
.
References DMA .
| __STATIC_INLINE uint32_t DMA_IntGet | ( | void |
|
) |
Get pending DMA interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- DMA interrupt sources pending. Returns one or more valid interrupt flags for the DMA module (DMA_IF_nnn).
Definition at line
483
of file
em_dma.h
.
References DMA .
| __STATIC_INLINE uint32_t DMA_IntGetEnabled | ( | void |
|
) |
Get enabled and pending DMA interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled DMA interrupt sources Return value is the bitwise AND of
- the enabled interrupt sources in DMA_IEN and
- the pending interrupt flags DMA_IF.
Definition at line
502
of file
em_dma.h
.
References DMA .
| __STATIC_INLINE void DMA_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending DMA interrupts.
- Parameters
-
[in] flagsDMA interrupt sources to set to pending. Use one or more valid interrupt flags for the DMA module (DMA_IFS_nnn).
Definition at line
518
of file
em_dma.h
.
References DMA .
| void DMA_IRQHandler | ( | void |
|
) |
Interrupt handler for the DMA cycle completion handling.
Clears any pending flags and calls registered callback (if any).
If using the default interrupt vector table setup provided, this function is automatically placed in the IRQ table due to weak linking. If taking control over the interrupt vector table in some other way, this interrupt handler must be installed to support callback actions.
For the user to implement a custom IRQ handler or run without a DMA IRQ handler, define EXCLUDE_DEFAULT_DMA_IRQ_HANDLER with a #define statement or with the compiler option -D.
Definition at line
265
of file
em_dma.c
.
References DMA_CB_TypeDef::cbFunc , DMA , DMA_IF_ERR , DMA_CB_TypeDef::primary , and DMA_CB_TypeDef::userPtr .
| void DMA_RefreshPingPong | ( | unsigned int |
channel,
|
| bool |
primary,
|
||
| bool |
useBurst,
|
||
| void * |
dst,
|
||
| const void * |
src,
|
||
| unsigned int |
nMinus1,
|
||
| bool |
stop
|
||
| ) |
Refresh a descriptor used in a DMA ping-pong cycle.
During a ping-pong DMA cycle, the DMA controller automatically alternates between the primary and alternate descriptors, when completing use of a descriptor. While the other descriptor is in use by the DMA controller, the software should refresh the completed descriptor. This is typically done from the callback defined for the ping-pong cycle.
- Parameters
-
[in] channelThe DMA channel to refresh the ping-pong descriptor for. [in] primary- true - refresh the primary descriptor
- false - refresh an alternate descriptor
[in] useBurstThe burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage. [in] dstAn address to a start location to transfer data to. If NULL, leave setting in descriptor as is. [in] srcAn address to a start location to transfer data from. If NULL, leave setting in descriptor as is. [in] nMinus1A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr() . [in] stopIndicate that the DMA ping-pong cycle stops when done using this descriptor.
Definition at line
1067
of file
em_dma.c
.
References _DMA_CTRL_CYCLE_CTRL_MASK , _DMA_CTRL_CYCLE_CTRL_SHIFT , _DMA_CTRL_DST_INC_MASK , _DMA_CTRL_DST_INC_NONE , _DMA_CTRL_DST_INC_SHIFT , _DMA_CTRL_N_MINUS_1_MASK , _DMA_CTRL_N_MINUS_1_SHIFT , _DMA_CTRL_SRC_INC_MASK , _DMA_CTRL_SRC_INC_NONE , _DMA_CTRL_SRC_INC_SHIFT , DMA_DESCRIPTOR_TypeDef::CTRL , DMA , DMA_CHAN_COUNT , dmaCycleCtrlBasic , dmaCycleCtrlPingPong , DMA_DESCRIPTOR_TypeDef::DSTEND , and DMA_DESCRIPTOR_TypeDef::SRCEND .
| void DMA_Reset | ( | void |
|
) |
Reset the DMA controller.
This functions will disable the DMA controller and set it to a reset state.
- Note
- Note that any ongoing transfers will be aborted.
Definition at line
1141
of file
em_dma.c
.
References _DMA_CH_CTRL_RESETVALUE , _DMA_CHALTC_MASK , _DMA_CHENC_MASK , _DMA_CHPRIC_MASK , _DMA_CHREQMASKC_MASK , _DMA_CHUSEBURSTC_MASK , _DMA_CONFIG_RESETVALUE , _DMA_IEN_RESETVALUE , _DMA_IFC_MASK , DMA , DMA_CHAN_COUNT , DMA_ERRORC_ERRORC , and DMA_IRQn .
Referenced by DMA_Init() .
| __STATIC_INLINE void DMA_ResetLoop | ( | unsigned int |
channel
|
) |
Clear Loop configuration for channel.
- Parameters
-
[in] channelChannel to reset loop configuration for.
Definition at line
379
of file
em_dma.h
.
References _DMA_LOOP0_RESETVALUE , _DMA_LOOP1_RESETVALUE , and DMA .
| __STATIC_INLINE void DMA_ResetRect | ( | unsigned int |
channel
|
) |
Clear Rect/2D DMA configuration for channel.
- Parameters
-
[in] channelChannel to reset loop configuration for.
Definition at line
403
of file
em_dma.h
.
References _DMA_RECT0_RESETVALUE , and DMA .