Transmit_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Transmit plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
struct | EZRADIODRV_FieldLength |
struct | EZRADIODRV_PacketLengthConfig |
EzRadio transmit packet length configuration structure.
|
|
struct | EZRADIODRV_PacketTxHandle |
EzRadio transmit plug-in instance initialization and handler structure.
|
|
Macros |
|
#define | ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED ( ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE | 0x00000001) |
Unable to start transmission.
|
|
#define | EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio transmit plug-in.
|
|
Typedefs |
|
typedef struct EZRADIODRV_FieldLength | EZRADIODRV_FieldLength_t |
typedef struct EZRADIODRV_PacketLengthConfig | EZRADIODRV_PacketLengthConfig_t |
EzRadio transmit packet length configuration structure.
|
|
typedef struct EZRADIODRV_PacketTxHandle | EZRADIODRV_PacketTxHandle_t |
EzRadio transmit plug-in instance initialization and handler structure.
|
|
typedef enum EZRADIODRV_TransmitLengthMode | EZRADIODRV_TransmitLengthMode_t |
EzRadio transmit packet length mode.
|
|
typedef enum EZRADIODRV_TransmitPacketType | EZRADIODRV_TransmitPacketType_t |
EzRadio transmit packet type.
|
|
Enumerations |
|
enum |
EZRADIODRV_TransmitLengthMode
{
ezradiodrvTransmitLenghtDefault = 0, ezradiodrvTransmitLenghtCustomPacketLen = 1, ezradiodrvTransmitLenghtCustomFieldLen = 2 } |
EzRadio transmit packet length mode.
|
|
enum |
EZRADIODRV_TransmitPacketType
{
ezradiodrvPacketTypeNormal = 0, ezradiodrvPacketTypeAutoAck = 1 } |
EzRadio transmit packet type.
|
|
Functions |
|
Ecode_t | ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle, uint16_t packetLength, uint8_t *pioRadioPacket) |
Start basic transmission. Radio transmits with data only in the first field in this case.
|
|
Ecode_t | ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
Start transmission using the packet parameters from the generated configuration header file.
|
|
Ecode_t | ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
Start transmission using the packet parameters from pktLengthConf.
|
|
Ecode_t | ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
|
|
Ecode_t | ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.
|
|
Macro Definition Documentation
#define EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio transmit plug-in.
Definition at line
101
of file
ezradio_transmit_plugin.h
.
Typedef Documentation
typedef struct EZRADIODRV_FieldLength EZRADIODRV_FieldLength_t |
EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.
Enumeration Type Documentation
EzRadio transmit packet length mode.
Definition at line
53
of file
ezradio_transmit_plugin.h
.
Function Documentation
Ecode_t ezradioStartTransmitBasic | ( | EZRADIODRV_Handle_t |
radioHandle,
|
uint16_t |
packetLength,
|
||
uint8_t * |
pioRadioPacket
|
||
) |
Start basic transmission. Radio transmits with data only in the first field in this case.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet length and channel configurations are set. packetLength
Length of the basic packet. pioRadioPacket
Pointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
55
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
Ecode_t ezradioStartTransmitConfigured | ( | EZRADIODRV_Handle_t |
radioHandle,
|
uint8_t * |
pioRadioPacket
|
||
) |
Start transmission using the packet parameters from the generated configuration header file.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet length and channel configurations are set. pioRadioPacket
Pointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
96
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtDefault , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
Ecode_t ezradioStartTransmitCustom | ( | EZRADIODRV_Handle_t |
radioHandle,
|
EZRADIODRV_PacketLengthConfig_t |
pktLengthConf,
|
||
uint8_t * |
pioRadioPacket
|
||
) |
Start transmission using the packet parameters from pktLengthConf.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet length and channel configurations are set. pktLengthConf
Packet length configuration structure configuration of the custom packet. pioRadioPacket
Pointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
137
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
Ecode_t ezradioStartTransmitDefault | ( | EZRADIODRV_Handle_t |
radioHandle,
|
uint8_t * |
pioRadioPacket
|
||
) |
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet length and channel configurations are set. pioRadioPacket
Pointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
206
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradioStartTransmitSmart() , EZRADIODRV_PacketTxHandle::lenConfig , and EZRADIODRV_HandleData::packetTx .
Ecode_t ezradioStartTransmitSmart | ( | EZRADIODRV_Handle_t |
radioHandle,
|
EZRADIODRV_PacketLengthConfig_t |
pktLengthConf,
|
||
uint8_t * |
pioRadioPacket
|
||
) |
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where packet length and channel configurations are set. pktLengthConf
Packet length configuration structure configuration of the custom packet. pioRadioPacket
Pointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
176
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomFieldLen , ezradiodrvTransmitLenghtCustomPacketLen , ezradiodrvTransmitLenghtDefault , ezradioStartTransmitBasic() , ezradioStartTransmitConfigured() , ezradioStartTransmitCustom() , EZRADIODRV_PacketLengthConfig::lenMode , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitDefault() .