CSEN_InitMode_TypeDef Struct ReferenceEMLIB > CSEN

Measurement mode initialization structure.

Definition at line 393 of file em_csen.h .

#include < em_csen.h >

Data Fields

CSEN_AccMode_TypeDef accMode
bool autoGnd
CSEN_CmpMode_TypeDef cmpMode
uint16_t cmpThr
CSEN_ConvSel_TypeDef convSel
uint8_t dmCycles
uint8_t dmDelta
bool dmFixedDelta
uint8_t dmIterPerCycle
CSEN_DMRes_TypeDef dmRes
CSEN_DriveSel_TypeDef driveSel
CSEN_EMASample_TypeDef emaSample
bool enableDma
CSEN_GainSel_TypeDef gainSel
uint32_t inputMask0
uint32_t inputMask1
CSEN_ResetPhaseSel_TypeDef resetPhase
CSEN_SampleMode_TypeDef sampleMode
CSEN_SARRes_TypeDef sarRes
CSEN_SingleSel_TypeDef singleSel
bool sumOnly
CSEN_TrigSel_TypeDef trigSel

Field Documentation

CSEN_AccMode_TypeDef CSEN_InitMode_TypeDef::accMode

Selects the number of samples to accumulate per conversion.

Definition at line 407 of file em_csen.h .

Referenced by CSEN_InitMode() .

bool CSEN_InitMode_TypeDef::autoGnd

Ground inactive inputs during a conversion.

Definition at line 434 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_CmpMode_TypeDef CSEN_InitMode_TypeDef::cmpMode

Enables the comparator and selects the comparison type.

Definition at line 413 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint16_t CSEN_InitMode_TypeDef::cmpThr

Comparator threshold value. Meaning depends on cmpMode .

Definition at line 416 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_ConvSel_TypeDef CSEN_InitMode_TypeDef::convSel

Selects the converter type.

Definition at line 437 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint8_t CSEN_InitMode_TypeDef::dmCycles

Sets number of DM converter cycles. Only applies to the Delta Modulation converter.

Definition at line 451 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint8_t CSEN_InitMode_TypeDef::dmDelta

Sets the DM converter initial delta value. Only applies to the Delta Modulation converter.

Definition at line 455 of file em_csen.h .

Referenced by CSEN_InitMode() .

bool CSEN_InitMode_TypeDef::dmFixedDelta

Disables DM automatic delta size reduction per cycle. Only applies to the Delta Modulation converter.

Definition at line 459 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint8_t CSEN_InitMode_TypeDef::dmIterPerCycle

Sets the number of DM iterations (comparisons) per cycle. Only applies to the Delta Modulation converter.

Definition at line 447 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_DMRes_TypeDef CSEN_InitMode_TypeDef::dmRes

Selects the Delta Modulation (DM) converter resolution.

Definition at line 443 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_DriveSel_TypeDef CSEN_InitMode_TypeDef::driveSel

Selects the output drive strength. Most measurements should use the default value. See reference manual for details on when to adjust.

Definition at line 467 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_EMASample_TypeDef CSEN_InitMode_TypeDef::emaSample

Selects the Exponential Moving Average sample weighting.

Definition at line 410 of file em_csen.h .

Referenced by CSEN_InitMode() .

bool CSEN_InitMode_TypeDef::enableDma

Enables DMA operation.

Definition at line 401 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_GainSel_TypeDef CSEN_InitMode_TypeDef::gainSel

Selects the converter gain.

Definition at line 470 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint32_t CSEN_InitMode_TypeDef::inputMask0

Mask selects inputs 0 to 31. Effect depends on sampleMode . If sample mode is bonded, then mask selects inputs to short together. If sample mode is scan, then mask selects which inputs will be scanned. If sample mode is single and auto-ground is on ( autoGnd is true), mask selects which pins are grounded.

Definition at line 428 of file em_csen.h .

Referenced by CSEN_InitMode() .

uint32_t CSEN_InitMode_TypeDef::inputMask1

Mask selects inputs 32 to 63. See inputMask0 for more information.

Definition at line 431 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_ResetPhaseSel_TypeDef CSEN_InitMode_TypeDef::resetPhase

Selects the reset phase timing. Most measurements should use the default value. See reference manual for details on when to adjust.

Definition at line 463 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_SampleMode_TypeDef CSEN_InitMode_TypeDef::sampleMode

Selects the conversion sample mode.

Definition at line 395 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_SARRes_TypeDef CSEN_InitMode_TypeDef::sarRes

Selects the Successive Approximation (SAR) converter resolution.

Definition at line 440 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_SingleSel_TypeDef CSEN_InitMode_TypeDef::singleSel

Selects an APORT channel for a single conversion.

Definition at line 419 of file em_csen.h .

Referenced by CSEN_InitMode() .

bool CSEN_InitMode_TypeDef::sumOnly

Disables dividing the accumulated result.

Definition at line 404 of file em_csen.h .

Referenced by CSEN_InitMode() .

CSEN_TrigSel_TypeDef CSEN_InitMode_TypeDef::trigSel

Selects the conversion trigger source.

Definition at line 398 of file em_csen.h .

Referenced by CSEN_InitMode() .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_csen.h