ACMP_TypeDef Struct ReferenceDevices > ACMP

ACMP Register Declaration

Definition at line 48 of file efm32jg12b_acmp.h.

#include <efm32jg12b_acmp.h>

Data Fields

__IM uint32_t APORTCONFLICT
 
__IM uint32_t APORTREQ
 
__IOM uint32_t CTRL
 
__IOM uint32_t EXTIFCTRL
 
__IOM uint32_t HYSTERESIS0
 
__IOM uint32_t HYSTERESIS1
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t INPUTSEL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [4U]
 
__IOM uint32_t ROUTELOC0
 
__IOM uint32_t ROUTEPEN
 
__IM uint32_t STATUS
 

Field Documentation

__IM uint32_t ACMP_TypeDef::APORTCONFLICT

APORT Conflict Status Register

Definition at line 58 of file efm32jg12b_acmp.h.

__IM uint32_t ACMP_TypeDef::APORTREQ

APORT Request Status Register

Definition at line 57 of file efm32jg12b_acmp.h.

__IOM uint32_t ACMP_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32jg12b_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Disable(), ACMP_Enable(), ACMP_GPIOSetup(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::EXTIFCTRL

External Override Interface Control

Definition at line 65 of file efm32jg12b_acmp.h.

Referenced by ACMP_ExternalInputSelect().

__IOM uint32_t ACMP_TypeDef::HYSTERESIS0

Hysteresis 0 Register

Definition at line 59 of file efm32jg12b_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Init(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().

__IOM uint32_t ACMP_TypeDef::HYSTERESIS1

Hysteresis 1 Register

Definition at line 60 of file efm32jg12b_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Init(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().

__IOM uint32_t ACMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 55 of file efm32jg12b_acmp.h.

Referenced by ACMP_IntDisable(), ACMP_IntEnable(), ACMP_IntGetEnabled(), and ACMP_Reset().

__IM uint32_t ACMP_TypeDef::IF

Interrupt Flag Register

Definition at line 52 of file efm32jg12b_acmp.h.

Referenced by ACMP_IntGet(), and ACMP_IntGetEnabled().

__IOM uint32_t ACMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 54 of file efm32jg12b_acmp.h.

Referenced by ACMP_IntClear(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 53 of file efm32jg12b_acmp.h.

Referenced by ACMP_IntSet().

__IOM uint32_t ACMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 50 of file efm32jg12b_acmp.h.

Referenced by ACMP_CapsenseChannelSet(), ACMP_CapsenseInit(), ACMP_ChannelSet(), ACMP_Init(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().

uint32_t ACMP_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 56 of file efm32jg12b_acmp.h.

uint32_t ACMP_TypeDef::RESERVED1[4U]

Reserved for future use

Definition at line 62 of file efm32jg12b_acmp.h.

__IOM uint32_t ACMP_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 64 of file efm32jg12b_acmp.h.

Referenced by ACMP_GPIOSetup().

__IOM uint32_t ACMP_TypeDef::ROUTEPEN

I/O Routing Pine Enable Register

Definition at line 63 of file efm32jg12b_acmp.h.

Referenced by ACMP_GPIOSetup().

__IM uint32_t ACMP_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32jg12b_acmp.h.

Referenced by ACMP_ExternalInputSelect().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/efm32jg12b_acmp.h