PRS_TypeDef Struct ReferenceDevices > PRS
PRS Register Declaration
Definition at line 48
of file efm32jg12b_prs.h
.
#include <
efm32jg12b_prs.h
>
Data Fields | |
PRS_CH_TypeDef | CH [12U] |
__IOM uint32_t | CTRL |
__IOM uint32_t | DMAREQ0 |
__IOM uint32_t | DMAREQ1 |
__IM uint32_t | PEEK |
uint32_t | RESERVED0 [1U] |
uint32_t | RESERVED1 [5U] |
uint32_t | RESERVED2 [1U] |
uint32_t | RESERVED3 [3U] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTELOC1 |
__IOM uint32_t | ROUTELOC2 |
__IOM uint32_t | ROUTEPEN |
__IOM uint32_t | SWLEVEL |
__IOM uint32_t | SWPULSE |
Field Documentation
PRS_CH_TypeDef PRS_TypeDef::CH[12U] |
Channel registers
Definition at line 65
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::CTRL |
Control Register
Definition at line 58
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::DMAREQ0 |
DMA Request 0 Register
Definition at line 59
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::DMAREQ1 |
DMA Request 1 Register
Definition at line 60
of file efm32jg12b_prs.h
.
__IM uint32_t PRS_TypeDef::PEEK |
PRS Channel Values
Definition at line 62
of file efm32jg12b_prs.h
.
uint32_t PRS_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line 52
of file efm32jg12b_prs.h
.
uint32_t PRS_TypeDef::RESERVED1[5U] |
Reserved for future use
Definition at line 57
of file efm32jg12b_prs.h
.
uint32_t PRS_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line 61
of file efm32jg12b_prs.h
.
uint32_t PRS_TypeDef::RESERVED3[3U] |
Reserved registers
Definition at line 64
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 53
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC1 |
I/O Routing Location Register
Definition at line 54
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC2 |
I/O Routing Location Register
Definition at line 55
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 51
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line 50
of file efm32jg12b_prs.h
.
__IOM uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line 49
of file efm32jg12b_prs.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_prs.h