LDMA_Init_t Struct ReferenceEMLIB > LDMA

LDMA initialization configuration structure.

Definition at line 851 of file em_ldma.h .

#include < em_ldma.h >

Data Fields

uint8_t ldmaInitCtrlNumFixed
uint8_t ldmaInitCtrlSyncPrsClrEn
uint8_t ldmaInitCtrlSyncPrsSetEn
uint8_t ldmaInitIrqPriority

Field Documentation

uint8_t LDMA_Init_t::ldmaInitCtrlNumFixed

Arbitration mode separator.

Definition at line 852 of file em_ldma.h .

Referenced by DMADRV_Init() , and LDMA_Init() .

uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsClrEn

PRS Synctrig clear enable.

Definition at line 853 of file em_ldma.h .

Referenced by LDMA_Init() .

uint8_t LDMA_Init_t::ldmaInitCtrlSyncPrsSetEn

PRS Synctrig set enable.

Definition at line 854 of file em_ldma.h .

Referenced by LDMA_Init() .

uint8_t LDMA_Init_t::ldmaInitIrqPriority

LDMA IRQ priority (0..7).

Definition at line 855 of file em_ldma.h .

Referenced by DMADRV_Init() , and LDMA_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_ldma.h