LESENSE_TypeDef Struct ReferenceDevices > LESENSE
LESENSE Register Declaration
Definition at line 48
of file efm32jg12b_lesense.h
.
#include <
efm32jg12b_lesense.h
>
Data Fields | |
__IOM uint32_t | ALTEXCONF |
__IOM uint32_t | BIASCTRL |
LESENSE_BUF_TypeDef | BUF [16U] |
__IM uint32_t | BUFDATA |
LESENSE_CH_TypeDef | CH [16U] |
__IOM uint32_t | CHEN |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IM uint32_t | CURCH |
__IOM uint32_t | DECCTRL |
__IOM uint32_t | DECSTATE |
__IOM uint32_t | EVALCTRL |
__IOM uint32_t | IDLECONF |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PERCTRL |
__IOM uint32_t | PRSCTRL |
__IM uint32_t | PTR |
uint32_t | RESERVED0 [2U] |
uint32_t | RESERVED1 [38U] |
__IOM uint32_t | ROUTEPEN |
__IOM uint32_t | SCANRES |
__IOM uint32_t | SENSORSTATE |
LESENSE_ST_TypeDef | ST [32U] |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IOM uint32_t | TIMCTRL |
Field Documentation
__IOM uint32_t LESENSE_TypeDef::ALTEXCONF |
Alternative Excite Pin Configuration
Definition at line 66
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::BIASCTRL |
Bias Control Register
Definition at line 53
of file efm32jg12b_lesense.h
.
LESENSE_BUF_TypeDef LESENSE_TypeDef::BUF[16U] |
Scanresult
Definition at line 78
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::BUFDATA |
Result Buffer Data Register
Definition at line 61
of file efm32jg12b_lesense.h
.
LESENSE_CH_TypeDef LESENSE_TypeDef::CH[16U] |
Scanconfig
Definition at line 80
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CHEN |
Channel Enable Register
Definition at line 57
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CMD |
Command Register
Definition at line 56
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::CURCH |
Current Channel Index
Definition at line 62
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::DECCTRL |
Decoder Control Register
Definition at line 52
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::DECSTATE |
Current Decoder State
Definition at line 63
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::EVALCTRL |
LESENSE Evaluation Control
Definition at line 54
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IDLECONF |
GPIO Idle Phase Configuration
Definition at line 65
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IEN |
Interrupt Enable Register
Definition at line 71
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::IF |
Interrupt Flag Register
Definition at line 68
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 70
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 69
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::PERCTRL |
Peripheral Control Register
Definition at line 51
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::PRSCTRL |
PRS Control Register
Definition at line 55
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::PTR |
Result Buffer Pointers
Definition at line 60
of file efm32jg12b_lesense.h
.
uint32_t LESENSE_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line 67
of file efm32jg12b_lesense.h
.
uint32_t LESENSE_TypeDef::RESERVED1[38U] |
Reserved registers
Definition at line 75
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::ROUTEPEN |
I/O Routing Register
Definition at line 73
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::SCANRES |
Scan Result Register
Definition at line 58
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::SENSORSTATE |
Decoder Input Register
Definition at line 64
of file efm32jg12b_lesense.h
.
LESENSE_ST_TypeDef LESENSE_TypeDef::ST[32U] |
Decoding states
Definition at line 76
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::STATUS |
Status Register
Definition at line 59
of file efm32jg12b_lesense.h
.
__IM uint32_t LESENSE_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 72
of file efm32jg12b_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::TIMCTRL |
Timing Control Register
Definition at line 50
of file efm32jg12b_lesense.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_lesense.h