EZRADIODRV_DirectTxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Direct_Transmit_Plugin
EzRadio direct tx plug-in instance initialization and handler structure.
Definition at line 50
of file ezradio_direct_transmit_plugin.h
.
#include <
ezradio_direct_transmit_plugin.h
>
Data Fields | |
uint8_t | channel |
Direct transmit channel. | |
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emdrv/ezradiodrv/plugins/inc/
ezradio_direct_transmit_plugin.h