PCNT_TypeDef Struct ReferenceDevices > PCNT
PCNT Register Declaration
Definition at line 48
of file efm32jg12b_pcnt.h
.
#include <
efm32jg12b_pcnt.h
>
Data Fields | |
__IM uint32_t | AUXCNT |
__IOM uint32_t | CMD |
__IM uint32_t | CNT |
__IOM uint32_t | CTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INPUT |
__IOM uint32_t | OVSCFG |
uint32_t | RESERVED0 [1U] |
uint32_t | RESERVED1 [4U] |
uint32_t | RESERVED2 [7U] |
__IOM uint32_t | ROUTELOC0 |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IM uint32_t | TOP |
__IOM uint32_t | TOPB |
Field Documentation
__IM uint32_t PCNT_TypeDef::AUXCNT |
Auxiliary Counter Value Register
Definition at line 67
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_AuxCounterGet().
__IOM uint32_t PCNT_TypeDef::CMD |
Command Register
Definition at line 50
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_CounterTopSet(), PCNT_Init(), and PCNT_TopSet().
__IM uint32_t PCNT_TypeDef::CNT |
Counter Value Register
Definition at line 52
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_CounterGet().
__IOM uint32_t PCNT_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_CounterReset(), PCNT_CounterTopSet(), PCNT_Enable(), PCNT_FilterConfiguration(), PCNT_Init(), PCNT_Reset(), and PCNT_TCCConfiguration().
__IOM uint32_t PCNT_TypeDef::FREEZE |
__IOM uint32_t PCNT_TypeDef::IEN |
Interrupt Enable Register
Definition at line 58
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_IntDisable(), PCNT_IntEnable(), PCNT_IntGetEnabled(), and PCNT_Reset().
__IM uint32_t PCNT_TypeDef::IF |
Interrupt Flag Register
Definition at line 55
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_IntGet(), and PCNT_IntGetEnabled().
__IOM uint32_t PCNT_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 57
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_IntClear(), and PCNT_Reset().
__IOM uint32_t PCNT_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 56
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_IntSet().
__IOM uint32_t PCNT_TypeDef::INPUT |
PCNT Input Register
Definition at line 68
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_Init(), and PCNT_PRSInputEnable().
__IOM uint32_t PCNT_TypeDef::OVSCFG |
Oversampling Config Register
Definition at line 69
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_FilterConfiguration().
uint32_t PCNT_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line 59
of file efm32jg12b_pcnt.h
.
uint32_t PCNT_TypeDef::RESERVED1[4U] |
Reserved for future use
Definition at line 62
of file efm32jg12b_pcnt.h
.
uint32_t PCNT_TypeDef::RESERVED2[7U] |
Reserved for future use
Definition at line 66
of file efm32jg12b_pcnt.h
.
__IOM uint32_t PCNT_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 60
of file efm32jg12b_pcnt.h
.
__IM uint32_t PCNT_TypeDef::STATUS |
Status Register
Definition at line 51
of file efm32jg12b_pcnt.h
.
__IM uint32_t PCNT_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 64
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_FreezeEnable().
__IM uint32_t PCNT_TypeDef::TOP |
Top Value Register
Definition at line 53
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_CounterSet(), and PCNT_TopGet().
__IOM uint32_t PCNT_TypeDef::TOPB |
Top Value Buffer Register
Definition at line 54
of file efm32jg12b_pcnt.h
.
Referenced by PCNT_CounterTopSet(), PCNT_Init(), PCNT_TopBufferGet(), PCNT_TopBufferSet(), and PCNT_TopSet().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFM32JG12B/Include/
efm32jg12b_pcnt.h