sl_sleeptimer_timer_handle Struct ReferenceEMDRV > SLEEPTIMER
Definition at line 66
of file sleeptimer.h
.
Data Fields | |
sl_sleeptimer_timer_callback_t | callback |
Function to call when timer expires. | |
void * | callback_data |
User data to pass to callback function. | |
uint32_t | delta |
Delay relative to previous element in list. | |
sl_sleeptimer_timer_handle_t * | next |
Pointer to next element in list. | |
uint8_t | priority |
Priority of timer. | |
uint32_t | timeout_periodic |
Periodic timeout. | |
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emdrv/sleeptimer/inc/
sleeptimer.h