API for STKs and WSTKs
Data Structures |
|
| struct | BCP_Packet |
|
BCP Packet Structure - Board controller communication protocol version 2.
|
|
| struct | BCP_Packet_ |
|
BCP Packet Structure - Board controller communication protocol version 1.
|
|
| struct | BCP_PacketHeader |
|
BCP Packet Header definition.
|
|
Macros |
|
| #define | BSP_BCP_ACK 5 |
| #define | BSP_BCP_CURRENT_REPLY 16 |
| #define | BSP_BCP_CURRENT_REQ 14 |
| #define | BSP_BCP_ECHO_REPLY 11 |
| #define | BSP_BCP_ECHO_REQ 10 |
| #define | BSP_BCP_ENERGYMODE 22 |
| #define | BSP_BCP_FIRST 1 |
| #define | BSP_BCP_INVALID 0 |
| #define | BSP_BCP_LAST 100 |
| #define | BSP_BCP_MAGIC 0xF1 |
| #define | BSP_BCP_NET_REPLY 65 |
| #define | BSP_BCP_NET_REQUEST 64 |
| #define | BSP_BCP_PACKET_SIZe 30 |
| #define | BSP_BCP_PACKET_SIZE 132 |
| #define | BSP_BCP_STDERR 26 |
| #define | BSP_BCP_STDOUT 24 |
| #define | BSP_BCP_TEST 32 |
| #define | BSP_BCP_TEST_REPLY 33 |
| #define | BSP_BCP_VOLTAGE_REPLY 20 |
| #define | BSP_BCP_VOLTAGE_REQ 18 |
Enumerations |
|
| enum |
BSP_Peripheral_TypeDef
{
BSP_RS232_SHUTDOWN , BSP_RS232_UART , BSP_RS232_LEUART , BSP_I2C , BSP_ETH , BSP_I2S , BSP_TRACE , BSP_TOUCH , BSP_AUDIO_IN , BSP_AUDIO_OUT , BSP_ANALOG_DIFF , BSP_ANALOG_SE , BSP_MICROSD , BSP_TFT , BSP_IOEXP_LEDS , BSP_IOEXP_SENSORS , BSP_IOEXP_DISPLAY , BSP_IOEXP_VCOM , BSP_VCOM } |
Functions |
|
| int | BSP_BccDeInit (void) |
|
Deinitialize board controller communication support (BCC) functionality. Reverse actions performed by
BSP_BccInit()
.
|
|
| int | BSP_BccInit (void) |
|
Initialize board controller communication support (BCC) functionality.
|
|
| bool | BSP_BccPacketReceive ( BCP_Packet *pkt) |
|
Get a packet from the board controller.
|
|
| int | BSP_BccPacketSend ( BCP_Packet *pkt) |
|
Send a packet to the board controller.
|
|
| void | BSP_BccPinsEnable (bool enable) |
|
Enable GPIO pins for the USART/LEUART used for board communication.
|
|
| float | BSP_CurrentGet (void) |
|
Request AEM (Advanced Energy Monitoring) current from board controller.
|
|
| int | BSP_EbiDeInit (void) |
|
Deinitialize the EBI interface for accessing the onboard nandflash.
|
|
| int | BSP_EbiInit (void) |
|
Initialize the EBI interface for accessing the onboard nandflash.
|
|
| uint32_t | BSP_IOExpGetDeviceId (void) |
|
Get IO Expander Device id.
|
|
| float | BSP_VoltageGet (void) |
|
Request AEM (Advanced Energy Monitoring) voltage from board controller.
|
|
Macro Definition Documentation
| #define BSP_BCP_ACK 5 |
Generic ACK for one way packages
Definition at line
59
of file
bsp_bcp.h
.
| #define BSP_BCP_CURRENT_REPLY 16 |
| #define BSP_BCP_CURRENT_REQ 14 |
EFM32 Request AEM current
Definition at line
62
of file
bsp_bcp.h
.
Referenced by BSP_CurrentGet() .
| #define BSP_BCP_ECHO_REPLY 11 |
BC alive response
Definition at line
61
of file
bsp_bcp.h
.
| #define BSP_BCP_ECHO_REQ 10 |
EFM32 BC alive request
Definition at line
60
of file
bsp_bcp.h
.
| #define BSP_BCP_ENERGYMODE 22 |
EFM32 Report Energy Mode (for AEM)
Definition at line
66
of file
bsp_bcp.h
.
| #define BSP_BCP_FIRST 1 |
Smallest numerical value of message type
Definition at line
57
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() .
| #define BSP_BCP_INVALID 0 |
Invalid packet received
Definition at line
55
of file
bsp_bcp.h
.
| #define BSP_BCP_LAST 100 |
Last defined message type
Definition at line
74
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() .
| #define BSP_BCP_MAGIC 0xF1 |
Magic byte to indicate start of packet
Definition at line
76
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() , and BSP_BccPacketSend() .
| #define BSP_BCP_NET_REPLY 65 |
Net gateway reply packet
Definition at line
72
of file
bsp_bcp.h
.
| #define BSP_BCP_NET_REQUEST 64 |
Net gateway request packet
Definition at line
71
of file
bsp_bcp.h
.
| #define BSP_BCP_PACKET_SIZe 30 |
Max packet size for version 1 of the protocol.
Definition at line
82
of file
bsp_bcp.h
.
| #define BSP_BCP_PACKET_SIZE 132 |
Max packet size for version 2 of the protocol.
Definition at line
102
of file
bsp_bcp.h
.
Referenced by BSP_BccPacketReceive() .
| #define BSP_BCP_STDERR 26 |
Debug packet (not used)
Definition at line
68
of file
bsp_bcp.h
.
| #define BSP_BCP_STDOUT 24 |
Debug packet (not used)
Definition at line
67
of file
bsp_bcp.h
.
| #define BSP_BCP_TEST 32 |
Reserved type for test
Definition at line
69
of file
bsp_bcp.h
.
| #define BSP_BCP_TEST_REPLY 33 |
Reserved type for test (reply)
Definition at line
70
of file
bsp_bcp.h
.
| #define BSP_BCP_VOLTAGE_REPLY 20 |
| #define BSP_BCP_VOLTAGE_REQ 18 |
EFM32 Request AEM voltage
Definition at line
64
of file
bsp_bcp.h
.
Referenced by BSP_VoltageGet() .
Enumeration Type Documentation
Peripherals control structure for STK's, WSTK's and similar.
Definition at line
160
of file
bsp.h
.
Function Documentation
| int BSP_BccDeInit | ( | void |
|
) |
Deinitialize board controller communication support (BCC) functionality. Reverse actions performed by BSP_BccInit() .
- Returns
- BSP_STATUS_OK .
Definition at line
74
of file
bsp_bcc.c
.
References BSP_BccPinsEnable() , BSP_STATUS_OK , CMU_ClockEnable() , LEUART_Reset() , and USART_Reset() .
| int BSP_BccInit | ( | void |
|
) |
Initialize board controller communication support (BCC) functionality.
- Returns
- BSP_STATUS_OK .
Definition at line
102
of file
bsp_bcc.c
.
References LEUART_Init_TypeDef::baudrate , BSP_BccPinsEnable() , BSP_STATUS_OK , CMU_ClockEnable() , CMU_ClockSelectSet() , cmuClock_GPIO , cmuClock_HFPER , cmuClock_LFB , LEUART_Init() , LEUART_INIT_DEFAULT , USART_InitAsync() , and USART_INITASYNC_DEFAULT .
| bool BSP_BccPacketReceive | ( | BCP_Packet * |
pkt
|
) |
Get a packet from the board controller.
- Parameters
-
[in] pktPointer to a BCP_Packet instance.
- Returns
- True if packet received without errors, false otherwise.
Definition at line
152
of file
bsp_bcc.c
.
References BSP_BCP_FIRST , BSP_BCP_LAST , BSP_BCP_MAGIC , BSP_BCP_PACKET_SIZE , BCP_Packet::magic , BCP_Packet::payloadLength , and BCP_Packet::type .
Referenced by BSP_CurrentGet() , and BSP_VoltageGet() .
| int BSP_BccPacketSend | ( | BCP_Packet * |
pkt
|
) |
Send a packet to the board controller.
- Parameters
-
[in] pktPointer to a BCP_Packet instance.
- Returns
- BSP_STATUS_OK .
Definition at line
205
of file
bsp_bcc.c
.
References BSP_BCP_MAGIC , BSP_STATUS_OK , BCP_Packet::data , BCP_Packet::magic , BCP_Packet::payloadLength , BCP_Packet::reserved , and BCP_Packet::type .
Referenced by BSP_CurrentGet() , and BSP_VoltageGet() .
| void BSP_BccPinsEnable | ( | bool |
enable
|
) |
Enable GPIO pins for the USART/LEUART used for board communication.
- Parameters
-
[in] enableSet to true to enable pins, set to false to disable.
Definition at line
239
of file
bsp_bcc.c
.
References GPIO_PinModeSet() , gpioModeDisabled , gpioModeInput , and gpioModePushPull .
Referenced by BSP_BccDeInit() , and BSP_BccInit() .
| float BSP_CurrentGet | ( | void |
|
) |
Request AEM (Advanced Energy Monitoring) current from board controller.
- Note
- Assumes that BSP_Init() has been called with BSP_INIT_BCC bitmask.
- Returns
- The current expressed in milliamperes. Returns 0.0 on board controller communication error.
Definition at line
357
of file
bsp_stk.c
.
References BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_BCP_CURRENT_REPLY , BSP_BCP_CURRENT_REQ , BCP_Packet::data , BCP_Packet::payloadLength , and BCP_Packet::type .
| int BSP_EbiDeInit | ( | void |
|
) |
Deinitialize the EBI interface for accessing the onboard nandflash.
- Note
- This function is not relevant for Gxxx_STK's. This function is provided for API completeness, it does not perform an actual EBI deinitialization.
- Returns
- BSP_STATUS_OK or BSP_STATUS_NOT_IMPLEMENTED
Definition at line
178
of file
bsp_stk.c
.
References BSP_STATUS_NOT_IMPLEMENTED , and BSP_STATUS_OK .
| int BSP_EbiInit | ( | void |
|
) |
Initialize the EBI interface for accessing the onboard nandflash.
- Note
- This function is not relevant for Gxxx_STK's.
- Returns
- BSP_STATUS_OK or BSP_STATUS_NOT_IMPLEMENTED
Definition at line
85
of file
bsp_stk.c
.
References BSP_STATUS_NOT_IMPLEMENTED , BSP_STATUS_OK , CMU_ClockEnable() , cmuClock_EBI , cmuClock_GPIO , cmuClock_HFPER , EBI_BANK0 , EBI_Init() , ebiActiveLow , ebiModeD8A8 , GPIO_PinModeSet() , gpioModeInput , and gpioModePushPull .
| uint32_t BSP_IOExpGetDeviceId | ( | void |
|
) |
Get IO Expander Device id.
- Returns
- The device id of a connected IO Expander Device id or 0 if no IO expander is connected.
Definition at line
194
of file
bsp_stk.c
.
| float BSP_VoltageGet | ( | void |
|
) |
Request AEM (Advanced Energy Monitoring) voltage from board controller.
- Note
- Assumes that BSP_Init() has been called with BSP_INIT_BCC bitmask.
- Returns
- The voltage. Returns 0.0 on board controller communication error.
Definition at line
392
of file
bsp_stk.c
.
References BSP_BccPacketReceive() , BSP_BccPacketSend() , BSP_BCP_VOLTAGE_REPLY , BSP_BCP_VOLTAGE_REQ , BCP_Packet::data , BCP_Packet::payloadLength , and BCP_Packet::type .