VCMP
Detailed Description
Voltage Comparator (VCMP) Peripheral API.
This module contains functions to control the VCMP peripheral of Silicon Labs 32-bit MCUs and SoCs. The VCMP monitors the input voltage supply and generates interrupts on events using as little as 100 nA.
Data Structures |
|
| struct | VCMP_Init_TypeDef |
Macros |
|
| #define | VCMP_INIT_DEFAULT |
Enumerations |
|
| enum |
VCMP_Hysteresis_TypeDef
{
vcmpHystNone , vcmpHyst20mV } |
| enum |
VCMP_WarmTime_TypeDef
{
vcmpWarmTime4Cycles = _VCMP_CTRL_WARMTIME_4CYCLES, vcmpWarmTime8Cycles = _VCMP_CTRL_WARMTIME_8CYCLES, vcmpWarmTime16Cycles = _VCMP_CTRL_WARMTIME_16CYCLES, vcmpWarmTime32Cycles = _VCMP_CTRL_WARMTIME_32CYCLES, vcmpWarmTime64Cycles = _VCMP_CTRL_WARMTIME_64CYCLES, vcmpWarmTime128Cycles = _VCMP_CTRL_WARMTIME_128CYCLES, vcmpWarmTime256Cycles = _VCMP_CTRL_WARMTIME_256CYCLES, vcmpWarmTime512Cycles = _VCMP_CTRL_WARMTIME_512CYCLES } |
Functions |
|
| __STATIC_INLINE void | VCMP_Disable (void) |
|
Disable Voltage Comparator.
|
|
| __STATIC_INLINE void | VCMP_Enable (void) |
|
Enable Voltage Comparator.
|
|
| void | VCMP_Init (const VCMP_Init_TypeDef *vcmpInit) |
|
Configure and enable Voltage Comparator.
|
|
| __STATIC_INLINE void | VCMP_IntClear (uint32_t flags) |
|
Clear one or more pending VCMP interrupts.
|
|
| __STATIC_INLINE void | VCMP_IntDisable (uint32_t flags) |
|
Disable one or more VCMP interrupts.
|
|
| __STATIC_INLINE void | VCMP_IntEnable (uint32_t flags) |
|
Enable one or more VCMP interrupts.
|
|
| __STATIC_INLINE uint32_t | VCMP_IntGet (void) |
|
Get pending VCMP interrupt flags.
|
|
| __STATIC_INLINE uint32_t | VCMP_IntGetEnabled (void) |
|
Get enabled and pending VCMP interrupt flags.
|
|
| __STATIC_INLINE void | VCMP_IntSet (uint32_t flags) |
|
Set one or more pending VCMP interrupts from SW.
|
|
| void | VCMP_LowPowerRefSet (bool enable) |
|
Enable or disable Low Power Reference setting.
|
|
| __STATIC_INLINE bool | VCMP_Ready (void) |
|
VCMP output is ready.
|
|
| void | VCMP_TriggerSet (int level) |
|
Configure the trigger level of the voltage comparator.
|
|
| __STATIC_INLINE bool | VCMP_VDDHigher (void) |
|
Returns true if Voltage Comparator indicated VDD > trigger level, else returns false.
|
|
| __STATIC_INLINE bool | VCMP_VDDLower (void) |
|
Returns true if Voltage Comparator indicated VDD < trigger level, else returns false.
|
|
| __STATIC_INLINE uint32_t | VCMP_VoltageToLevel (float v) |
|
Calculate voltage to trigger level.
|
|
Macro Definition Documentation
| #define VCMP_INIT_DEFAULT |
Default VCMP initialization structure.
Definition at line
118
of file
em_vcmp.h
.
Referenced by VDDCHECK_LowVoltage() .
Enumeration Type Documentation
Warm-up Time in High Frequency Peripheral Clock cycles.
Definition at line
59
of file
em_vcmp.h
.
Function Documentation
| void VCMP_Init | ( | const VCMP_Init_TypeDef * |
vcmpInit
|
) |
Configure and enable Voltage Comparator.
- Parameters
-
[in] vcmpInitThe VCMP Initialization structure.
Definition at line
58
of file
em_vcmp.c
.
References VCMP_Init_TypeDef::biasProg , VCMP_Init_TypeDef::enable , VCMP_Init_TypeDef::halfBias , VCMP_Init_TypeDef::hyst , VCMP_Init_TypeDef::inactive , VCMP_Init_TypeDef::irqFalling , VCMP_Init_TypeDef::irqRising , VCMP_Init_TypeDef::lowPowerRef , VCMP_Init_TypeDef::triggerLevel , VCMP_IntClear() , VCMP_LowPowerRefSet() , VCMP_Ready() , VCMP_TriggerSet() , vcmpHyst20mV , vcmpHystNone , and VCMP_Init_TypeDef::warmup .
Referenced by VDDCHECK_LowVoltage() .
| __STATIC_INLINE void VCMP_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending VCMP interrupts.
- Parameters
-
[in] flagsVCMP interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
Definition at line
223
of file
em_vcmp.h
.
Referenced by VCMP_Init() .
| __STATIC_INLINE void VCMP_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more VCMP interrupts.
- Parameters
-
[in] flagsVCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
Definition at line
251
of file
em_vcmp.h
.
| __STATIC_INLINE void VCMP_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more VCMP interrupts.
- Parameters
-
[in] flagsVCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
Definition at line
265
of file
em_vcmp.h
.
| __STATIC_INLINE uint32_t VCMP_IntGet | ( | void |
|
) |
Get pending VCMP interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending VCMP interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the VCMP module (VCMP_IFS_nnn).
Definition at line
281
of file
em_vcmp.h
.
| __STATIC_INLINE uint32_t VCMP_IntGetEnabled | ( | void |
|
) |
Get enabled and pending VCMP interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- The event bits are not cleared by the use of this function.
- Returns
-
Pending and enabled VCMP interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in VCMP_IEN_nnn register (VCMP_IEN_nnn) and
- the OR combination of valid interrupt flags of the VCMP module (VCMP_IF_nnn).
Definition at line
304
of file
em_vcmp.h
.
| __STATIC_INLINE void VCMP_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending VCMP interrupts from SW.
- Parameters
-
[in] flagsVCMP interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
Definition at line
237
of file
em_vcmp.h
.
| void VCMP_LowPowerRefSet | ( | bool |
enable
|
) |
Enable or disable Low Power Reference setting.
- Parameters
-
[in] enableIf true, enables low power reference. If false, disable low power reference.
Definition at line
138
of file
em_vcmp.c
.
Referenced by VCMP_Init() .
| void VCMP_TriggerSet | ( | int |
level
|
) |
Configure the trigger level of the voltage comparator.
- Parameters
-
[in] levelA trigger value, in range 0-63.
Definition at line
154
of file
em_vcmp.c
.
Referenced by VCMP_Init() .
| __STATIC_INLINE uint32_t VCMP_VoltageToLevel | ( | float |
v
|
) |
Calculate voltage to trigger level.
- Note
- Soft float support is needed for this function to work.
- Parameters
-
[in] vVoltage Level for trigger.
Definition at line
168
of file
em_vcmp.h
.
Referenced by VDDCHECK_LowVoltage() .