COMMON
Detailed Description
General purpose utilities and cross-compiler support.
This SDK supports the following compilers/IDEs:
- Simplicity Studio
- IAR Embedded Workbench
- Keil µVision IDE
- Plain armgcc
Certain compiler features such as alignment is implemented differently in the tools. Therefore, macros such as SL_ALIGN are provided to enable compiler independent code.
- Note
- RAM code macros are implemented in a separate module RAMFUNC. Cross-compiler RAM code support needs extended documentation and it is therefore implemented as a separate module.
Macros | |
#define | SL_ALIGN(X) |
A macro for aligning a variable. Use this macro before the variable definition. X denotes the storage alignment value in bytes. To be GCC-compatible, use SL_ATTRIBUTE_ALIGN(X) before the semicolon on normal variables. Use SL_ATTRIBUTE_ALIGN(X) before the opening curly brace on structure variables. | |
#define | SL_ATTRIBUTE_ALIGN(X) __attribute__ ((aligned(X))) |
GCC style macro for aligning a variable. | |
#define | SL_ATTRIBUTE_PACKED __attribute__ ((packed)) |
A GCC style macro for handling packed structures. | |
#define | SL_ATTRIBUTE_SECTION(X) __attribute__ ((section(X))) |
#define | SL_CEILING(n, i) ((((n) + (i) - 1U) / (i)) * (i)) |
Round n up to closest interval of i. | |
#define | SL_FALLTHROUGH |
A macro for notifying the compiler of an intended switch case fallthrough. | |
#define | SL_FLOOR(n, i) ((n / i) * i)) |
Round n down to closest interval of i. | |
#define | SL_MAX(a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a > _b ? _a : _b; }) |
A macro for getting the maximum value. No sideeffects, a and b are evaluated one time only. | |
#define | SL_MIN(a, b) __extension__({ __typeof__(a)_a = (a); __typeof__(b)_b = (b); _a < _b ? _a : _b; }) |
A macro for getting the minimum value. No sideeffects, a and b are evaluated one time only. | |
#define | SL_NORETURN __attribute__ ((noreturn)) |
A macro for handling non-returning functions. | |
#define | SL_PACK_END() |
A macro for handling packed structures. Use this macro after the structure definition. With GCC, add SL_ATTRIBUTE_PACKED after the closing curly braces of the structure definition. | |
#define | SL_PACK_START(x) |
A macro for handling packed structures. Use this macro before the structure definition. X denotes the maximum alignment of structure members. X is not supported with GCC. GCC always uses 1 byte maximum alignment. | |
#define | SL_WEAK __attribute__ ((weak)) |
A macro for defining a weak symbol. | |
#define | STRINGIZE(X) #X |
Stringify X. | |
Functions | |
__STATIC_INLINE uint32_t | EFM32_CTZ (uint32_t value) |
__STATIC_INLINE uint32_t | SL_CTZ (uint32_t value) |
Count trailing number of zeros. Use CLZ instruction if available. | |
__STATIC_INLINE uint32_t | SL_Log2ToDiv (uint32_t log2) |
Convert logarithm of 2 to division factor. | |
__STATIC_INLINE uint32_t | SL_RBIT (uint32_t value) |
Reverse the bits. Use the RBIT instruction if available, else process. | |
__STATIC_INLINE uint32_t | SL_RBIT16 (uint32_t value) |
Reverse the bits. Use the RBIT instruction if available, else process. | |
Macro Definition Documentation
#define SL_ATTRIBUTE_SECTION | ( | X | ) | __attribute__ ((section(X))) |
A macro for placing a variable in a section.
Use this macro after the variable definition, before the equal sign or a semicolon.
X denotes the section to place the variable in.
Definition at line 200
of file em_common.h
.
Function Documentation
__STATIC_INLINE uint32_t SL_CTZ | ( | uint32_t | value | ) |
Count trailing number of zeros. Use CLZ instruction if available.
- Parameters
-
[in] value
Data value to check for number of trailing zero bits.
- Returns
- A number of trailing zeros in value.
Definition at line 222
of file em_common.h
.
Referenced by GPIOINT_CallbackRegister(), and RMU_ResetControl().
__STATIC_INLINE uint32_t SL_Log2ToDiv | ( | uint32_t | log2 | ) |
Convert logarithm of 2 to division factor.
- Parameters
-
[in] log2
Logarithm of 2.
- Returns
- Dividend.
Definition at line 297
of file em_common.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockFreqGet(), and CMU_Log2ToDiv().
__STATIC_INLINE uint32_t SL_RBIT | ( | uint32_t | value | ) |
Reverse the bits. Use the RBIT instruction if available, else process.
- Parameters
-
[in] value
Data value to reverse.
- Returns
- A reversed value.
Definition at line 252
of file em_common.h
.
Referenced by SL_RBIT16().
__STATIC_INLINE uint32_t SL_RBIT16 | ( | uint32_t | value | ) |
Reverse the bits. Use the RBIT instruction if available, else process.
- Parameters
-
[in] value
16-bit data value to reverse.
- Returns
- A 16-bit reversed value.
Definition at line 282
of file em_common.h
.
References SL_RBIT().