HALL - Hall Effect Sensor
Detailed Description
Driver for Hall effect sensor.
Modules | |
Si7210 - Hall Effect Sensor | |
Driver for the Silicon Labs Si7210 Hall effect sensor. | |
Data Structures | |
struct | __HALL_Config |
Structure to configure the Hall effect sensor device. | |
Typedefs | |
typedef struct __HALL_Config | HALL_Config |
Structure to configure the Hall effect sensor device. | |
typedef void(* | HALL_IntCallback) (bool pinHigh) |
Functions | |
uint32_t | HALL_configure (HALL_Config *config) |
Configures the Si7210 chip. | |
void | HALL_deInit (void) |
De-initializes the Hall sensor. Disables the sensor power domain. | |
uint32_t | HALL_deInitDevice (void) |
Does device-specific de-initializaiton for the Si7210 chip. | |
float | HALL_getTamperLevel (void) |
Returns the tamper level configured in the chip. | |
uint32_t | HALL_init (void) |
Initializes the Hall sensor. | |
uint32_t | HALL_initDevice (void) |
Does device-specific initializaiton for the Si7210 chip. | |
uint32_t | HALL_measure (uint32_t scale, float *result) |
Performs a measurement. | |
void | HALL_registerCallback (HALL_IntCallback callback) |
Register GPIO interrupt callback function. This function will be called when the ALERT pin of the Hall sensor changes state and the interrupt functions are enabled. | |
Error Codes | |
#define | HALL_OK 0x0000 |
#define | HALL_ERROR_DRIVER_NOT_INITIALIZED 0x0001 |
#define | HALL_ERROR_I2C_TRANSACTION_FAILED 0x0002 |
#define | HALL_ERROR_DEVICE_ID_MISMATCH 0x0003 |
Configuration values | |
#define | HALL_CONFIG_POLARITY_OMNIPOLAR 0x00 |
#define | HALL_CONFIG_POLARITY_NEGATIVE 0x01 |
#define | HALL_CONFIG_POLARITY_POSITIVE 0x02 |
Macro Definition Documentation
#define HALL_CONFIG_POLARITY_NEGATIVE 0x01 |
Negative field polarity
Definition at line 59
of file hall.h
.
#define HALL_CONFIG_POLARITY_OMNIPOLAR 0x00 |
Omnipolar field polarity
Definition at line 58
of file hall.h
.
#define HALL_CONFIG_POLARITY_POSITIVE 0x02 |
Positive field polarity
Definition at line 60
of file hall.h
.
#define HALL_ERROR_DEVICE_ID_MISMATCH 0x0003 |
The device ID does not match the expected value
Definition at line 51
of file hall.h
.
Referenced by HALL_initDevice().
#define HALL_ERROR_DRIVER_NOT_INITIALIZED 0x0001 |
The driver is not initialized
Definition at line 49
of file hall.h
.
#define HALL_ERROR_I2C_TRANSACTION_FAILED 0x0002 |
I2C transaction failed
Definition at line 50
of file hall.h
.
Referenced by SI7210_registerRead(), SI7210_registerWrite(), and SI7210_wakeUp().
#define HALL_OK 0x0000 |
No errors
Definition at line 48
of file hall.h
.
Referenced by HALL_configure(), HALL_initDevice(), SI7210_loadCoeffsFromOtp(), SI7210_regClearBits(), SI7210_registerRead(), SI7210_registerWrite(), SI7210_regReadOTP(), SI7210_regSetBits(), and SI7210_wakeUp().
Typedef Documentation
typedef void(* HALL_IntCallback) (bool pinHigh) |
Interrupt callback function
Definition at line 74
of file hall.h
.
Function Documentation
uint32_t HALL_configure | ( | HALL_Config * | config | ) |
Configures the Si7210 chip.
- Parameters
-
[in] config
The structure, which contains the configuration parameters. If all fields are set to zero, the chip will revert to use default values.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 120
of file hall_si7210.c
.
References HALL_OK, __HALL_Config::hysteresis, __HALL_Config::outputInvert, __HALL_Config::polarity, SI7210_calculateSWHYST(), SI7210_calculateSWOP(), SI7210_REG_ADDR_CTRL1, SI7210_REG_ADDR_CTRL2, SI7210_REG_ADDR_CTRL3, SI7210_REG_ADDR_POWER_CTRL, SI7210_REG_CTRL1_SW_LOW4FIELD_MASK, SI7210_REG_CTRL1_SW_LOW4FIELD_SHIFT, SI7210_REG_CTRL1_SW_OP_MASK, SI7210_REG_CTRL1_SW_OP_SHIFT, SI7210_REG_CTRL2_SW_FIELDPOLSEL_MASK, SI7210_REG_CTRL2_SW_FIELDPOLSEL_SHIFT, SI7210_REG_CTRL2_SW_HYST_MASK, SI7210_REG_CTRL2_SW_HYST_SHIFT, SI7210_REG_CTRL3_SLTIMEENA_MASK, SI7210_REG_POWER_CTRL_STOP_MASK, SI7210_REG_POWER_CTRL_USESTORE_MASK, SI7210_regClearBits(), SI7210_registerWrite(), SI7210_regSetBits(), SI7210_wakeUp(), and __HALL_Config::threshold.
void HALL_deInit | ( | void |
| ) |
De-initializes the Hall sensor. Disables the sensor power domain.
- Returns
- None
Definition at line 97
of file hall.c
.
References BOARD_hallSensorEnable(), BOARD_hallSensorEnableIRQ(), and HALL_deInitDevice().
uint32_t HALL_deInitDevice | ( | void |
| ) |
Does device-specific de-initializaiton for the Si7210 chip.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 104
of file hall_si7210.c
.
Referenced by HALL_deInit().
float HALL_getTamperLevel | ( | void |
| ) |
Returns the tamper level configured in the chip.
- Returns
- The tamper level in mT
Definition at line 243
of file hall_si7210.c
.
uint32_t HALL_init | ( | void |
| ) |
Initializes the Hall sensor.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 69
of file hall.c
.
References BOARD_hallSensorEnable(), BOARD_hallSensorEnableIRQ(), BOARD_hallSensorSetIRQCallback(), HALL_initDevice(), and UTIL_delay().
uint32_t HALL_initDevice | ( | void |
| ) |
Does device-specific initializaiton for the Si7210 chip.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 71
of file hall_si7210.c
.
References HALL_ERROR_DEVICE_ID_MISMATCH, HALL_OK, SI7210_identify(), and SI7210_wakeUp().
Referenced by HALL_init().
uint32_t HALL_measure | ( | uint32_t | scale, |
float * | result |
||
) |
Performs a measurement.
- Parameters
-
[in] scale
Desired scale in uT [out] result
The measured field strength value in mT
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 217
of file hall_si7210.c
.
References SI7210_readmTDataSltimeena().
void HALL_registerCallback | ( | HALL_IntCallback | callback | ) |
Register GPIO interrupt callback function. This function will be called when the ALERT pin of the Hall sensor changes state and the interrupt functions are enabled.
- Parameters
-
[in] callback
Pointer to the callback function
- Returns
- None
Definition at line 120
of file hall.c
.