State Transitions
Data Structures |
|
| struct | RAIL_StateTransitions_t |
|
Used to specify radio states to transition to on success or failure.
|
|
| struct | RAIL_StateTiming_t |
|
A timing configuration structure for the RAIL State Machine.
|
|
Macros |
|
| #define | RAIL_RF_STATE_DETAIL_INACTIVE (0U) |
|
Radio is inactive.
|
|
| #define | RAIL_RF_STATE_DETAIL_IDLE_STATE (1U << RAIL_RF_STATE_DETAIL_IDLE_STATE_SHIFT) |
|
Radio is in or headed to the idle state.
|
|
| #define | RAIL_RF_STATE_DETAIL_RX_STATE (1U << RAIL_RF_STATE_DETAIL_RX_STATE_SHIFT) |
|
Radio is in or headed to the receive state.
|
|
| #define | RAIL_RF_STATE_DETAIL_TX_STATE (1U << RAIL_RF_STATE_DETAIL_TX_STATE_SHIFT) |
|
Radio is in or headed to the transmit state.
|
|
| #define | RAIL_RF_STATE_DETAIL_TRANSITION (1U << RAIL_RF_STATE_DETAIL_TRANSITION_SHIFT) |
|
Radio is headed to the idle, receive, or transmit state.
|
|
| #define | RAIL_RF_STATE_DETAIL_ACTIVE (1U << RAIL_RF_STATE_DETAIL_ACTIVE_SHIFT) |
|
Radio is actively transmitting or receiving.
|
|
| #define | RAIL_RF_STATE_DETAIL_NO_FRAMES (1U << RAIL_RF_STATE_DETAIL_NO_FRAMES_SHIFT) |
|
Radio has frame detect disabled.
|
|
| #define | RAIL_RF_STATE_DETAIL_LBT (1U << RAIL_RF_STATE_DETAIL_LBT_SHIFT) |
|
LBT/CSMA operation is currently onging.
|
|
| #define | RAIL_RF_STATE_DETAIL_CORE_STATE_MASK |
|
Mask for core radio state bits.
|
|
| #define | RAIL_MINIMUM_TRANSITION_US (100U) |
|
The minimum value for a consistent RAIL transition.
|
|
| #define | RAIL_MAXIMUM_TRANSITION_US (13000U) |
|
The maximum value for a consistent RAIL transition.
|
|
Enumerations |
|
| enum |
RAIL_RadioState_t
{
RAIL_RF_STATE_INACTIVE = 0u, RAIL_RF_STATE_ACTIVE = (1u << 0), RAIL_RF_STATE_RX = (1u << 1), RAIL_RF_STATE_TX = (1u << 2), RAIL_RF_STATE_IDLE = (RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_RX_ACTIVE = (RAIL_RF_STATE_RX | RAIL_RF_STATE_ACTIVE), RAIL_RF_STATE_TX_ACTIVE = (RAIL_RF_STATE_TX | RAIL_RF_STATE_ACTIVE) } |
|
The state of the radio.
|
|
| enum |
RAIL_RadioStateDetail_t
{
RAIL_RF_STATE_DETAIL_IDLE_STATE_SHIFT = 0u, RAIL_RF_STATE_DETAIL_RX_STATE_SHIFT , RAIL_RF_STATE_DETAIL_TX_STATE_SHIFT , RAIL_RF_STATE_DETAIL_TRANSITION_SHIFT , RAIL_RF_STATE_DETAIL_ACTIVE_SHIFT , RAIL_RF_STATE_DETAIL_NO_FRAMES_SHIFT , RAIL_RF_STATE_DETAIL_LBT_SHIFT } |
|
The detailed state of the radio.
|
|
| enum |
RAIL_IdleMode_t
{
RAIL_IDLE , RAIL_IDLE_ABORT , RAIL_IDLE_FORCE_SHUTDOWN , RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS } |
|
An enumeration for the different types of supported idle modes.
|
|
Functions |
|
| RAIL_Status_t | RAIL_SetRxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
|
Configure RAIL automatic state transitions after RX.
|
|
| RAIL_Status_t | RAIL_GetRxTransitions ( RAIL_Handle_t railHandle, RAIL_StateTransitions_t *transitions) |
|
Get the current RAIL automatic state transitions after RX.
|
|
| RAIL_Status_t | RAIL_SetTxTransitions ( RAIL_Handle_t railHandle, const RAIL_StateTransitions_t *transitions) |
|
Configure RAIL automatic state transitions after TX.
|
|
| RAIL_Status_t | RAIL_GetTxTransitions ( RAIL_Handle_t railHandle, RAIL_StateTransitions_t *transitions) |
|
Get the current RAIL automatic state transitions after TX.
|
|
| RAIL_Status_t | RAIL_SetStateTiming ( RAIL_Handle_t railHandle, RAIL_StateTiming_t *timings) |
|
Configure RAIL automatic state transition timing.
|
|
| void | RAIL_Idle ( RAIL_Handle_t railHandle, RAIL_IdleMode_t mode, bool wait) |
|
Place the radio into an idle state.
|
|
| RAIL_RadioState_t | RAIL_GetRadioState ( RAIL_Handle_t railHandle) |
|
Get the current radio state.
|
|
| RAIL_RadioStateDetail_t | RAIL_GetRadioStateDetail ( RAIL_Handle_t railHandle) |
|
Get the detailed current radio state.
|
|
Macro Definition Documentation
◆ RAIL_MINIMUM_TRANSITION_US
| #define RAIL_MINIMUM_TRANSITION_US (100U) |
The minimum value for a consistent RAIL transition.
- Note
- Transitions may need to be slower than this when using longer RAIL_TxPowerConfig_t::rampTime values
Definition at line
1874
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_ACTIVE
| #define RAIL_RF_STATE_DETAIL_ACTIVE (1U << RAIL_RF_STATE_DETAIL_ACTIVE_SHIFT) |
Radio is actively transmitting or receiving.
Definition at line
1858
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_CORE_STATE_MASK
| #define RAIL_RF_STATE_DETAIL_CORE_STATE_MASK |
rail_types.h:1854
rail_types.h:1852
rail_types.h:1850
Mask for core radio state bits.
Definition at line
1864
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_IDLE_STATE
| #define RAIL_RF_STATE_DETAIL_IDLE_STATE (1U << RAIL_RF_STATE_DETAIL_IDLE_STATE_SHIFT) |
Radio is in or headed to the idle state.
Definition at line
1850
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_INACTIVE
| #define RAIL_RF_STATE_DETAIL_INACTIVE (0U) |
Radio is inactive.
Definition at line
1848
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_LBT
| #define RAIL_RF_STATE_DETAIL_LBT (1U << RAIL_RF_STATE_DETAIL_LBT_SHIFT) |
LBT/CSMA operation is currently onging.
Definition at line
1862
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_NO_FRAMES
| #define RAIL_RF_STATE_DETAIL_NO_FRAMES (1U << RAIL_RF_STATE_DETAIL_NO_FRAMES_SHIFT) |
Radio has frame detect disabled.
Definition at line
1860
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_RX_STATE
| #define RAIL_RF_STATE_DETAIL_RX_STATE (1U << RAIL_RF_STATE_DETAIL_RX_STATE_SHIFT) |
Radio is in or headed to the receive state.
Definition at line
1852
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_TRANSITION
| #define RAIL_RF_STATE_DETAIL_TRANSITION (1U << RAIL_RF_STATE_DETAIL_TRANSITION_SHIFT) |
Radio is headed to the idle, receive, or transmit state.
Definition at line
1856
of file
rail_types.h
.
◆ RAIL_RF_STATE_DETAIL_TX_STATE
| #define RAIL_RF_STATE_DETAIL_TX_STATE (1U << RAIL_RF_STATE_DETAIL_TX_STATE_SHIFT) |
Radio is in or headed to the transmit state.
Definition at line
1854
of file
rail_types.h
.
Enumeration Type Documentation
◆ RAIL_IdleMode_t
| enum RAIL_IdleMode_t |
An enumeration for the different types of supported idle modes.
These vary how quickly and destructively they put the radio into idle.
| Enumerator | |
|---|---|
| RAIL_IDLE |
Idle the radio by turning off receive and canceling any future scheduled receive or transmit operations. It does not abort a receive or transmit in progress. |
| RAIL_IDLE_ABORT |
Idle the radio by turning off receive and any scheduled events. It also aborts any receive, transmit, or scheduled events in progress. |
| RAIL_IDLE_FORCE_SHUTDOWN |
Force the radio into a shutdown mode by stopping whatever state is in progress. This is a more destructive shutdown than RAIL_IDLE or RAIL_IDLE_ABORT and can be useful in certain situations when directed by the support team or for debugging. Note that this method may corrupt receive and transmit buffers so it requires a more thorough cleanup and any held packets will be lost. |
| RAIL_IDLE_FORCE_SHUTDOWN_CLEAR_FLAGS |
Similar to the RAIL_IDLE_FORCE_SHUTDOWN command, however, it will also clear any pending RAIL events related to receive and transmit. |
Definition at line
1918
of file
rail_types.h
.
◆ RAIL_RadioState_t
| enum RAIL_RadioState_t |
The state of the radio.
Definition at line
1764
of file
rail_types.h
.
◆ RAIL_RadioStateDetail_t
The detailed state of the radio.
The three radio state bits RAIL_RF_STATE_DETAIL_IDLE_STATE , RAIL_RF_STATE_DETAIL_RX_STATE , and RAIL_RF_STATE_DETAIL_TX_STATE comprise a set of mutually exclusive core radio states. Only one (or none) of these bits can be set at a time; otherwise the value is invalid.
The precise meaning of each of these three core bits, when set, depends on the value of the two bits RAIL_RF_STATE_DETAIL_TRANSITION and RAIL_RF_STATE_DETAIL_ACTIVE . When RAIL_RF_STATE_DETAIL_TRANSITION is set, the radio is transitioning into the core radio state corresponding to the set state bit; when clear, the radio is already in the core radio state that corresponds to the set state bit. When RAIL_RF_STATE_DETAIL_ACTIVE is set, the radio is actively transmitting or receiving; when clear, the radio is not actively transmitting or receiving. This bit will always be clear when RAIL_RF_STATE_DETAIL_IDLE_STATE is set, and will always be set when RAIL_RF_STATE_DETAIL_TX_STATE is set; otherwise the value is invalid.
The bit RAIL_RF_STATE_DETAIL_NO_FRAMES is set if the radio is currently operating with frame detection disabled, and clear otherwise. The bit RAIL_RF_STATE_DETAIL_LBT_SHIFT is set if an LBT/CSMA operation (e.g. performing CCA) is currently ongoing, and clear otherwise.
| Enumerator | |
|---|---|
| RAIL_RF_STATE_DETAIL_IDLE_STATE_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_IDLE_STATE bit. |
| RAIL_RF_STATE_DETAIL_RX_STATE_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_RX_STATE bit. |
| RAIL_RF_STATE_DETAIL_TX_STATE_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_TX_STATE bit. |
| RAIL_RF_STATE_DETAIL_TRANSITION_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_TRANSITION bit. |
| RAIL_RF_STATE_DETAIL_ACTIVE_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_ACTIVE bit. |
| RAIL_RF_STATE_DETAIL_NO_FRAMES_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_NO_FRAMES bit. |
| RAIL_RF_STATE_DETAIL_LBT_SHIFT |
Shift position of RAIL_RF_STATE_DETAIL_LBT bit. |
Definition at line
1830
of file
rail_types.h
.
Function Documentation
◆ RAIL_GetRadioState()
| RAIL_RadioState_t RAIL_GetRadioState | ( | RAIL_Handle_t |
railHandle
|
) |
Get the current radio state.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- An enumeration for the current radio state.
Returns the state of the radio as a bitmask containing: RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , RAIL_RF_STATE_TX , and RAIL_RF_STATE_ACTIVE . RAIL_RF_STATE_IDLE , RAIL_RF_STATE_RX , and RAIL_RF_STATE_TX bits are mutually exclusive. The radio can transition through intermediate states, which are not reported but are instead considered part of the state most closely associated. For example, when the radio is warming up or shutting down the transmitter or receiver, this function returns RAIL_RF_STATE_TX or RAIL_RF_STATE_RX , respectively. When transitioning directly from RX to TX or vice-versa, this function returns the earlier state.
- Note
- For a more detailed radio state, see RAIL_GetRadioStateDetail
◆ RAIL_GetRadioStateDetail()
| RAIL_RadioStateDetail_t RAIL_GetRadioStateDetail | ( | RAIL_Handle_t |
railHandle
|
) |
Get the detailed current radio state.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- An enumeration for the current detailed radio state.
Returns the state of the radio as a bitmask. The three core radio states IDLE, RX, and TX are represented by mutually exclusive bits RAIL_RF_STATE_DETAIL_IDLE_STATE , RAIL_RF_STATE_DETAIL_RX_STATE , and RAIL_RF_STATE_DETAIL_TX_STATE respectively. If the radio is transitioning between these three states, the returned bitmask will have RAIL_RF_STATE_DETAIL_TRANSITION set along with a bit corresponding to the destination core radio state. If, while in the receive state, the radio is actively receiving a packet, RAIL_RF_STATE_DETAIL_ACTIVE will be set; otherwise, this bit will be clear. If frame detection is disabled, RAIL_RF_STATE_DETAIL_NO_FRAMES in the returned state bitmask will be set; otherwise, this bit will be clear. If the radio is performing an LBT/CSMA operation (e.g. a backoff period) RAIL_RF_STATE_DETAIL_LBT in the returned state bitmask will be set; otherwise, this bit will be clear.
For the most part, the more detailed radio states returned by this API correspond to radio states returned by RAIL_GetRadioState as follows:
RAIL_RadioStateDetail_t RAIL_RadioState_t RAIL_RF_STATE_DETAIL_INACTIVE RAIL_RF_STATE_INACTIVE RAIL_RF_STATE_DETAIL_IDLE_STATE | RAIL_STATE_DETAIL_TRANSITION If RX overflow or leaving RX unforced: RAIL_RF_STATE_RX Else if leaving TX unforced: RAIL_RF_STATE_TX Else: RAIL_RF_STATE_IDLE RAIL_RF_STATE_DETAIL_IDLE_STATE RAIL_RF_STATE_IDLE RAIL_RF_STATE_DETAIL_IDLE_STATE | RAIL_STATE_DETAIL_LBT RAIL_RF_STATE_TX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_STATE_DETAIL_TRANSITION If leaving TX: RAIL_RF_STATE_TX Else: RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_RF_STATE_DETAIL_TRANSITION | RAIL_RF_STATE_DETAIL_NO_FRAMES If leaving TX: RAIL_RF_STATE_TX Else: RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_RF_STATE_DETAIL_NO_FRAMES RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_RF_STATE_DETAIL_LBT RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_RF_STATE_DETAIL_NO_FRAMES | RAIL_RF_STATE_DETAIL_LBT RAIL_RF_STATE_RX RAIL_RF_STATE_DETAIL_RX_STATE | RAIL_RF_STATE_DETAIL_ACTIVE RAIL_RF_STATE_RX_ACTIVE RAIL_RF_STATE_DETAIL_TX_STATE | RAIL_RF_STATE_TRANSITION If leaving RX: RAIL_RF_STATE_RX Else: RAIL_RF_STATE_TX RAIL_RF_STATE_DETAIL_TX_STATE | RAIL_RF_STATE_ACTIVE RAIL_RF_STATE_TX_ACTIVE
◆ RAIL_GetRxTransitions()
| RAIL_Status_t RAIL_GetRxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Get the current RAIL automatic state transitions after RX.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] transitionsThe state transitions that apply after receive.
- Returns
- Status code indicating a success of the function call.
Retrieves the current state transitions after RX and stores them in the transitions argument.
◆ RAIL_GetTxTransitions()
| RAIL_Status_t RAIL_GetTxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Get the current RAIL automatic state transitions after TX.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] transitionsThe state transitions that apply after transmission.
- Returns
- Status code indicating a success of the function call.
Retrieves the current state transitions after TX and stores them in the transitions argument.
◆ RAIL_Idle()
| void RAIL_Idle | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_IdleMode_t |
mode,
|
||
| bool |
wait
|
||
| ) |
Place the radio into an idle state.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] modeThe method for shutting down the radio. [in] waitWhether this function should wait for the radio to reach idle before returning.
This function is used to remove the radio from TX and RX states. How these states are left is defined by the mode parameter.
In multiprotocol, this API will also cause the radio to be yielded so that other tasks can be run. See Yielding the radio for more details.
◆ RAIL_SetRxTransitions()
| RAIL_Status_t RAIL_SetRxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Configure RAIL automatic state transitions after RX.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] transitionsThe state transitions to apply after reception.
- Returns
- Status code indicating success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the RX state. Success can transition to TX, RX, or IDLE, while error can transition to RX or IDLE. The timings of state transitions from the RX state are not guaranteed when packets are longer than 16 seconds on-air.
◆ RAIL_SetStateTiming()
| RAIL_Status_t RAIL_SetStateTiming | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_StateTiming_t * |
timings
|
||
| ) |
Configure RAIL automatic state transition timing.
- Parameters
-
[in] railHandleA RAIL instance handle. [in,out] timingsThe timings used to configure the RAIL state machine. This structure is overwritten with the actual times that were set, if an input timing is invalid.
- Returns
- Status code indicating a success of the function call.
The timings given are close to the actual transition time. However, a still uncharacterized software overhead occurs. Also, timings are not always adhered to when using an automatic transition after an error, due to the cleanup required to recover from the error.
◆ RAIL_SetTxTransitions()
| RAIL_Status_t RAIL_SetTxTransitions | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_StateTransitions_t * |
transitions
|
||
| ) |
Configure RAIL automatic state transitions after TX.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] transitionsThe state transitions to apply after transmission.
- Returns
- Status code indicating a success of the function call.
This function fails if unsupported transitions are passed in or if the radio is currently in the TX state. Success and error can each transition to RX or IDLE.