Recommended Utility
RAIL Recommended Utility
This optional software component can be enabled to include a recommended collection of other optional RAIL utilities.
This RAIL utility attempts to identify those RAIL utilities most commonly used by applications. If a list of utilities different from what is auto-selected here is sought, this component must be removed from the project with the custom list manually being added to the project.
Common RAIL utilities recommended for general use include:
- Initialization
- Callbacks
- Protocol
- Power Amplifier (PA)
- Packet Trace Interface (PTI)
- Received Signal Strength Indicator (RSSI)
-
Direct Memory Access (DMA)
- This primarily accelerates radio initialization, so it is currently included only for dynamic multiprotocol (DMP) scenarios.