Callbacks Utility
RAIL Callbacks Utility
This optional software component can be enabled to include default functionality related to RAIL callback configuration.
This utility provides basic callbacks that can be made available to RAIL. If a callback is not registered for use, it will be compiled out. The provided callbacks include:
-
RAILCb_AssertFailed
- This callback is called when a RAIL library-level assertion occurs. This callback occurs regardless of the other configuration options enabled in this software component.
- This callback overrides a weak function in the RAIL library and as such cannot be compiled out. Any assert within the RAIL library will cause this callback to run and provide information as to the cause.
-
The weak function
sl_rail_util_on_assert_failedis provided for application use and will be called when RAILCb_AssertFailed is called.
-
sli_rail_util_on_rf_ready- This callback is called when the call to RAIL_Init completes.
-
The
Initialize RAILconfiguration option must be enabled, and this callback must be passed as a parameter to RAIL_Init in order to enable its use. -
The weak function
sl_rail_util_on_rf_readyis provided for application use and will be called whensli_rail_util_on_rf_readyis called.
-
sli_rail_util_on_channel_config_change- This callback is called when an automatic switch from one channel configuration entry to another is performed internal to the RAIL library.
-
The
Initialize RAILandProtocol Configurationconfiguration options must be enabled, and this callback must be passed as a parameter to RAIL_ConfigChannels in order to enable its use. -
The weak function
sl_rail_util_on_channel_config_changeis provided for application use and will be called whensli_rail_util_on_channel_config_changeis called.
-
sli_rail_util_on_event- This callback is called when a configured radio event occurs. The radio events capable of causing this callback are identified in RAIL_Events_t .
-
The
Initialize RAILandRadio Event Configurationconfiguration options must be enabled, and this callback must be passed as a parameter to RAIL_Init in order to enable its use. -
The weak function
sl_rail_util_on_eventis provided for application use and will be called whensli_rail_util_on_eventis called.