You are viewing documentation for version: 2.10 | 2.13 (latest) | Version History
RAIL 2.10.x:
- 605067: The SL_RAIL_TEST_PER warning has been removed from RAILtest when a PER pin is not configured for use.
RAIL 2.9.x:
- 381485: Added
configChannelHoppingMulti
command for pre-configuring channel hopping multi-sense mode parameters prior to issuing configRxChannelHopping
command. Also augmented configRxDutyCycle
command to allow parameterization of this mode.
- 402203: Augmented
configChannelHoppingOptions
command to allow specifying RSSI threshold when enabling that option. Augmented configRxDutyCycle
command to allow specifying options in general including the RSSI threshold.
- 427841: Updated the Command Line Interface (CLI) help display format.
- 488425: CLI commands are now displayed back to the user using the same capitalization as they are entered (e.g. entering command
configTXoptions
will display configTXoptions
and not configTxOptions
).
- 454890: Restructured RAILtest to use a common main.c template with a software component-based architecture to select software features.
- 487098: Disabled graphics, buttons, LEDs and PER test GPIO pin by default.
- 484333: Standardized spelling of
RAILtest
for consistency.
- Updated bootup message example:
{{(reset)}{App:RAILtest}{Built:Jul 19 2019 13:36:24}}
- 633846: Altered CLI input of command
setDebugSignal
.
- 630457: Fixed an issue where the RAIL PTI component would automatically reserve hardware pins when no pins were specified for use.
RAIL 2.8.x:
- 344361: Added new command
getCteSampleRate
to retrieve the actual ADC sample rate used to capture the CTE.
- 369727: Added new commands
setTxTimePos
and setRxTimePos
to designate the time position of displayed packet timestamps among the RAIL_PacketTimePosition_t choices. In txEnd messages, now also display the lastTxStart time, and fixed a bug with the lastTxStatus display.
- 406293: Fixed an issue where a memory pointer could be discarded from the event queue on queue overflow and never released. This can occur if the memory buffer pool is greater than the event queue size.
- 415017: Updated the RAILTest bootup message to incorporate the
reset
command, the application name and the date and time of the RAILTest build.
- Updated bootup message example:
{{(reset)}{App:RAIL Test App}{Built:Jul 19 2019 13:36:24}}
- 406080: Added new commands
configRfSenseWakeupPhy
and setRfSenseTxPayload
to support waking up chips that support RFSENSE Selective(OOK) mode. Updated sleep
and rfsense
commands to allow setting the syncword length and syncword for EFR32XG22 chips which support RFSENSE Selective(OOK) mode. The tx
command will always overwrite the TX FIFO with a default payload, hence setRfSenseTxPayload
must be used with fifoModeTestOptions
set to use txFifoManual
to prevent the FIFO being overwritten.
- 460516: Fixed minor railtest problem where
setConfigIndex
might not restart receiver listening like setChannel
would if the receiver was on when the command was issued.
RAIL 2.7.x:
- 368510: Fixed an issue if receive was entered because of a transmit state transition where we would not change the channel when calling setChannel and would ignore calls to
rx 1
to enter normal receive mode.
- 394431: Fixed an issue where the configured antenna diversity settings in HAL config would not be applied to the radio at startup.
RAIL 2.6.x:
- Fixed
setMultiTimer
which was ignoring its mode argument; abs
mode now works.
- The commands
setRxOptions
and configTxOptions
can now be called without any parameters to print the current state of these options.
- RAILTest now uses its config-changed callback for both external and internal radio configs to ensure that the appropriate PA level is always selected.
- Added 802.15.4
setDataReqLatency
command for testing purposes.
- Fixed some asynchronous event print outs related to Z-Wave beam frame reception since they could corrupt the output.
- Added
getChannelHoppingRssi
command to read the RSSI when in channel hopping mode on each available channel.
RAIL 2.5.x:
- Added the following multitimer commands.
enableMultiTimer
, setMultiTimer
, multiTimerCancel
, printMultiTimerStats
- Added
printRxErrors
command to enable/disable printing of unsuccessfully received packets.
- Added the ability to save command scripts to flash and run them from flash. Renamed command
startScript
to runScript
. Added command clearScript
.
RAIL 2.4.x:
- Added the RAM Modem Reconfiguration commands. These commands allow the dynamic configuration of the modem via a set of studio scripted commands.
RAIL 2.0.x:
setChannel
no longer requires the radio be idle.
RAIL 1.6.x:
- simple
tx
command transmits with defaults (i.e. don't wait for ack, send CRC, use sync word 0)
- configTxOptions now controls 3 options
- BIT0: Wait for ack
- BIT1: Send CRC
- BIT2: Sync Word ID
- setRxOptions now controls 3 options
- BIT0: Store CRC
- BIT1: Ignore CRC errors
- BIT2: Enable dual sync
RAIL 1.5.x:
- Added the following commands:
rxConfig
, setRxOptions
, setFixedLength
, fifoStatus
, dataConfig
, setTxFifoThreshold
, setRxFifoThreshold
, iqCapture
RAIL 1.4.1:
- Added the following commands:
setPtiProtcol
, sweepPower
, startAvgRssi
, getAvgRssi
, setBle1Mbps
, setBle2Mbps
RAIL 1.3.1:
- Added Bluetooth Low Energy commands
setBleMode
, getBleMode
, setBleChannelParams
, setBleAdvertising
- Fixed help text for
setPanId802154
, setshortAddr802154
, setLongAddr802154
- Changed parameters for
acceptFrames
separating the bitmask into individual elements
RAIL 1.3.0:
- Added Auto Acknowledgement commands
autoAckConfig
, autoAckDisable
, setAckPayload
, setAckLength
, printAckPacket
, getAutoAck
, autoAckPause
, setTxAckOptions
- Added IEEE 802.15.4 commands
enable802154
, config2p4GHz802154
, acceptFrames
, setPromiscuousMode
, setPanCoordinator
, setPanId802154
, setShortAddr802154
, setLongAddr802154
- Added scheduled RX command
rxAt
- Added
transmitWithOptions
and configTxOptions
commands
- Added
setDebugSignal
command.
RAIL 1.2.1:
- Added
setPaCtune
which can configure custom PA capacitor tuning values for TX and RX
- Fixed RSSI slope requiring a 4dB power change for 1dB change in the received packet print
RAIL 1.2.0:
- Added bit error rate test commands -
setBerConfig
, berRx
, and berStatus
.
- Added packet error rate test commands -
perRx
, perStatus
.
- Added the ability to set the RAIL timebase in microseconds -
setTime
.
- RxOverflow counter now only counts number of overflows, instead of mistakenly counting some non-overflow events.
- Removed the RfUs output parameter from the 'sleep' command due to it being incorrect.
RAIL 1.1 - May 15, 2016:
- Automatic state transitions and timings added via
setRxTransitions
, setTxTransitions
, and setTimings
.
- Ability to selectively enable the address filter on certain frame types added through
addressFilterByFrame
command.
- Independent status booleans were removed in favor of a single
AppMode
status variable, which keeps track of the state of RAILtest.
- More validation is done to ensure that certain RAIL commands are only run in the correct AppMode and radio state. The radio must be IDLE for
setChannel
, freqOverride
, setPower
, and setCtune
to succeed.
setTestMode
was removed in favor of individual commands for setTxUnderflow
, setRxOverflow
, and setCalibrations
toggleTone
became setTxTone
, and toggleStream
became setTxStream
.
- Removed command
getTicks
, since the RAIL_GetTime() function made the timer used unnecessary.
- Removed command
txTimeReport
, since it was exposing implemenation-specific behavior encapsulated by RAIL.
Beta 1 - November 16, 2015:
- New library features for RF Energy Sensing exposed via new
rfSense
and sleep
commands.
- New RAIL timer functionality exposed via the
setTimer
, timerCancel
, and printTimerStats
commands.
- New
printDataRates
command to get information about the current PHY's data rates.
- Documentation clean up.
Alpha 2 - September 14, 2015:
- Commands for filtering of receive packets based on defined address fields and compare values.
- Scheduling of packet transmission at an absolute time or after a defined delay.
- Packet transmission conditional on Clear Channel Assessment (CSMA, LBT).
- The ability to read RSSI manually.
- Capability to switch between multiple PHY configurations at runtime.
- Revised help text (more uniform parameter descriptions).