RAIL_ChannelConfig_t Struct Reference
A channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g., RAIL_StartTx() and RAIL_StartRx() .
#include <
rail_types.h
>
Data Fields |
|
| const uint32_t * | phyConfigBase |
|
Base radio configuration for the corresponding channel configuration entries.
|
|
| const uint32_t * | phyConfigDeltaSubtract |
|
Minimum radio configuration to restore channel entries back to base configuration.
|
|
| const RAIL_ChannelConfigEntry_t * | configs |
|
Pointer to an array of
RAIL_ChannelConfigEntry_t
entries.
|
|
| uint32_t | length |
|
Number of
RAIL_ChannelConfigEntry_t
entries.
|
|
| uint32_t | signature |
|
Signature for this structure.
|
|
A channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g., RAIL_StartTx() and RAIL_StartRx() .
A RAIL_ChannelConfig_t structure defines the channel scheme that an application uses when registered in RAIL_ConfigChannels() .
These are a few examples of different channel configurations:
Definition at line
1593
of file
rail_types.h
.
Field Documentation
◆ configs
| const RAIL_ChannelConfigEntry_t * RAIL_ChannelConfig_t::configs |
Pointer to an array of RAIL_ChannelConfigEntry_t entries.
Definition at line
1599
of file
rail_types.h
.
◆ length
| uint32_t RAIL_ChannelConfig_t::length |
Number of RAIL_ChannelConfigEntry_t entries.
Definition at line
1602
of file
rail_types.h
.
◆ phyConfigBase
| const uint32_t* RAIL_ChannelConfig_t::phyConfigBase |
Base radio configuration for the corresponding channel configuration entries.
Definition at line
1594
of file
rail_types.h
.
◆ phyConfigDeltaSubtract
| const uint32_t* RAIL_ChannelConfig_t::phyConfigDeltaSubtract |
Minimum radio configuration to restore channel entries back to base configuration.
Definition at line
1596
of file
rail_types.h
.
◆ signature
| uint32_t RAIL_ChannelConfig_t::signature |
Signature for this structure.
Only used on modules.
Definition at line
1603
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h