Angle of Arrival/Departure
These APIs are to a stack implementing BLE's angle of arrival and angle of departure functionality.
Data Structures |
|
| struct | RAIL_BLE_AoxConfig_t |
|
Contains arguments for
RAIL_BLE_ConfigAox
function.
|
|
| struct | RAIL_BLE_AoxAntennaPortPins_t |
|
Contains elements of
RAIL_BLE_AoxAntennaConfig_t
struct.
|
|
| struct | RAIL_BLE_AoxAntennaConfig_t |
|
Contains arguments for
RAIL_BLE_ConfigAoxAntenna
function for EFR32XG22.
|
|
Macros |
|
| #define | RAIL_BLE_AOX_ANTENNA_PIN_COUNT (6U) |
|
The maximum number of GPIO pins used for AoX Antenna switching.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_DO_SWITCH (0U) |
|
Deprecated AOX options.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_TX_ENABLED (0U) |
|
Deprecated AOX options.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_RX_ENABLED (0U) |
|
Deprecated AOX options.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_DISABLED (0U) |
|
Disable the AoX feature.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE (1U << RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT) |
|
Sets one of the two AoX sampling/switching modes: 1 us or 2 us window.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_CONNLESS (1U << RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT) |
|
Enables connectionless AoX Rx packets.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_CONN (1U << RAIL_BLE_AOX_OPTIONS_CONN_SHIFT) |
|
Enables connection based AoX Rx packets.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK (1U << RAIL_BLE_AOX_OPTIONS_BUFFER_LOCK_SHIFT) |
|
Disables CTE buffer lock.
|
|
| #define | RAIL_BLE_AOX_OPTIONS_ENABLED ( RAIL_BLE_AOX_OPTIONS_CONN | RAIL_BLE_AOX_OPTIONS_CONNLESS ) |
|
Enables connection based or connectionless AoX Rx packets.
|
|
Enumerations |
|
| enum |
RAIL_BLE_AoxOptions_t
{
RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT = 0, RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT = 1, RAIL_BLE_AOX_OPTIONS_CONN_SHIFT = 2, RAIL_BLE_AOX_OPTIONS_LOCK_CTE_BUFFER_SHIFT = 3 } |
|
Angle of Arrival/Departure options bit fields.
|
|
Functions |
|
| bool | RAIL_BLE_LockCteBuffer ( RAIL_Handle_t railHandle, bool lock) |
|
Lock/unlock the CTE buffer from the application's perspective.
|
|
| bool | RAIL_BLE_CteBufferIsLocked ( RAIL_Handle_t railHandle) |
|
Determine whether the CTE buffer is currently locked or not.
|
|
| uint32_t | RAIL_BLE_GetCteSampleRate ( RAIL_Handle_t railHandle) |
|
Get the effective sample rate used by the ADC to capture the CTE samples.
|
|
| RAIL_Status_t | RAIL_BLE_ConfigAox ( RAIL_Handle_t railHandle, const RAIL_BLE_AoxConfig_t *aoxConfig) |
|
Configure Angle of Arrival/Departure (AoX) functionality.
|
|
| RAIL_Status_t | RAIL_BLE_InitCte ( RAIL_Handle_t railHandle) |
|
Perform one time initialization of AoX registers.
|
|
| RAIL_Status_t | RAIL_BLE_ConfigAoxAntenna ( RAIL_Handle_t railHandle, RAIL_BLE_AoxAntennaConfig_t *antennaConfig) |
|
Perform initialization of AoX antenna GPIO pins.
|
|
Detailed Description
These APIs are to a stack implementing BLE's angle of arrival and angle of departure functionality.
They are designed for use by the Silicon Labs BLE stack only at this time and may cause problems if accessed directly.
Macro Definition Documentation
◆ RAIL_BLE_AOX_ANTENNA_PIN_COUNT
| #define RAIL_BLE_AOX_ANTENNA_PIN_COUNT (6U) |
The maximum number of GPIO pins used for AoX Antenna switching.
If the user configures more pins using RAIL_BLE_ConfigAoxAntenna than allowed RAIL_BLE_AOX_ANTENNA_PIN_COUNT , then RAIL_STATUS_INVALID_PARAMETER status will be returned.
RAIL_STATUS_INVALID_CALL is returned if : RAIL_BLE_AOX_ANTENNA_PIN_COUNT is set to 0 or The user configures no pins.
The maximum value RAIL_BLE_AOX_ANTENNA_PIN_COUNT can take depends on number of Antenna route pins , a chip provides. For EFR32XG22, the maximum value of RAIL_BLE_AOX_ANTENNA_PIN_COUNT is 6. If the user configures fewer pins than RAIL_BLE_AOX_ANTENNA_PIN_COUNT , then only number of pins asked by user will be configured with RAIL_STATUS_NO_ERROR .
Definition at line
436
of file
rail_ble.h
.
Enumeration Type Documentation
◆ RAIL_BLE_AoxOptions_t
Angle of Arrival/Departure options bit fields.
| Enumerator | |
|---|---|
| RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT |
Shift position of RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE bit. |
| RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT |
Shift position of RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT bit. |
| RAIL_BLE_AOX_OPTIONS_CONN_SHIFT |
Shift position of RAIL_BLE_AOX_OPTIONS_CONN_SHIFT bit. |
| RAIL_BLE_AOX_OPTIONS_LOCK_CTE_BUFFER_SHIFT |
Shift position of RAIL_BLE_AOX_OPTIONS_LOCK_CTE_BUFFER_SHIFT bit. |
Definition at line
442
of file
rail_ble.h
.
Function Documentation
◆ RAIL_BLE_ConfigAox()
| RAIL_Status_t RAIL_BLE_ConfigAox | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_BLE_AoxConfig_t * |
aoxConfig
|
||
| ) |
Configure Angle of Arrival/Departure (AoX) functionality.
AoX is a method of radio localization which infers angle of arrival/departure of the signal based on different phases of the raw I/Q signal from different antennas by controlling external RF switch during the continuous tone extension (CTE). Connection based AoX packets are different than normal BLE packets in that they have 3 header bytes instead of 2 and they have CTE appended after the payload's CRC. 3rd byte or CTE info contains CTE length. Connectionless AoX packets have 2 header bytes and CTE info is part of the payload. AoX is supported on EFR32XG12/13/14 only on legacy 1Mbps BLE PHY. Note that calling RAIL_GetRadioEntropy during AoX reception may break receiving packets.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] aoxConfigConfiguration options for AoX
- Returns
- RAIL_Status_t indicating success or failure of the call.
◆ RAIL_BLE_ConfigAoxAntenna()
| RAIL_Status_t RAIL_BLE_ConfigAoxAntenna | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_BLE_AoxAntennaConfig_t * |
antennaConfig
|
||
| ) |
Perform initialization of AoX antenna GPIO pins.
This function must be called before RAIL_BLE_ConfigAox and RAIL_BLE_InitCte , else a RAIL_STATUS_INVALID_CALL is returned.
If user configures more pins, i.e., antCount in RAIL_BLE_AoxAntennaConfig_t , than allowed RAIL_BLE_AOX_ANTENNA_PIN_COUNT , then the API returns RAIL_STATUS_INVALID_PARAMETER .
If user configures lesser than or equal to number of pins allowed by RAIL_BLE_AOX_ANTENNA_PIN_COUNT , then the requested number of pins are configured and RAIL_STATUS_NO_ERROR is returned.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] antennaConfigstructure to hold the set of ports and pins to configure Antenna pins for AoX Antenna switching.
- Returns
- RAIL_Status_t indicating success or failure of the call.
◆ RAIL_BLE_CteBufferIsLocked()
| bool RAIL_BLE_CteBufferIsLocked | ( | RAIL_Handle_t |
railHandle
|
) |
Determine whether the CTE buffer is currently locked or not.
- Parameters
-
[in] railHandleA handle for RAIL instance.
- Returns
- True if CTE buffer is locked and false otherwise.
◆ RAIL_BLE_GetCteSampleRate()
| uint32_t RAIL_BLE_GetCteSampleRate | ( | RAIL_Handle_t |
railHandle
|
) |
Get the effective sample rate used by the ADC to capture the CTE samples.
- Parameters
-
[in] railHandleA handle for RAIL instance.
- Returns
- The actual sample rate used to capture the CTE in samples per second. On unsupported platforms this returns 0.
◆ RAIL_BLE_InitCte()
| RAIL_Status_t RAIL_BLE_InitCte | ( | RAIL_Handle_t |
railHandle
|
) |
Perform one time initialization of AoX registers.
This function must be called before RAIL_BLE_ConfigAox
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- RAIL_Status_t indicating success or failure of the call.
◆ RAIL_BLE_LockCteBuffer()
| bool RAIL_BLE_LockCteBuffer | ( | RAIL_Handle_t |
railHandle,
|
| bool |
lock
|
||
| ) |
Lock/unlock the CTE buffer from the application's perspective.
The radio will write to the buffer only if the bit is NOT set at the beginning of the sampling period. The radio will set the bit once the sampling period starts to indicate that some CTE data has been collected, which will not be overwritten during the next sampling period, unless the buffer is unlocked by the application.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] lockLock the CTE buffer if true and unlock it if false.
- Returns
- True if the CTE buffer is locked after the call, otherwise false.