Basic information about a packet being received or already completed and awaiting processing, including memory pointers to its data in the circular receive FIFO buffer.
#include <
rail_types.h
>
Data Fields | |
RAIL_RxPacketStatus_t | packetStatus |
The packet status of this packet. | |
uint16_t | packetBytes |
The number of packet data bytes available to read in this packet. | |
uint16_t | firstPortionBytes |
The number of bytes in the first portion. | |
uint8_t * | firstPortionData |
The pointer to the first portion of packet data containing firstPortionBytes number of bytes. | |
uint8_t * | lastPortionData |
The pointer to the last portion of a packet, if any; NULL otherwise. | |
RAIL_AddrFilterMask_t | filterMask |
A bitmask representing which address filter(s) this packet has passed. |
Basic information about a packet being received or already completed and awaiting processing, including memory pointers to its data in the circular receive FIFO buffer.
This packet information refers to remaining packet data that has not already been consumed by RAIL_ReadRxFifo().
- Note
- Because the receive FIFO buffer is circular, a packet might start near the end of the buffer and wrap around to the beginning of the buffer to finish, hence the distinction between the first and last portions. Packets that fit without wrapping only have a first portion (firstPortionBytes == packetBytes and lastPortionData will be NULL).
Definition at line 3023
of file rail_types.h
.
Field Documentation
◆ filterMask
RAIL_AddrFilterMask_t RAIL_RxPacketInfo_t::filterMask |
A bitmask representing which address filter(s) this packet has passed.
Will be 0 when not filtering or if packet info is retrieved before filtering has completed. It's undefined on platforms lacking RAIL_SUPPORTS_ADDR_FILTER_MASK
Definition at line 3035
of file rail_types.h
.
◆ firstPortionBytes
uint16_t RAIL_RxPacketInfo_t::firstPortionBytes |
The number of bytes in the first portion.
Definition at line 3027
of file rail_types.h
.
◆ firstPortionData
uint8_t* RAIL_RxPacketInfo_t::firstPortionData |
The pointer to the first portion of packet data containing firstPortionBytes number of bytes.
Definition at line 3028
of file rail_types.h
.
◆ lastPortionData
uint8_t* RAIL_RxPacketInfo_t::lastPortionData |
The pointer to the last portion of a packet, if any; NULL otherwise.
The number of bytes in this portion is packetBytes - firstPortionBytes.
Definition at line 3031
of file rail_types.h
.
◆ packetBytes
uint16_t RAIL_RxPacketInfo_t::packetBytes |
The number of packet data bytes available to read in this packet.
Definition at line 3025
of file rail_types.h
.
◆ packetStatus
RAIL_RxPacketStatus_t RAIL_RxPacketInfo_t::packetStatus |
The packet status of this packet.
Definition at line 3024
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h